FAQ: [#6422] [ltp] sendfile04 and sendfile04_64 fail in latest trunk(2010)

Document created by Aaronwu Employee on Sep 11, 2013
Version 1Show Document
  • View in full screen mode

[#6422] [ltp] sendfile04 and sendfile04_64 fail in latest trunk

Submitted By: Vivi Li

Open Date

2010-12-23 22:57:07     Close Date

2011-01-12 22:35:23

Priority:

Medium     Assignee:

steven miao

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2011R1     Release:

Category:

N/A     Board:

N/A

Processor:

ALL     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Rejected

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.3-trunk

App binary format:

N/A     

Summary: [ltp] sendfile04 and sendfile04_64 fail in latest trunk

Details:

 

LTP test cases of sendfile04 and sendfile04_64 fail in latest trunk, with ltp-full-20101031.

They are new cases, not a regression bug.

 

--

root:/> sendfile04

sendfile04    1  TFAIL  :  call succeeded unexpectedly

sendfile04    2  TFAIL  :  call succeeded unexpectedly

sendfile04    3  TFAIL  :  call succeeded unexpectedly

sendfile04    4  TFAIL  :  call succeeded unexpectedly

sendfile04    5  TFAIL  :  call succeeded unexpectedly

root:/> sendfile04_64

sendfile04_64    1  TFAIL  :  call succeeded unexpectedly

sendfile04_64    2  TFAIL  :  call succeeded unexpectedly

sendfile04_64    3  TFAIL  :  call succeeded unexpectedly

sendfile04_64    4  TFAIL  :  call succeeded unexpectedly

sendfile04_64    5  TFAIL  :  call succeeded unexpectedly

root:/>

--

 

Follow-ups

 

--- steven miao                                              2011-01-05 03:07:50

since blackfin arch has no process vm area protection implementation, it will

not return -EFAULT as expected when you pass a unmapped buffer pointer or

protected buffer pointer.

 

--- Vivi Li                                                  2011-01-12 22:35:22

So disable sendfile04 and sendfile04_64 in ltp_auto_test.exp.

Close it.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes