FAQ:[#6337] kernel_xip can not be build when xenomai is enabled.(2010)

Document created by Aaronwu Employee on Sep 11, 2013
Version 1Show Document
  • View in full screen mode

[#6337] kernel_xip can not be build when xenomai is enabled.

Submitted By: Vivi Li

Open Date

2010-11-10 23:35:45     Close Date

2010-11-29 01:23:30

Priority:

Medium     Assignee:

steven miao

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2010R1     Release:

Category:

N/A     Board:

N/A

Processor:

ALL     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

2010r1-rc4

App binary format:

N/A     

Summary: kernel_xip can not be build when xenomai is enabled.

Details:

 

kernel_xip can not be build when xenomai is enabled.

Both fdpic and shared-flat format are failed.

 

Before build the kernel, xenomai patch is applied to kernel and kernel is cleaned up.

 

Bellow is the error message:

--

  LD      vmlinux.o

  MODPOST vmlinux.o

  GEN     .version

  CHK     include/generated/compile.h

  UPD     include/generated/compile.h

  CC      init/version.o

  LD      init/built-in.o

  LD      .tmp_vmlinux1

arch/blackfin/mach-common/built-in.o: In function `system_call':

arch/blackfin/mach-common/entry.S:618: relocation truncated to fit: R_BFIN_PCREL24 against symbol `__ipipe_syscall_root' defined in .text section in arch/blackfin/kernel/built-in.o

arch/blackfin/mach-common/entry.S:695: relocation truncated to fit: R_BFIN_PCREL24 against symbol `__ipipe_sync_root' defined in .text section in arch/blackfin/kernel/built-in.o

make: *** [.tmp_vmlinux1] Error 1

--

 

Follow-ups

 

--- Mike Frysinger                                           2010-11-13 19:04:29

should be fixed in now by using pseudo_long_call.  although i dont know how

useful xenomai+xip really is ...

 

--- Vivi Li                                                  2010-11-29 01:23:30

OK now, close it.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

config.linux.kernel_xip.fdpic    application/octet-stream    32811    Vivi Li

Outcomes