FAQ: [#6248] test fail on bf537-stamp with suspend to ram mode in ad1836 power testing(2010)

Document created by Aaronwu Employee on Sep 11, 2013
Version 1Show Document
  • View in full screen mode

[#6248] test fail on bf537-stamp with suspend to ram mode in ad1836 power testing

Submitted By: angelia wu

Open Date

2010-09-09 03:40:24     Close Date

2010-10-21 01:31:48

Priority:

Medium     Assignee:

Bob Liu

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2010R1     Release:

Blackfin Linux:2010R1

Category:

N/A     Board:

N/A

Processor:

BF537     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Not reproducible

Uboot version or rev.:

    Toolchain version or rev.:

svn-4681

App binary format:

N/A     

Summary: test fail on bf537-stamp with suspend to ram mode in ad1836 power testing

Details:

 

test fail on bf537-stamp with suspend to ram mode in ad1836 power testing.

when test "Rvrec -w -S -b 16 -s 48000 -t 5|vplay", it show "NULL pointer access"

And this test with "standby" mode on bf537-stamp is ok and "ram" mode on bf533-stamp is also ok.

 

the log as follow.

 

 

U-Boot 2010.06-svn2366 (ADI-2010R1-pre) (Jul 27 2010 - 21:47:44)

 

CPU:   ADSP bf537-0.2 (Detected Rev: 0.2) (bypass boot)

Board: ADI BF537 stamp board

       Support: http://blackfin.uclinux.org/

Clock: VCO: 500 MHz, Core: 500 MHz, System: 125 MHz

RAM:   64 MiB

RAM size is 64 MB.

 

Flash: 4 MiB

In:    serial

Out:   serial

Err:   serial

KGDB:  [on serial] ready

Net:   bfin_mac

Hit any key to stop autoboot:  0

bfin> set bootargs root=/dev/mtdblock0 rw ip=10.100.4.50 earlyprintk=serial,uart0,57600 console=ttyBF0,57600

bfin> set serverip 10.100.4.174

bfin> set ipaddr 10.100.4.50

bfin> save

Saving Environment to Flash...

. done

Un-Protected 1 sectors

Erasing Flash...

. done

Erased 1 sectors

Writing to Flash... done

. done

Protected 1 sectors

bfin> printenv ethaddr

ethaddr=00:E0:22:FE:47:9E

bfin> mac address=00:E0:22:FE:47:9E

tftpboot 0x2000000 uImage

Using bfin_mac device

TFTP from server 10.100.4.174; our IP address is 10.100.4.50

Filename 'uImage'.

Load address: 0x2000000

Loading: #################################################################

     #################################################################

     #################################################################

     #################################################################

     ###########################################

done

Bytes transferred = 4444531 (43d173 hex)

Image size is 43d173

bfin> run addip

bfin> bootm

## Booting kernel from Legacy Image at 02000000 ...

   Image Name:   bf537-2.6.34.6-ADI-2010R1-pre-sv

   Created:      2010-09-09   7:12:55 UTC

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    4444467 Bytes = 4.2 MiB

   Load Address: 00001000

   Entry Point:  001c7684

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 001c7684

Linux version 2.6.34.6-ADI-2010R1-pre-svn9118 (test@uclinux41) (gcc version 4.3.5 (ADI-trunk/svn-4681) ) #210 Thu Sep 9 15:12:50 CST 2010

register early platform devices

bootconsole [early_shadow0] enabled

bootconsole [early_BFuart0] enabled

early printk enabled on early_BFuart0

Limiting kernel memory to 56MB due to anomaly 05000263

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x00132d48

  rodata    = 0x00132d48-0x00197968

  bss       = 0x00198000-0x001a8cb4

  data      = 0x001a8cb4-0x001bc000

    stack   = 0x001ba000-0x001bc000

  init      = 0x001bc000-0x008ec000

  available = 0x008ec000-0x03800000

  DMA Zone  = 0x03e00000-0x04000000

Hardware Trace Active and Enabled

Boot Mode: 0

Reset caused by Software reset

Blackfin support (C) 2004-2010 Analog Devices, Inc.

Compiled for ADSP-BF537 Rev 0.2

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 500 MHz core clock and 125 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

  External memory: cacheable in instruction cache

Data Cache Enabled for CPU0

  External memory: cacheable (write-back) in data cache

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 14224

Kernel command line: root=/dev/mtdblock0 rw ip=10.100.4.50 earlyprintk=serial,uart0,57600 console=ttyBF0,57600 ip=10.100.4.50:10.100.4.174:10.99.29.1:255.255.255.0:bf537-stamp:eth0:off

PID hash table entries: 256 (order: -2, 1024 bytes)

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 47640k/65536k RAM, (7360k init code, 1223k kernel code, 549k data, 2048k dma, 6716k reserved)

Hierarchical RCU implementation.

NR_IRQS:138

Configuring Blackfin Priority Driven Interrupts

console [ttyBF0] enabled, bootconsole disabled

console [ttyBF0] enabled, bootconsole disabled

Calibrating delay loop... 995.32 BogoMIPS (lpj=1990656)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (16 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (35 KB free)

NET: Registered protocol family 16

Blackfin DMA Controller

stamp_init(): registering device resources

bio: create slab <bio-0> at 0

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@7

Advanced Linux Sound Architecture Driver Version 1.0.22.1.

Switching to clocksource bfin_cs_cycles

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

UDP hash table entries: 256 (order: 0, 4096 bytes)

UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)

NET: Registered protocol family 1

msgmni has been set to 93

io scheduler noop registered

io scheduler cfq registered (default)

bfin-uart: Blackfin serial driver

bfin-uart.0: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART

brd: module loaded

bfin_mii_bus: probed

bfin_mii_bus: Can't get IRQ 65535 (PHY)

bfin_mac: attached PHY driver [SMSC LAN83C185] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=24)@sclk=125MHz)

bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

ALSA device list:

  No soundcards found.

TCP cubic registered

NET: Registered protocol family 17

,IP-Config: Gateway not on directly connected network.13:15:44 UTC (306944)

dma_alloc_init: dma_page @ 0x02943000 - 512 pages at 0x03e00000

Freeing unused kernel memory: 7360k freed

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            - http://blackfin.uclinux.org/

\    YP"    `| 8P  `.          - http://docs.blackfin.uclinux.org/

/     \.___.d|    .'           - http://www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    - http://www.analog.com/blackfin

 

Have a lot of fun...

 

 

BusyBox v1.16.2 (2010-09-09 15:10:45 CST) hush - the humble shell

 

root:/> version^[[56;9R

kernel:    Linux release 2.6.34.6-ADI-2010R1-pre-svn9118, build #210 Thu Sep 9 15:12:50 CST 2010

toolchain: bfin-linux-uclibc-gcc release gcc version 4.3.5 (ADI-trunk/svn-4681)

user-dist: release svn-9801, build #99 Thu Sep 9 15:12:14 CST 2010

root:/>

*******************************************************************

STEP 3: Start testing

 

 

^[[56;9RPHY: 0:01 - Link is Up - 100/Full

 

root:/> ^[[56;9Rmodprobe snd_ad183x

dma rx:3 tx:4, err irq:45, regs:ffc00800

asoc: AD183X <-> bf5xx-tdm mapping ok

root:/> ^[[56;9Rlsmod

Module                  Size  Used by

snd_ad183x               801  0

snd_bf5xx_tdm           1853  1 snd_ad183x

snd_soc_ad183x          7921  1 snd_ad183x

snd_soc_bf5xx_tdm       2157  1 snd_ad183x

snd_soc_bf5xx_sport     9444  2 snd_bf5xx_tdm,snd_soc_bf5xx_tdm

root:/>

Case 1 ...PASS

^[[56;9Rvrec -w -S -b 16 -s 48000 -t 5|vplay

Recording WAVE : 16 bit, Speed 48000 Hz Stereo ...

Playing WAVE : 16 bit, Speed 48000 Hz Stereo ...

root:/>

Case 2 ...PASS

arecord -t wav -c 2 -f S16_LE -r 48000 -d 5 |aplay^[[56;1R

Recording WAVE 'stdin' : Signed 16 bit Little Endian, Rate 48000 Hz, Stereo

Playing WAVE 'stdin' : Signed 16 bit Little Endian, Rate 48000 Hz, Stereo

root:/>

Case 3 ...PASS

^[[56;9Rcat /proc/mounts

rootfs / rootfs rw 0 0

proc /proc proc rw,nosuid,nodev,noexec,relatime 0 0

sysfs /sys sysfs rw,nosuid,nodev,noexec,relatime 0 0

mdev /dev tmpfs rw,nosuid,relatime,mode=0755,size=10M 0 0

devpts /dev/pts devpts rw,nosuid,noexec,relatime,mode=600 0 0

var /var ramfs rw,relatime 0 0

tmp /tmp tmpfs rw,nosuid,nodev,relatime 0 0

debugfs /sys/kernel/debug debugfs rw,relatime 0 0

root:/>

Case 4 ...PASS

^[[56;9Rls /sys/power

pm_async  state

root:/>

Case 5 ...PASS

^[[56;9R

root:/> rtcwake -s 15 -m mem

wakeup from "mem" at Sun Jan  4 13:16:33 1970

PM: Syncing filesystems ... done.

Freezing user space processes ... (elapsed 0.01 seconds) done.

Freezing remaining freezable tasks ... (elapsed 0.01 seconds) done.

Suspending console(s) (use no_console_suspend to debug)

PM: suspend of devices complete after 924.949 msecs

PM: late suspend of devices complete after 0.125 msecs

PM: early resume of devices complete after 0.061 msecs

PM: resume of devices complete after 1.088 msecs

Restarting tasks ... done.

root:/>

Case 6 ...PASS

^[[56;1Rvrec -w -S -b 16 -s 48000 -t 5|vplay

NULL pointer access

Kernel OOPS in progress

Deferred Exception context

CURRENT PROCESS:

COMM=vrec PID=201  CPU=0

TEXT = 0x02c00000-0x02c02890        DATA = 0x02085890-0x02085bf0

BSS = 0x02085bf0-0x02be0000  USER-STACK = 0x02bffe80

 

return address: [0x000d7ac8]; contents of:

0x000d7aa0:  c682  802b  67f8  5010  2ef8  4d81  608a  2fe4

0x000d7ab0:  6003  2fdd  04c4  3228  0167  6fa6  0c45  180b

0x000d7ac0:  0000  0000  e52c  001c [e5a0] 0210  4800  1012

0x000d7ad0:  4808  1006  6000  6c66  0127  0484  0010  3045

 

ADSP-BF537-0.2 500(MHz CCLK) 125(MHz SCLK) (mpu off)

Linux version 2.6.34.6-ADI-2010R1-pre-svn9118 (test@uclinux41) (gcc version 4.3.5 (ADI-trunk/svn-4681) ) #210 Thu Sep 9 15:12:50 CST 2010

 

SEQUENCER STATUS:        Not tainted

SEQSTAT: 00000027  IPEND: 8008  IMASK: ffff  SYSCFG: 0006

  EXCAUSE   : 0x27

  physical IVG3 asserted : <0xffa007d8> { _trap + 0x0 }

  physical IVG15 asserted : <0xffa010bc> { _evt_system_call + 0x0 }

  logical irq   6 mapped  : <0xffa003ec> { _bfin_coretmr_interrupt + 0x0 }

  logical irq  10 mapped  : <0x000bdf08> { _bfin_rtc_interrupt + 0x0 }

  logical irq  12 mapped  : <0x02c05198> { :snd_soc_bf5xx_sport:_sport_done + 0x458 }

  logical irq  13 mapped  : <0x02c05130> { :snd_soc_bf5xx_sport:_sport_done + 0x3f0 }

  logical irq  18 mapped  : <0x000a9968> { _bfin_serial_dma_rx_int + 0x0 }

  logical irq  19 mapped  : <0x000a96c0> { _bfin_serial_dma_tx_int + 0x0 }

  logical irq  24 mapped  : <0x000b9438> { _bfin_mac_interrupt + 0x0 }

  logical irq  45 mapped  : <0x02c04e5c> { :snd_soc_bf5xx_sport:_sport_done + 0x11c }

RETE: <0x00000000> /* Maybe null pointer? */

RETN: <0x02d3bc1c> /* kernel dynamic memory (maybe user-space) */

RETX: <0x00000480> /* Maybe fixed code section */

RETS: <0x000d7d1c> { _snd_pcm_oss_set_trigger + 0x18 }

PC  : <0x000d7ac8> { _snd_pcm_oss_make_ready + 0x14 }

DCPLB_FAULT_ADDR: <0x00000210> /* Maybe null pointer? */

ICPLB_FAULT_ADDR: <0x000d7ac8> { _snd_pcm_oss_make_ready + 0x14 }

PROCESSOR STATE:

R0 : 02b31800    R1 : 000d7024    R2 : 001a700c    R3 : 00000003

R4 : 00000001    R5 : 02d3bd08    R6 : 00000001    R7 : 000d7024

P0 : 00000040    P1 : 02d3bd08    P2 : 02d38ea0    P3 : 02b31800

P4 : 00000000    P5 : 02b31800    FP : 02b318d8    SP : 02d3bb40

LB0: ffa017aa    LT0: ffa017aa    LC0: 00000000

LB1: 000d8584    LT1: 000d8584    LC1: 00000000

B0 : 00000137    L0 : 00000000    M0 : fffffffc    I0 : 02d3bcd4

B1 : 000000c0    L1 : 00000000    M1 : 00000001    I1 : 02d8ec00

B2 : 7ffff000    L2 : 00000000    M2 : 00001802    I2 : 00000003

B3 : 00000000    L3 : 00000000    M3 : 0000005b    I3 : 00000006

A0.w: 0000147a   A0.x: 00000000   A1.w: 0000147a   A1.x: 00000000

USP : 02bffd74  ASTAT: 02003004

 

Hardware Trace:

   0 Target : <0x00003ef8> { _trap_c + 0x0 }

     Source : <0xffa0076c> { _exception_to_level5 + 0xa4 } CALL pcrel

   1 Target : <0xffa006c8> { _exception_to_level5 + 0x0 }

     Source : <0xffa0057c> { _bfin_return_from_exception + 0x20 } RTX

   2 Target : <0xffa0055c> { _bfin_return_from_exception + 0x0 }

     Source : <0xffa00620> { _ex_trap_c + 0x74 } JUMP.S

   3 Target : <0xffa005ac> { _ex_trap_c + 0x0 }

     Source : <0xffa00484> { _ex_workaround_261 + 0x1c } JUMP.S

   4 Target : <0xffa00468> { _ex_workaround_261 + 0x0 }

     Source : <0xffa00840> { _trap + 0x68 } JUMP (P4)

   5 Target : <0xffa007f6> { _trap + 0x1e }

     Source : <0xffa007f2> { _trap + 0x1a } IF CC JUMP pcrel

   6 Target : <0xffa007d8> { _trap + 0x0 }

      FAULT : <0x000d7ac8> { _snd_pcm_oss_make_ready + 0x14 } R0 = B[P4 + 0x40](X)

     Source : <0xffa0057c> { _bfin_return_from_exception + 0x20 } RTX

   7 Target : <0xffa0055c> { _bfin_return_from_exception + 0x0 }

     Source : <0xffa0047a> { _ex_workaround_261 + 0x12 } IF !CC JUMP pcrel

   8 Target : <0xffa00468> { _ex_workaround_261 + 0x0 }

     Source : <0xffa00840> { _trap + 0x68 } JUMP (P4)

   9 Target : <0xffa007f6> { _trap + 0x1e }

     Source : <0xffa007f2> { _trap + 0x1a } IF CC JUMP pcrel

  10 Target : <0xffa007d8> { _trap + 0x0 }

     Source : <0x000d7ac4> { _snd_pcm_oss_make_ready + 0x10 } P4 = [P5 + 0x70]

  11 Target : <0x000d7ab4> { _snd_pcm_oss_make_ready + 0x0 }

     Source : <0x000d7d18> { _snd_pcm_oss_set_trigger + 0x14 } JUMP.L

  12 Target : <0x000d7d04> { _snd_pcm_oss_set_trigger + 0x0 }

     Source : <0x000d7ee4> { _snd_pcm_oss_poll + 0xd0 } CALL pcrel

  13 Target : <0x000d7ee4> { _snd_pcm_oss_poll + 0xd0 }

     Source : <0x000d8518> { _snd_pcm_oss_open_file + 0xb4 } JUMP.S

  14 Target : <0x000d850a> { _snd_pcm_oss_open_file + 0xa6 }

     Source : <0x000d8642> { _snd_pcm_oss_open_file + 0x1de } IF !CC JUMP pcrel (BP)

  15 Target : <0x000d863e> { _snd_pcm_oss_open_file + 0x1da }

     Source : <0x000d8508> { _snd_pcm_oss_open_file + 0xa4 } IF CC JUMP pcrel

Kernel Stack

Stack info:

SP: [0x02d3bf24] <0x02d3bf24> /* kernel dynamic memory (maybe user-space) */

Memory from 0x02d3bf20 to 02d3c000

02d3bf20: 02c023b4 [029cd350] 00008000  00000000  00000000  02d3c000  029cd350  029cd350

02d3bf40: 02c01fe4  ffa01120  02002021  02963ffb  029645cf  02963ff8  029645ce  00000000

02d3bf60: 00000000  0000147a  00000000  0000147a  00000000  00000000  7ffff000  000000c0

02d3bf80: 00000137  00000000  00000000  00000000  00000000  0000005b  00001802  00000001

02d3bfa0: fffffffc  00000006  00000003  020711f0  02bffff0  02bffd74  02bffd80  02c026d0

02d3bfc0: 02085a40  020711f0  02cb828c  029cd334  00000005  02bffe84  00000009  02c023b4

02d3bfe0: 02085bd8  02c023b4  00000000  00000000  02c023b4  02c023b4  00000005  00000006

Return addresses in stack:

Modules linked in: snd_ad183x snd_bf5xx_tdm snd_soc_ad183x snd_soc_bf5xx_tdm snd_soc_bf5xx_sport

Kernel panic - not syncing: Kernel exception

Hardware Trace:

Stack info:

SP: [0x02d3ba64] <0x02d3ba64> /* kernel dynamic memory (maybe user-space) */

FP: (0x02d3bf00)

Memory from 0x02d3ba60 to 02d3c000

02d3ba60: 00000013 [001651c4] 00132cba  02d3bb40  001651c4  0019d3ce  0019d3ce  0019d3ce

02d3ba80: 02d3ba94  00004330  02d3bb40  00008008  02d3bb40  0000003f  0000003f  001b85dc

02d3baa0: 00000001  0003000b  001b7bb0  00000000  02d3bae0  000039ac  0000002c  00000000

02d3bac0: 001b7bd0  020084ec  00039e62  000240d0  001b85e0  020084e0  00000001  00000000

02d3bae0: 00000001  0000ffff  ffb01000  ffa011fc  04830000  00000000  00000041  02000600

02d3bb00: 00044696  00044162  02000600  02002420  00044bec  00000000  00000000  ffa00770

02d3bb20: 0019a000  00008008  00000027  02d3bd08  00000001  000000d0  00000000  00000480

02d3bb40: 00000480  00008008  00000027  00000000  02d3bc1c  00000480  000d7ac8  000d7d1c

02d3bb60: 02b31800  02003004  000d8584  ffa017aa  000d8584  ffa017aa  00000000  00000000

02d3bb80: 0000147a  00000000  0000147a  00000000  00000000  7ffff000  000000c0  00000137

02d3bba0: 00000000  00000000  00000000  00000000  0000005b  00001802  00000001  fffffffc

02d3bbc0: 00000006  00000003  02d8ec00  02d3bcd4  02bffd74  02b318d8  02b31800  00000000

02d3bbe0: 02b31800  02d38ea0  02d3bd08  00000040  000d7024  00000001  02d3bd08  00000001

02d3bc00: 00000003  001a700c  000d7024  02b31800  02b31800  00000040  00000006  02a940bc

02d3bc20: 0000000b  ffffffff  000d7d1c  02a94000  02d38ea0  00000000  ffffffe0  00000000

02d3bc40: 02dfc620  000d7ee8  02a94000  02d38ea0  02d8dd20  00000000  ffa02948  00044696

02d3bc60: 00000000  02d3bc70  00000003  00000100  02d38ea0  02d3bcac  000d87a0  02b31800

02d3bc80: 02d3a000  00000001  02d3a000  02b31908  00000000  02b31914  02952f00  02b31800

02d3bca0: 02dfdf80  00000003  02d3bcac  00000000  00000000  00000000  00000000  00000000

02d3bcc0: 00000000  00000000  00000000  00000000  00000000  63657276  00000000  00000000

02d3bce0: 00000000  00036300  00934960  ffffffc0  0000003f  00000000  0204f3c0  0000f628

02d3bd00: 02b31914  02b31914  02d8dd20  02d8cad4 <000c477c> 001409d4  02dfc620  001a688c

02d3bd20: 00000000  00000003  00000003  00000024  02d8cad4  02dfc620  0200d220  02d3bdcc

02d3bd40: 02e552b4 <00048fb2> 02055720  02d8cad4  02dfc620  00000000  00048f44  00000000

02d3bd60: 02d3be30  00000000  0004cbd6  02d8cad4 <0004544a> 02dfc620  02d8cad4  0200d220

02d3bd80: 00000000  0004cce4  02d8cad4  00000024  00000001  00045670  02dfc620  02bbb000

02d3bda0: 00000000  00000000  00000000  02d3be30  0004e578  02d3be30  00000000  020546e0

02d3bdc0: 0004e15c  02d3be30  ffffff9c  00000000  00000000  00000001  0004fbba  0004fbba

02d3bde0: 02d3be30  02bbb000  ffffff9c  00000000  00000000  00000024  0000002d  1ba909ab

02d3be00: 0000002d  00000024  00000000  02bbb000  7fffffff  1ba909ab  02d3a000  02d3be44

02d3be20: 02d3a000  00000000  001acac4  02d3be7c  0200d220  02e552b4  0024543e  00000003

02d3be40: 02bbb005  0200d7a0  02011794  00000101  00000000  00000000  0000e100 <0009fc08>

02d3be60: 02075a20  0009fc1a  00000000  00005401  02bffd80  00044696  00000001  00000001

02d3be80: 00000000  02dfc620  001a3b70  0004e5ea  0200d220  02e552b4  02bffd80  000452e0

02d3bea0: 00000000  00000005  020711f0  ffffff9c  00000003  02bbb000  00000000  ffffff9c

02d3bec0: 0204f0e0  02d3bef4  00000000  00000000  00050e6c  000453a4  00045388  00000005

02d3bee0: 020711f0  00000000  ffffe000  02c023b4  02085bd8 <ffa0097a> 00050e0c  00000000

02d3bf00:(00000000)<ffa0097a> 00000000  029c22f0  00032b60  0000fffe  02c023b4  02085bd8

02d3bf20: 02c023b4  029cd350  00008000  00000000  00000000  02d3c000  029cd350  029cd350

02d3bf40: 02c01fe4  ffa01120  02002021  02963ffb  029645cf  02963ff8  029645ce  00000000

02d3bf60: 00000000  0000147a  00000000  0000147a  00000000  00000000  7ffff000  000000c0

02d3bf80: 00000137  00000000  00000000  00000000  00000000  0000005b  00001802  00000001

02d3bfa0: fffffffc  00000006  00000003  020711f0  02bffff0  02bffd74  02bffd80  02c026d0

02d3bfc0: 02085a40  020711f0  02cb828c  029cd334  00000005  02bffe84  00000009  02c023b4

02d3bfe0: 02085bd8  02c023b4  00000000  00000000  02c023b4  02c023b4  00000005  00000006

Return addresses in stack:

    address : <0x000c477c> { _soundcore_open + 0x7c }

    address : <0x00048fb2> { _chrdev_open + 0x6e }

    address : <0x0004544a> { ___dentry_open + 0x92 }

    address : <0x0009fc08> { _tty_ioctl + 0xc8 }

    address : <0xffa0097a> { _system_call + 0x6a }

   frame  1 : <0xffa0097a> { _system_call + 0x6a }

 

Last passed test result is not found!!

 

Case 7 ...FAIL

 

POWER AD1836 TEST (SUSPEND-TO-RAM) FAIL

 

Follow-ups

 

--- Bob Liu                                                  2010-09-13 04:30:57

I can't repeat this problem in lastest svn trunk.

 

By the way, if there is error like this:

 

root:/> arecord -t wav -c 2 -f S16_LE -r 48000 -d 5 |aplay

arecord: can't resolve symbol '___snd_pcm_hw_params_{et_period_size_last'

aplay: can't resolve symbol '___snd_pcm_hw_params_{et_period_size_last'

root:/>

 

Don't forget add a pull down resistor to SCKE.

 

Refer Bug[#5370]:

http://blackfin.uclinux.org/gf/project/uclinux-dist/tracker/?action=TrackerItemEdit&tracker_item_id=5370

 

--- angelia wu                                               2010-10-21 01:31:48

I test it again and now the case is pass.

I closed it.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

kernel.537ad1836.power.config    application/x-config    36895    angelia wu

test_537ad1836_power_log    application/octet-stream    46367    angelia wu

user.537ad1836.power.config    application/x-config    49070    angelia wu

Outcomes