FAQ: [#6180] Build directfb with bf527-ezkit-v2 board config, application fails to run(2010)

Document created by Aaronwu Employee on Sep 11, 2013
Version 1Show Document
  • View in full screen mode

[#6180] Build directfb with bf527-ezkit-v2 board config, application fails to run

Submitted By: Vivi Li

Open Date

2010-08-12 23:59:43     Close Date

2010-08-20 03:22:16

Priority:

Medium     Assignee:

Michael Hennerich

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2010R1     Release:

Category:

N/A     Board:

EZKIT Lite

Processor:

BF527     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.3-2010_Aug_04

App binary format:

N/A     

Summary: Build directfb with bf527-ezkit-v2 board config, application fails to run

Details:

 

Build directfb with bf527-ezkit-v2 board config, application fails to run.

 

Bellow is the log:

--

Linux version 2.6.34.3-ADI-2010R1-pre-svn9076 (test@uclinux60-bf527-std) (gcc version 4.3.5 (ADI-trunk/svn-4747) ) #12 Thu Aug 10

register early platform devices

bootconsole [early_shadow0] enabled

bootconsole [early_BFuart1] enabled

early printk enabled on early_BFuart1

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x0015dda8

  rodata    = 0x0015dda8-0x001d53ec

  bss       = 0x001d6000-0x001ea95c

  data      = 0x001ea95c-0x00204000

    stack   = 0x00202000-0x00204000

  init      = 0x00204000-0x00b2d000

  available = 0x00b2d000-0x03f00000

  DMA Zone  = 0x03f00000-0x04000000

Hardware Trace Active and Enabled

Boot Mode: 1

Blackfin support (C) 2004-2010 Analog Devices, Inc.

Compiled for ADSP-BF527 Rev 0.2

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 525 MHz core clock and 131 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

  External memory: cacheable in instruction cache

Data Cache Enabled for CPU0

  External memory: cacheable (write-back) in data cache

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 16002

Kernel command line: root=/dev/mtdblock2 rw clkin_hz=25000000 earlyprintk=serial,uart1,57600 console=tty0 console=ttyBF1,57600 if

PID hash table entries: 256 (order: -2, 1024 bytes)

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 52500k/65536k RAM, (9380k init code, 1395k kernel code, 665k data, 1024k dma, 572k reserved)

Hierarchical RCU implementation.

NR_IRQS:159

Configuring Blackfin Priority Driven Interrupts

Console: colour dummy device 80x25

Linux version 2.6.34.3-ADI-2010R1-pre-svn9076 (test@uclinux60-bf527-std) (gcc version 4.3.5 (ADI-trunk/svn-4747) ) #12 Thu Aug 10

register early platform devices

bootconsole [early_shadow0] enabled

bootconsole [early_BFuart1] enabled

early printk enabled on early_BFuart1

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x0015dda8

  rodata    = 0x0015dda8-0x001d53ec

  bss       = 0x001d6000-0x001ea95c

  data      = 0x001ea95c-0x00204000

    stack   = 0x00202000-0x00204000

  init      = 0x00204000-0x00b2d000

  available = 0x00b2d000-0x03f00000

  DMA Zone  = 0x03f00000-0x04000000

Hardware Trace Active and Enabled

Boot Mode: 1

Blackfin support (C) 2004-2010 Analog Devices, Inc.

Compiled for ADSP-BF527 Rev 0.2

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 525 MHz core clock and 131 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

  External memory: cacheable in instruction cache

Data Cache Enabled for CPU0

  External memory: cacheable (write-back) in data cache

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 16002

Kernel command line: root=/dev/mtdblock2 rw clkin_hz=25000000 earlyprintk=serial,uart1,57600 console=tty0 console=ttyBF1,57600 if

PID hash table entries: 256 (order: -2, 1024 bytes)

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 52500k/65536k RAM, (9380k init code, 1395k kernel code, 665k data, 1024k dma, 572k reserved)

Hierarchical RCU implementation.

NR_IRQS:159

Configuring Blackfin Priority Driven Interrupts

Console: colour dummy device 80x25

console [tty0] enabled

console [ttyBF1] enabled, bootconsole disabled

console [ttyBF1] enabled, bootconsole disabled

Calibrating delay loop... 1046.52 BogoMIPS (lpj=2093056)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (16 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (42 KB free)

NET: Registered protocol family 16

Blackfin DMA Controller

ezkit_init(): registering device resources

bio: create slab <bio-0> at 0

SCSI subsystem initialized

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@7

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

i2c-bfin-twi i2c-bfin-twi.0: Blackfin BF5xx on-chip I2C TWI Contoller, regs_base@ffc01400

musb_hdrc: version 6.0, pio, host, debug=0

musb_hdrc musb_hdrc.0: MUSB HDRC host driver

musb_hdrc musb_hdrc.0: new USB bus registered, assigned bus number 1

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

musb_hdrc musb_hdrc.0: USB Host mode controller at ffc03800 using PIO, IRQ 59

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

UDP hash table entries: 256 (order: 0, 4096 bytes)

UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)

NET: Registered protocol family 1

msgmni has been set to 102

io scheduler noop registered

io scheduler cfq registered (default)

dma_alloc_init: dma_page @ 0x02b36000 - 256 pages at 0x03f00000

Console: switching to colour frame buffer device 53x21

bfin-lq035q1 bfin-lq035q1: 320x240 16-bit RGB FrameBuffer initialized

bfin-otp: initialized

bfin-uart: Blackfin serial driver

bfin-uart.1: ttyBF1 at MMIO 0xffc02000 (irq = 31) is a BFIN-UART

brd: module loaded

adp5520 0-0032: failed writing 0x80 to 0x00

adp5520 0-0032: failed to write

adp5520: probe of 0-0032 failed with error -1

m25p80 spi0.1: m25p16 (2048 Kbytes)

Creating 2 MTD partitions on "m25p80":

0x000000000000-0x000000040000 : "bootloader(spi)"

0x000000040000-0x000000200000 : "linux kernel(spi)"

bfin_mii_bus: probed

bfin_mac: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:03, irq=-1, mdc_clk=2500000Hz(mdc_div=25)@sclk=131MHz)

bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1

Initializing USB Mass Storage driver...

usbcore: registered new interface driver usb-storage

USB Mass Storage support registered.

mice: PS/2 mouse device common for all mice

ad7879 0-002c: Failed to write AD7879 Touchscreen

ad7879: probe of 0-002c failed with error -1

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

usbcore: registered new interface driver usbhid

usbhid: USB HID core driver

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 2004-06-01 03:13:25 UTC (1086059605)

IP-Config: Complete:

     device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,

     host=bf527-ezkit, domain=, nis-domain=(none),

     bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=

Freeing unused kernel memory: 9380k freed

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            - http://blackfin.uclinux.org/

\    YP"    `| 8P  `.          - http://docs.blackfin.uclinux.org/

/     \.___.d|    .'           - http://www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    - http://www.analog.com/blackfin

 

Have a lot of fun...

 

 

BusyBox v1.16.2 (2010-08-12 19:02:19 CST) hush - the humble shell

 

root:/>

root:/> df_dok --noresults

 

   ~~~~~~~~~~~~~~~~~~~~~~~~~~| DirectFB 1.4.3 |~~~~~~~~~~~~~~~~~~~~~~~~~~

        (c) 2001-2009  The world wide DirectFB Open Source Community

        (c) 2000-2004  Convergence (integrated media) GmbH

      ----------------------------------------------------------------

 

(*) DirectFB/Core: Single Application Core. (2010-08-12 11:01)

(*) Direct/Thread: Started 'VT Switcher' (-1) [CRITICAL OTHER/OTHER 0/0] <12288>...

(*) Direct/Thread: Started 'VT Flusher' (-1) [DEFAULT OTHER/OTHER 0/0] <12288>...

(*) DirectFB/FBDev: Found 'bfin-lq035q1' (ID 0) with frame buffer at 0x03f00500, 151k (MMIO 0x00000000, 0k)

(*) Direct/Thread: Started 'PS/2 Input' (-1) [INPUT OTHER/OTHER 0/0] <12288>...

(*) DirectFB/Input: IMPS/2 Mouse 1.0 (directfb.org)

(*) Direct/Thread: Started 'Keyboard Input' (-1) [INPUT OTHER/OTHER 0/0] <12288>...

(*) DirectFB/Input: Keyboard 0.9 (directfb.org)

(*) DirectFB/Graphics: Generic Software Rasterizer 0.6 (directfb.org)

(*) DirectFB/Core/WM: Default 0.3 (directfb.org)

/home/test/work/cruise/checkouts/uclinux-dist/user/DirectFB-examples/DirectFB-examples-1.2.0/src/df_dok.c <1472>:

        (#) DirectFBError [dfb->CreateSurface( dfb, &dsc, &primary )]: Not supported!

(!!!)  *** WARNING [Application exited without deinitialization of DirectFB!] *** [/home/test/work/cruise/checkouts/uclinux-dis]

(!!!)  *** WARNING [still objects in 'Layer Context Pool'] *** [/home/test/work/cruise/checkouts/uclinux-dist/lib/DirectFB/Dire]

root:/>

--

 

Follow-ups

 

--- Michael Hennerich                                        2010-08-13 04:32:10

I checked a fix into trunk - can you try again?

 

Index: directfbrc

===================================================================

--- directfbrc  (revision 9715)

+++ directfbrc  (working copy)

@@ -1,3 +1,3 @@

mode=320x240

-depth=24

-pixelformat=RGB24

+depth=16

+pixelformat=RGB16

 

 

--- Vivi Li                                                  2010-08-20 03:22:15

OK now. Close it.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

config.linux.directfb    application/octet-stream    47064    Vivi Li

Attachments

Outcomes