FAQ:[#6178] rsh no longer works in trunk(2010)

Document created by Aaronwu Employee on Sep 11, 2013
Version 1Show Document
  • View in full screen mode

[#6178] rsh no longer works in trunk

Submitted By: Mike Frysinger

Open Date

2010-08-12 18:15:14     Close Date

2010-08-16 14:26:59

Priority:

Medium     Assignee:

Sonic Zhang

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2010R1     Release:

Category:

N/A     Board:

N/A

Processor:

ALL     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

trunk

App binary format:

N/A     

Summary: rsh no longer works in trunk

Details:

 

in 2009R1, using rsh from a board to another board worked.  i have one board at 192.168.0.15 and another one at 192.168.0.16 both running the same uImage.

 

from the .15 board:

root:/> rsh 192.168.0.16 ls

uclinux-config.gz

vendor-board-config.gz

 

however, booting up current trunk and doing the same thing ends up with rsh hanging and getting no output.  /var/log/messages on the other board shows that the server received the command just fine though ...

 

Follow-ups

 

--- Sonic Zhang                                              2010-08-16 06:25:45

Fixed. Vivi forgot the replace the rsh with a reimplementation in rsh-redone,

which can be built for uClinux without change.

 

Jie did it in old version of inetutils.

 

--- Mike Frysinger                                           2010-08-16 14:26:59

yep, trunk works fine for me, thanks

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes