FAQ: [#6168] kernel autoboot when i input "hciconfig hci0 up" in bluetooth cf testing(2010)

Document created by Aaronwu Employee on Sep 11, 2013
Version 1Show Document
  • View in full screen mode

[#6168] kernel autoboot when i input "hciconfig hci0 up" in bluetooth cf testing

Submitted By: angelia wu

Open Date

2010-08-09 02:27:49     Close Date

2010-08-18 22:46:13

Priority:

Medium     Assignee:

steven miao

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2010R1     Release:

Blackfin Linux:2010R1

Category:

N/A     Board:

STAMP

Processor:

BF537     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Duplicate

Uboot version or rev.:

    Toolchain version or rev.:

svn-4681

App binary format:

N/A     

Summary: kernel autoboot when i input "hciconfig hci0 up" in bluetooth cf testing

Details:

 

kernel autoboot when i input "hciconfig hci0 up" in bluetooth cf testing.it will show the following message.

 

U-Boot 2010.06-svn2366 (ADI-2010R1-pre) (Jul 27 2010 - 21:47:44)

 

CPU:   ADSP bf537-0.2 (Detected Rev: 0.2) (bypass boot)

Board: ADI BF537 stamp board

       Support: http://blackfin.uclinux.org/

Clock: VCO: 500 MHz, Core: 500 MHz, System: 125 MHz

RAM:   64 MiB

Flash: 4 MiB

In:    serial

Out:   serial

Err:   serial

KGDB:  [on serial] ready

Net:   bfin_mac

Hit any key to stop autoboot:  0

 

 

Besides,it can't autoboot successfully.only drag power line out ,it can autoboot successfully.

 

 

 

Follow-ups

 

--- steven miao                                              2010-08-18 21:39:22

We should drop the test case as well.

The reason is same as bug 6166.

 

--- Vivi Li                                                  2010-08-18 22:46:13

OK, this test is deleted from test list.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

config-config-blcf    application/octet-stream    49129    angelia wu

kernel-config-blcf    application/octet-stream    36941    angelia wu

Outcomes