FAQ: [#6019] Build default kernel fail at libpng-1.2.42 for zlib(2010)

Document created by Aaronwu Employee on Sep 10, 2013
Version 1Show Document
  • View in full screen mode

[#6019] Build default kernel fail at libpng-1.2.42 for zlib

Submitted By: Vivi Li

Open Date

2010-05-05 02:27:48     Close Date

2010-05-05 05:39:25

Priority:

Medium High     Assignee:

Vivi Li

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2010R1     Release:

Category:

Make Errors     Board:

N/A

Processor:

ALL     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.3-svn3815

App binary format:

N/A     

Summary: Build default kernel fail at libpng-1.2.42 for zlib

Details:

 

Build libpng-1.2.42 fail for zlib in latest trunk. Building log for libpng is attached.

 

First failed version:

--

kernel:    Linux release 2.6.33.3-ADI-2010R1-pre-svn8681, build #4 Fri Apr 30 05:30:51 CST 2010

toolchain: bfin-uclinux-gcc release gcc version 4.3.4 (ADI-trunk/svn-3815)

user-dist: release svn-9599, build #27 Fri Apr 30 05:29:41 CST 2010

--

 

Last passed version:

--

kernel:    Linux release 2.6.33.3-ADI-2010R1-pre-svn8668, build #44 Tue Apr 27 23:42:33 CST 2010

toolchain: bfin-uclinux-gcc release gcc version 4.3.4 (ADI-trunk/svn-3815)

user-dist: release svn-9593, build #880 Tue Apr 27 23:39:56 CST 2010

--

 

Bellow is the error log:

--

test@uclinux59-kernel-perf:~/work/cruise/checkouts/uclinux-dist> make lib/libpng_only

make[1]: Entering directory `/home/test/work/cruise/checkouts/uclinux-dist/lib'

touch libpng/.sgbuilt_lib && make -C libpng -j1

make[2]: Entering directory `/home/test/work/cruise/checkouts/uclinux-dist/lib/libpng'

set -e ; conf="$PWD/libpng-1.2.42/configure" ; chmod a+rx "$conf" ; find libpng-1.2.42 -type f -print0 | xargs -0 touch -r "$conf" ; rm -rf build-libpng-1.2.42 ; mkdir -p build-libpng-1.2.42 ; cd build-libpng-1.2.42 ; "$conf" --host=bfin-uclinux --build=i686-pc-linux-gnu --prefix=/usr --sysconfdir=/etc --datadir=/usr/share --mandir=/usr/share/man --infodir=/usr/share/info --localstatedir=/var/lib --disable-dependency-tracking --enable-fast-install

configure: loading site script /home/test/work/cruise/checkouts/uclinux-dist/vendors/config/config.site

config.site: loading extra site script frag /home/test/work/cruise/checkouts/uclinux-dist/vendors/config/config.site.build

config.site: loading site script frag /home/test/work/cruise/checkouts/uclinux-dist/vendors/config/bfin/config.site

config.site: loading site script frag /home/test/work/cruise/checkouts/uclinux-dist/vendors/config/bfin-unknown-uclinux

checking for a BSD-compatible install... (cached) /usr/bin/install -c

checking whether build environment is sane... yes

checking for bfin-uclinux-strip... (cached) bfin-uclinux-strip

checking for a thread-safe mkdir -p... (cached) /bin/mkdir -p

checking for gawk... (cached) gawk

checking whether make sets $(MAKE)... (cached) yes

checking whether to enable maintainer-specific portions of Makefiles... no

checking for bfin-uclinux-gcc... (cached) bfin-uclinux-gcc

checking whether the C compiler works... yes

checking for C compiler default output file name... a.out

checking for suffix of executables...

checking whether we are cross compiling... yes

checking for suffix of object files... (cached) o

checking whether we are using the GNU C compiler... (cached) yes

checking whether bfin-uclinux-gcc accepts -g... (cached) yes

checking for bfin-uclinux-gcc option to accept ISO C89... none needed

checking for style of include used by make... GNU

checking dependency style of bfin-uclinux-gcc... (cached) none

checking build system type... (cached) i686-pc-linux-gnu

checking host system type... (cached) bfin-unknown-uclinux

checking for a sed that does not truncate output... (cached) /usr/bin/sed

checking for grep that handles long lines and -e... (cached) /usr/bin/grep

checking for egrep... (cached) /usr/bin/grep -E

checking for fgrep... (cached) /usr/bin/grep -F

checking for ld used by bfin-uclinux-gcc... (cached) bfin-uclinux-ld

checking if the linker (bfin-uclinux-ld) is GNU ld... (cached) yes

checking how to run the C preprocessor... (cached) bfin-uclinux-gcc -E

checking for bfin-uclinux-sed... /usr/bin/sed

checking whether ln -s works... yes

checking whether make sets $(MAKE)... (cached) yes

checking for BSD- or MS-compatible name lister (nm)... (cached) bfin-uclinux-nm

checking the name lister (bfin-uclinux-nm) interface... (cached) BSD nm

checking the maximum length of command line arguments... 805306365

checking whether the shell understands some XSI constructs... yes

checking whether the shell understands "+="... yes

checking for bfin-uclinux-ld option to reload object files... (cached) -r

checking for bfin-uclinux-objdump... (cached) bfin-uclinux-objdump

checking how to recognize dependent libraries... unknown

checking for bfin-uclinux-ar... (cached) bfin-uclinux-ar

checking for bfin-uclinux-strip... (cached) bfin-uclinux-strip

checking for bfin-uclinux-ranlib... (cached) bfin-uclinux-ranlib

checking command to parse bfin-uclinux-nm output from bfin-uclinux-gcc object... ok

checking for ANSI C header files... yes

checking for sys/types.h... (cached) yes

checking for sys/stat.h... (cached) yes

checking for stdlib.h... (cached) yes

checking for string.h... (cached) yes

checking for memory.h... (cached) yes

checking for strings.h... (cached) yes

checking for inttypes.h... (cached) yes

checking for stdint.h... (cached) yes

checking for unistd.h... (cached) yes

checking for dlfcn.h... (cached) no

checking for objdir... (cached) .libs

checking if bfin-uclinux-gcc supports -fno-rtti -fno-exceptions... (cached) no

checking for bfin-uclinux-gcc option to produce PIC... -fPIC -DPIC

checking if bfin-uclinux-gcc PIC flag -fPIC -DPIC works... (cached) yes

checking if bfin-uclinux-gcc static flag -static works... (cached) yes

checking if bfin-uclinux-gcc supports -c -o file.o... (cached) yes

checking if bfin-uclinux-gcc supports -c -o file.o... (cached) yes

checking whether the bfin-uclinux-gcc linker (bfin-uclinux-ld) supports shared libraries... yes

checking whether -lc should be explicitly linked in... no

checking dynamic linker characteristics... no

checking how to hardcode library paths into programs... immediate

checking whether stripping libraries is possible... yes

checking if libtool supports shared libraries... no

checking whether to build shared libraries... no

checking whether to build static libraries... yes

checking for ANSI C header files... (cached) yes

checking for malloc.h... (cached) yes

checking for stdlib.h... (cached) yes

checking for string.h... (cached) yes

checking for strings.h... (cached) yes

checking for an ANSI C-conforming const... (cached) yes

checking for size_t... (cached) yes

checking whether struct tm is in sys/time.h or time.h... time.h

checking for working strtod... (cached) yes

checking for memset... (cached) yes

checking for pow... no

checking for pow in -lm... yes

checking for zlibVersion in -lz... no

configure: error: zlib not installed

make[2]: *** [build-libpng-1.2.42/Makefile] Error 1

make[2]: Leaving directory `/home/test/work/cruise/checkouts/uclinux-dist/lib/libpng'

make[1]: *** [libpng_only] Error 2

make[1]: Leaving directory `/home/test/work/cruise/checkouts/uclinux-dist/lib'

make: *** [lib/libpng_only] Error 2

--

 

Follow-ups

 

--- Mike Frysinger                                           2010-05-05 03:25:02

your log shows you forcing a build of libpng.  this ignores dependencies like

zlib.  so unless a `make lib_only` fails, what you're showing here is not a bug.

 

--- Vivi Li                                                  2010-05-05 03:50:44

Yes, it still fails. And all kernel regressions ceased because libpng is

selected by default config and it can not build now.

 

--- Mike Frysinger                                           2010-05-05 04:01:28

so post the full build log as an attachment as well as a directory listing of

the staging/usr/lib/ directory.  zlib nor libpng have changed in months.

 

--- Vivi Li                                                  2010-05-05 05:15:07

Files are attached.

 

--

test@uclinux50-bf537-ad9960-ad1836:..checkouts/uclinux-dist> ls

staging/usr/lib

alsa-lib               libfaad.a          liblzo2.so.2         libosip2.so.4  

        libpopt.so.0.0.0

ao                     libfaad.la         liblzo2.so.2.0.0   

libosip2.so.4.2.0        libreadline.a

libao.la               libFLAC.a          libmad.a             libosipparser2.a

        libreadline.so

libao.so               libFLAC++.a        libmad.la          

libosipparser2.so        libreadline.so.6

libao.so.2             libFLAC.la         libmediastreamer.a 

libosipparser2.so.4      libreadline.so.6.1

libao.so.2.1.3         libFLAC++.la       libmediastreamer.la

libosipparser2.so.4.2.0  libspeex.a

libasound.a            libform.a          libmenu.a            libpanel.a     

        libspeexdsp.a

libasound.la           libform_g.a        libmenu_g.a          libpanel_g.a   

        libspeexdsp.la

libasound.so           libform.so         libmenu.so           libpanel.so    

        libspeexdsp.so

libasound.so.2         libform.so.5       libmenu.so.5         libpanel.so.5  

        libspeexdsp.so.1

libasound.so.2.0.0     libform.so.5.7     libmenu.so.5.7       libpanel.so.5.7

        libspeexdsp.so.1.5.0

libaudiofile.a         libhistory.a       libmp4ff.a           libpng12.a     

        libspeex.la

libaudiofile.la        libhistory.so      libmp4ff.la          libpng12.la    

        libspeex.so

libbluetooth.a         libhistory.so.6    libncurses.a         libpng12.so    

        libspeex.so.1

libbluetooth.la        libhistory.so.6.1  libncurses++.a       libpng12.so.0  

        libspeex.so.1.5.0

libbluetooth.so        libjpeg.a          libncurses_g.a     

libpng12.so.0.42.0       libvorbisidec.a

libbluetooth.so.2      libjpeg.la         libncurses.so        libpng.a       

        libvorbisidec.la

libbluetooth.so.2.9.6  libjpeg.so         libncurses.so.5      libpng.la      

        libz.a

libcurses.a            libjpeg.so.7       libncurses.so.5.7    libpng.so      

        libz.so

libcurses.so           libjpeg.so.7.0.0   libopenobex.a        libpng.so.3    

        libz.so.1

libeXosip2.a           liblinphone.a      libopenobex.la       libpng.so.3.42.0

        libz.so.1.2.3

libeXosip2.la          liblinphone.la     libortp.a            libpopt.a      

        pkgconfig

libeXosip2.so          liblzo2.a          libortp.la           libpopt.la     

        terminfo

libeXosip2.so.4        liblzo2.la         libosip2.a           libpopt.so

libeXosip2.so.4.2.0    liblzo2.so         libosip2.so          libpopt.so.0

--

 

--- Mike Frysinger                                           2010-05-05 05:23:02

something is broken on your test system and it looks like the testing script

isnt catching these failures.  both things need to be fixed i guess.

 

rm -rf /home/test/work/cruise/checkouts/uclinux-dist/romfs/*

rm: cannot remove directory

`/home/test/work/cruise/checkouts/uclinux-dist/romfs/dev/pts': Permission

denied

rm: cannot remove

`/home/test/work/cruise/checkouts/uclinux-dist/romfs/dev/log': Permission

denied

make: *** [clean] Error 1

 

--- Vivi Li                                                  2010-05-05 05:37:26

Thanks for point it out.

I've fixed it in regression machine.

 

Close this bug.

 

--- Mike Frysinger                                           2010-05-05 05:47:04

doesnt the .exp script need fixing so that it aborts when `make clean` fails ?

 

--- Vivi Li                                                  2010-05-06 00:12:46

OK, test scripts are updated.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

config.log    application/octet-stream    183490    Vivi Li

config.policy    application/octet-stream    37405    Vivi Li

build_policy_kernel_log    application/octet-stream    935843    Vivi Li

Outcomes