[#5834] Build bf537-stamp mpu kernel for kernel xip test failed

Document created by Aaronwu Employee on Sep 5, 2013
Version 1Show Document
  • View in full screen mode

[#5834] Build bf537-stamp mpu kernel for kernel xip test failed

Submitted By: Vivi Li

Open Date

2010-01-19 01:48:21     Close Date

2010-02-21 22:10:22

Priority:

Medium     Assignee:

Barry Song

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2010R1     Release:

Category:

N/A     Board:

STAMP

Processor:

BF537     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.3_trunk3771

App binary format:

N/A     

Summary: Build bf537-stamp mpu kernel for kernel xip test failed

Details:

 

Build bf537-stamp mpu kernel for kernel xip test failed.

 

Config is attached.

--

  CC      init/version.o

  LD      init/built-in.o

  LD      .tmp_vmlinux1

arch/blackfin/mach-common/built-in.o: In function `ex_icplb_miss':

arch/blackfin/mach-common/entry.S:107: relocation truncated to fit: R_BFIN_PCREL24 against symbol `cplb_hdr' defined in .text section in arch/blackfin/kernel/cplb-mpu/built-in.o

make[1]: *** [.tmp_vmlinux1] Error 1

make[1]: Leaving directory `/home/test/work/cruise/checkouts/uclinux-dist/linux-2.6.x'

--

 

Follow-ups

 

--- Barry Song                                               2010-01-20 02:27:11

Fixed.

mpu kernel lost to handle CONFIG_EXCPT_IRQ_SYSC_L1 in cplb manager.

 

--- Vivi Li                                                  2010-02-21 22:09:34

OK. Close it.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

config.xip.fdpic    application/octet-stream    28963    Vivi Li

Attachments

Outcomes