[#5801] No interrupt occurs when reconnect gadget device in OTG mode.

Document created by Aaronwu Employee on Sep 5, 2013
Version 1Show Document
  • View in full screen mode

[#5801] No interrupt occurs when reconnect gadget device in OTG mode.

Submitted By: Cliff Cai

Open Date

2009-12-30 00:21:22     Close Date

2009-12-31 04:46:35

Priority:

Medium     Assignee:

Cliff Cai

Status:

Closed     Fixed In Release:

N/A

Found In Release:

snaps     Release:

trunk

Category:

N/A     Board:

EZKIT Lite

Processor:

BF527     Silicon Revision:

0.0

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

trunk

App binary format:

N/A     

Summary: No interrupt occurs when reconnect gadget device in OTG mode.

Details:

 

In peripheral mode,when reconnect the gadget device to PC,a connection interrupt is supposed to occur in PC's USB host contoller,then,PC will reset the gadget device so that the device can be put into use again. But  in OTG mode,it seems that no such interrupt occurs, and PC never resets gadget device.

 

Cliff

 

Follow-ups

 

--- Cliff Cai                                                2009-12-31 04:46:40

this bug was fixed with the latest check in for OTG.

 

Cliff

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes