[#5799] Build qt fails at debug-mmrs.c in latest trunk

Document created by Aaronwu Employee on Sep 5, 2013
Version 1Show Document
  • View in full screen mode

[#5799] Build qt fails at debug-mmrs.c in latest trunk

Submitted By: Vivi Li

Open Date

2009-12-29 05:25:43     Close Date

2009-12-29 11:25:36

Priority:

Medium     Assignee:

Nobody

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2010R1     Release:

Category:

Make Errors     Board:

N/A

Processor:

ALL     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Duplicate

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.3_trunk_svn3771

App binary format:

N/A     

Summary: Build qt fails at debug-mmrs.c in latest trunk

Details:

 

Build qt fails at debug-mmrs.c in latest trunk.

 

--

  LD      .tmp_vmlinux1^M

arch/blackfin/kernel/built-in.o: In function `bfin_debug_mmrs_exit':^M

arch/blackfin/kernel/debug-mmrs.c:28158: relocation truncated to fit: R_BFIN_PCREL24_JUMP_L against symbol `debugfs_remove_recursive' defined in .text section in fs/built-in.o^M

kernel/built-in.o: In function `ikconfig_cleanup':^M

kernel/configs.c:88: relocation truncated to fit: R_BFIN_PCREL24_JUMP_L against symbol `remove_proc_entry' defined in .text section in fs/built-in.o^M

fs/built-in.o: In function `exit_pipe_fs':^M

fs/pipe.c:1154: relocation truncated to fit: R_BFIN_PCREL24 against symbol `unregister_filesystem' defined in .text section in fs/built-in.o^M

fs/built-in.o: In function `mntput':^M

include/linux/mount.h:106: relocation truncated to fit: R_BFIN_PCREL24_JUMP_L against symbol `mntput_no_expire' defined in .text section in fs/built-in.o^M

fs/built-in.o: In function `exit_script_binfmt':^M

fs/binfmt_script.c:113: relocation truncated to fit: R_BFIN_PCREL24_JUMP_L against symbol `unregister_binfmt' defined in .text section in fs/built-in.o^M

fs/built-in.o: In function `exit_elf_fdpic_binfmt':^M

fs/binfmt_elf_fdpic.c:98: relocation truncated to fit: R_BFIN_PCREL24_JUMP_L against symbol `unregister_binfmt' defined in .text section in fs/built-in.o^M

fs/built-in.o: In function `exit_ramfs_fs':^M

fs/ramfs/inode.c:301: relocation truncated to fit: R_BFIN_PCREL24_JUMP_L against symbol `unregister_filesystem' defined in .text section in fs/built-in.o^M

fs/built-in.o: In function `debugfs_exit':^M

fs/debugfs/inode.c:553: relocation truncated to fit: R_BFIN_PCREL24 against symbol `simple_release_fs' defined in .text section in fs/built-in.o^M

fs/debugfs/inode.c:554: relocation truncated to fit: R_BFIN_PCREL24 against symbol `unregister_filesystem' defined in .text section in fs/built-in.o^M

fs/debugfs/inode.c:555: relocation truncated to fit: R_BFIN_PCREL24_JUMP_L against symbol `kobject_put' defined in .text section in lib/lib.a(kobject.o)^M

block/built-in.o: In function `noop_exit':^M

block/noop-iosched.c:111: additional relocation overflows omitted from the output^M

make[5]: *** [.tmp_vmlinux1] Error 1^M

make[5]: Leaving directory `/home/test/work/cruise/checkouts/uclinux-dist/linux-2.6.x'^M

make[4]: *** [image.uimage.initramfs.force] Error 2^M

--

 

Follow-ups

 

--- Mike Frysinger                                           2009-12-29 11:25:41

duplicate of [#5752]

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes