[#5711] gfortran case default_format_1.exe fails on 09r1 kernel but pass on trunk head

Document created by Aaronwu Employee on Sep 5, 2013
Version 1Show Document
  • View in full screen mode

[#5711] gfortran case default_format_1.exe fails on 09r1 kernel but pass on trunk head

Submitted By: Mingquan Pan

Open Date

2009-11-20 03:11:18     Close Date

2010-01-05 04:07:36

Priority:

Low     Assignee:

Nobody

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2009R1-RC6     Release:

Category:

N/A     Board:

N/A

Processor:

BF537     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Duplicate

Uboot version or rev.:

    Toolchain version or rev.:

4。3 toolchain

App binary format:

N/A     

Summary: gfortran case default_format_1.exe fails on 09r1 kernel but pass on trunk head

Details:

 

gfortran case default_format_1.exe fails on 09r1 kernel but pass on trunk head.

 

root:/> ./default_format_1.exe

Abort

root:/> echo $?

134

root:/> version

kernel:    Linux release 2.6.28.10-ADI-2009R1-svn7840, build #10 Fri Nov 20 08:02:51 CST 2009

toolchain: bfin-uclinux-gcc release gcc version 4.3.4 (ADI-trunk/svn-3736)

user-dist: release svn-9139, build #4 Fri Nov 20 07:59:31 CST 2009

root:/>

 

root:/> ./default_format_1.exe

ABRT

root:/> echo $?

0

root:/> version

kernel:    Linux release 2.6.31.6-ADI-2010R1-pre-svn7850, build #97 Fri Nov 20 14:35:36 GMT 2009

toolchain: bfin-uclinux-gcc release gcc version 4.3.4 (ADI-trunk/svn-3679)

user-dist: release svn-9165, build #2903 Fri Nov 20 14:34:55 GMT 2009

root:/>

root:/>

 

log is:

Executing on host: bfin-linux-uclibc-gfortran /home/test/work/cruise/checkouts/toolchain/gcc-4.3/gcc/testsuite/gfortran.dg/default_format_1.f90   -O0   -pedantic-errors    -lm  -mcpu=bf537-0.2 -o ./default_format_1.exe    (timeout = 300)

spawn bfin-linux-uclibc-gfortran /home/test/work/cruise/checkouts/toolchain/gcc-4.3/gcc/testsuite/gfortran.dg/default_format_1.f90 -O0 -pedantic-errors -lm -mcpu=bf537-0.2 -o ./default_format_1.exe^M

PASS: gfortran.dg/default_format_1.f90  -O0  (test for excess errors)

Executing on bfin-linux-uclibc: /tmp/default_format_1.exe.14578    (timeout = 300)

Executing on bfin-linux-uclibc: rm -f  /tmp/default_format_1.exe.14578    (timeout = 300)

Executed ./default_format_1.exe, status 1

Abort

FAIL: gfortran.dg/default_format_1.f90  -O0  execution test

 

Follow-ups

 

--- Sonic Zhang                                              2010-01-04 04:48:24

This is a duplicated bug of 5796.

 

--- Mingquan Pan                                             2010-01-05 04:07:35

This case fails now on trunk too after the ABRT return code issue is fixed. So

Close.

 

Executing on host: bfin-uclinux-gfortran

/home/test/work/cruise/checkouts/toolchain/gcc-4.3/gcc/testsuite/gfortran.dg/default_format_1.f90

  -O3 -fomit-frame-pointer   -pedantic-errors -Wl,-elf2flt=-s80000   -lm   -o

./default_format_1.exe    (timeout = 300)

spawn bfin-uclinux-gfortran

/home/test/work/cruise/checkouts/toolchain/gcc-4.3/gcc/testsuite/gfortran.dg/default_format_1.f90

-O3 -fomit-frame-pointer -pedantic-errors -Wl,-elf2flt=-s80000 -lm -o

./default_format_1.exe^M

PASS: gfortran.dg/default_format_1.f90  -O3 -fomit-frame-pointer  (test for

excess errors)

Executing on bfin-uclinux: /tmp/default_format_1.exe.13619    (timeout = 300)

Executing on bfin-uclinux: rm -f  /tmp/default_format_1.exe.13619    (timeout =

300)

Executed ./default_format_1.exe, status 1

ABRT

FAIL: gfortran.dg/default_format_1.f90  -O3 -fomit-frame-pointer  execution

test

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

default_format_1.exe    application/x-msdownload    16602    Mingquan Pan

Attachments

Outcomes