[#5705] build default kernel with fdpic app fails to boot up on bf533 stamp sometimes

Document created by Aaronwu Employee on Sep 5, 2013
Version 1Show Document
  • View in full screen mode

[#5705] build default kernel with fdpic app fails to boot up on bf533 stamp sometimes

Submitted By: Mingquan Pan

Open Date

2009-11-19 04:07:42     Close Date

2010-06-11 04:37:04

Priority:

Medium     Assignee:

Barry Song

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2010R1     Release:

Category:

N/A     Board:

N/A

Processor:

BF533     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Duplicate

Uboot version or rev.:

    Toolchain version or rev.:

4.3.4 (ADI-trunk/svn-3679)

App binary format:

N/A     

Summary: build default kernel with fdpic app fails to boot up on bf533 stamp sometimes

Details:

 

build default kernel with fdpic app fails to boot up on bf533 stamp sometimes. This is frequently seen after using 4.3 toolchain on regression machine from the begining of Nov.

 

bfin> bootm

## Booting kernel from Legacy Image at 01000000 ...

   Image Name:   bf533-2.6.31.6-ADI-2010R1-pre-sv

   Created:      2009-11-19  23:20:17 UTC

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    3505309 Bytes =  3.3 MB

   Load Address: 00001000

   Entry Point:  00186554

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 00186554

Linux version 2.6.31.6-ADI-2010R1-pre-svn7848 (test@uclinux76-bf533-stamp-elf) (gcc version 4.3.4 (ADI-trunk/svn-3679) ) #135 Thu Nov 19 16:20:03 MST 2009

register early platform devices

bootconsole [early_shadow0] enabled

bootconsole [early_BFuart0] enabled

early printk enabled on early_BFuart0

Limiting kernel memory to 56MB due to anomaly 05000263

Board Memory: 128MB

Kernel Managed Memory: 128MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x0010b760

  rodata    = 0x0010b760-0x0015dc8c

  bss       = 0x0015e000-0x0016e9f4

  data      = 0x0016e9f4-0x0017e000

    stack   = 0x0017c000-0x0017e000

  init      = 0x0017e000-0x006e3000

  available = 0x006e3000-0x037ff000

  DMA Zone  = 0x07f00000-0x08000000

Hardware Trace Active and Enabled

Boot Mode: 0

Reset caused by Software reset

Blackfin support (C) 2004-2009 Analog Devices, Inc.

Compiled for ADSP-BF533 Rev 0.3

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 497 MHz core clock and 82 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

  External memory: cacheable in instruction cache

Data Cache Enabled for CPU0

  External memory: cacheable (write-back) in data cache

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 14223

Kernel command line: root=/dev/mtdblock0 rw ip=10.100.4.50 earlyprintk=serial,uart0,57600 console=ttyBF0,57600

PID hash table entries: 256 (order: 8, 1024 bytes)

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 49720k/131072k RAM, (5524k init code, 1065k kernel code, 459k data, 1024k dma, 73280k reserved)

NR_IRQS:49

Configuring Blackfin Priority Driven Interrupts

console [ttyBF0] enabled, bootconsole disabled

console [ttyBF0] enabled, bootconsole disabled

Calibrating delay loop... 991.23 BogoMIPS (lpj=1982464)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (16 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 64 KB (52 KB free)

NET: Registered protocol family 16

Blackfin DMA Controller

stamp_init(): registering device resources

bio: create slab <bio-0> at 0

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

NET: Registered protocol family 1

msgmni has been set to 97

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

bfin-uart: Blackfin serial driver

bfin-uart.0: ttyBF0 at MMIO 0xffc00400 (irq = 21) is a BFIN-UART

brd: module loaded

smc91x.c: v1.1, sep 22 2004 by Nicolas Pitre <nico@cam.org>

eth0: SMC91C11xFD (rev 1) at 20300300 IRQ 40 [nowait]

eth0: Ethernet addr: 00:e0:22:fe:04:da

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@5

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 1970-01-01 00:02:02 UTC (122)

eth0: link down

IP-Config: Guessing netmask 255.0.0.0

IP-Config: Complete:

     device=eth0, addr=10.100.4.50, mask=255.0.0.0, gw=255.255.255.255,

     host=10.100.4.50, domain=, nis-domain=(none),

     bootserver=255.255.255.255, rootserver=255.255.255.255, rootpath=

Freeing unused kernel memory: 5524k freed

dma_alloc_init: dma_page @ 0x0205f000 - 256 pages at 0x07f00000

 

 

Last passed time: 2009_Nov_08_20_29, ucdist ver: 9127, kernel ver: 7765

 

Case 1 ...FAIL

 

 

Follow-ups

 

--- Barry Song                                               2009-12-14 22:49:41

Duplicate with [#5748] and [#5739]?

In fact, linux has startup normally, but UART dies, we can telnet the board and

check the interrupts:

root@roc-desktop:~/develop/svn/uclinux-dist# telnet 10.99.29.118

Trying 10.99.29.118...

Connected to 10.99.29.118.

Escape character is '^]'.

 

 

BusyBox v1.15.2 (2009-12-15 11:20:03 CST) hush - the humble shell

 

root:/> cat /proc/interrupts

  6:      88410      CORE  Blackfin CoreTimer

14:          1      INTN  rtc-bfin

21:          0      INTN  BFIN_UART_RX

22:       4537      INTN  BFIN_UART_TX

40:        283      GPIO  eth0

NMI:          0      CORE  Non Maskable Interrupt

Err:          0

 

BFIN_UART_RX is always 0 no matter how many bytes are inputed in console.

 

 

When disabling DMA mode for UART, all get normal:

IP-Config: Gateway not on directly connected network.

Freeing unused kernel memory: 5608k freed

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            - http://blackfin.uclinux.org/

\    YP"    `| 8P  `.          - http://deth0: link up, 100Mbps,

full-duplex, lpa 0x45E1

ocs.blackfin.uclinux.org/

/     \.___.d|    .'           - http://www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    - http://www.analog.com/blackfin

 

Have a lot of fun...

 

 

BusyBox v1.15.2 (2009-12-15 11:20:03 CST) hush - the humble shell

 

root:/> ls

bin   etc   init  mnt   root  sys   usr

dev   home  lib   proc  sbin  tmp   var

root:/> cat /proc/interrupts

  6:      15280      CORE  Blackfin CoreTimer

14:          1      INTN  rtc-bfin

21:         25      INTN  BFIN_UART_RX

22:       1549      INTN  BFIN_UART_TX

40:         11      GPIO  eth0

NMI:          0      CORE  Non Maskable Interrupt

Err:          0

 

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes