[#5665] Build kernel fails when adau1761 is built as module

Document created by Aaronwu Employee on Sep 5, 2013
Version 1Show Document
  • View in full screen mode

[#5665] Build kernel fails when adau1761 is built as module

Submitted By: Vivi Li

Open Date

2009-11-06 04:57:22     Close Date

2009-11-10 01:12:06

Priority:

Medium     Assignee:

Mike Frysinger

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2010R1     Release:

Category:

Make Errors     Board:

N/A

Processor:

ALL     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.3.4_svn3679

App binary format:

N/A     

Summary: Build kernel fails when adau1761 is built as module

Details:

 

Build kernel fails when adau1761 is built as module.

Config file is attached.

 

--

  SYSMAP  System.map^M

  SYSMAP  .tmp_System.map^M

  OBJCOPY arch/blackfin/boot/vmlinux.bin^M

  GZIP    arch/blackfin/boot/vmlinux.bin.gz^M

  UIMAGE  arch/blackfin/boot/vmImage.gz^M

Image Name:   bf537-2.6.31.5-ADI-2010R1-pre-sv^M

Created:      Fri Nov  6 11:09:26 2009^M

Image Type:   Blackfin Linux Kernel Image (gzip compressed)^M

Data Size:    986519 Bytes = 963.40 kB = 0.94 MB^M

Load Address: 00001000^M

Entry Point:  001b1784^M

  Building modules, stage 2.^M

  MODPOST 52 modules^M

ERROR: "process_sigma_firmware" [sound/soc/codecs/snd-soc-adau1761.ko] undefined!^M

make[2]: *** [__modpost] Error 1^M

make[1]: *** [modules] Error 2^M

make[1]: Leaving directory `/home/test/work/cruise/checkouts/uclinux-dist/linux-2.6.x'^M

make: *** [linux] Error 1^M

--

 

Follow-ups

 

--- Mike Frysinger                                           2009-11-06 06:26:56

should be fixed now by exporting the symbol

 

--- Vivi Li                                                  2009-11-08 23:08:15

Still fails with the same error info.

 

--- Mike Frysinger                                           2009-11-09 09:04:32

should be fixed now by having the codecs select the firmware driver

 

--- Vivi Li                                                  2009-11-10 01:12:06

OK now. Close it.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

config.power.audio_i2s    application/octet-stream    35175    Vivi Li

Outcomes