[#5650] Fail to open video device node of camera vs6624 on bf537-stamp

Document created by Aaronwu Employee on Sep 5, 2013
Version 1Show Document
  • View in full screen mode

[#5650] Fail to open video device node of camera vs6624 on bf537-stamp

Submitted By: Vivi Li

Open Date

2009-10-28 00:21:14     Close Date

2009-10-29 02:46:23

Priority:

Medium     Assignee:

Michael Hennerich

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2010R1     Release:

Category:

Tests     Board:

N/A

Processor:

BF537     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Assigned (Not Start)

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.1-09r1-rc9

App binary format:

N/A     

Summary: Fail to open video device node of camera vs6624 on bf537-stamp

Details:

 

Test with camera vs6624 on bf537-stamp failed while opening /dev/video0.

 

Last passed version:

--

kernel:    Linux release 2.6.31.4-ADI-2010R1-pre-svn7692, build #164 Thu Oct 22 03:19:37 GMT 2009

toolchain: bfin-linux-uclibc-gcc release gcc version 4.1.2 (ADI svn)

user-dist: release svn-9022, build #2381 Thu Oct 22 03:17:44 GMT 2009

--

 

--

Linux version 2.6.31.4-ADI-2010R1-pre-svn7704 (test@uclinux57-usb176x) (gcc version 4.1.2 (ADI svn)) #168 Sat Oct 24 07:35:59

register early platform devices

bootconsole [early_shadow0] enabled

bootconsole [early_BFuart0] enabled

early printk enabled on early_BFuart0

Limiting kernel memory to 56MB due to anomaly 05000263

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00100000-0x0020cbc0

  rodata    = 0x0020cbc0-0x00266e74

  bss       = 0x00267000-0x00277b3c

  data      = 0x00277b3c-0x0028a000

    stack   = 0x00288000-0x0028a000

  init      = 0x0028a000-0x00e00000

  available = 0x00e00000-0x037ff000

  DMA Zone  = 0x03e00000-0x04000000

Hardware Trace Active and Enabled

Boot Mode: 0

Reset caused by Software reset

Blackfin support (C) 2004-2009 Analog Devices, Inc.

Compiled for ADSP-BF537 Rev 0.2

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 500 MHz core clock and 125 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

  External memory: cacheable in instruction cache

Data Cache Enabled for CPU0

  External memory: cacheable (write-back) in data cache

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 14223

Kernel command line: root=/dev/mtdblock0 rw clkin_hz=25000000 earlyprintk=serial,uart0,57600 console=ttyBF0,57600 ip=10.100.f

PID hash table entries: 256 (order: 8, 1024 bytes)

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 42436k/65536k RAM, (11736k init code, 1074k kernel code, 502k data, 2048k dma, 7740k reserved)

NR_IRQS:98

Configuring Blackfin Priority Driven Interrupts

console [ttyBF0] enabled, bootconsole disabled

console [ttyBF0] enabled, bootconsole disabled

Calibrating delay loop... 997.37 BogoMIPS (lpj=1994752)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (16 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (36 KB free)

NET: Registered protocol family 16

Blackfin DMA Controller

stamp_init(): registering device resources

bio: create slab <bio-0> at 0

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

NET: Registered protocol family 1

msgmni has been set to 82

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

bfin-uart: Blackfin serial driver

bfin-uart.0: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART

brd: module loaded

bfin_mii_bus: probed

bfin_mac: attached PHY driver [SMSC LAN83C185] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=24)@sclk=125MHz)

bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@7

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

i2c-bfin-twi i2c-bfin-twi.0: Blackfin BF5xx on-chip I2C TWI Contoller, regs_base@ffc01400

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 2014-11-15 16:20:21 UTC (1416068421)

dma_alloc_init: dma_page @ 0x02999000 - 512 pages at 0x03e00000

IP-Config: Complete:

     device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,

     host=bf537-stamp, domain=, nis-domain=(none),

     bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=

Freeing unused kernel memory: 11736k freed

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            - http://blackfin.uclinux.org/

\    YP"    `| 8P  `.          - http://docs.blackfin.uclinux.org/

/     \.___.d|    .'           - http://www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    - http://www.analog.com/blackfin

 

Have a lot of fun...

 

 

BusyBox v1.15.2 (2009-10-24 07:32:58 GMT) hush - the humble shell

 

root:/>

root:/> modprobe videodev

Linux video capture interface: v2.00

root:/>

root:/> modprobe blackfin-cam

VS6624: Firmware Version 0.12

VS6624: Patch Version 0.0

VS6624: detected client on address 0x10

VS6624: V4L driver Blackfin CMOS Camera now ready

root:/>

root:/> ffmpeg -f video4linux -s 320x240 -i /dev/video0 -f mpegts udp:10.100.4.1

74:1234

FFmpeg version SVN-r9049, Copyright (c) 2000-2009 Fabrice Bellard, et al.

  built on Oct 24 2009 07:32:18 with gcc 4.1.2 (ADI svn)

  configuration: --prefix=/usr --source-path=/home/test/work/cruise/checkouts/uclinux-dist/lib/ffmpeg/build/../ffmpeg-svn-20-

  libavutil     50. 3. 0 / 50. 3. 0

  libavcodec    52.37. 0 / 52.37. 0

  libavformat   52.39. 2 / 52.39. 2

  libavdevice   52. 2. 0 / 52. 2. 0

  libswscale     0. 7. 1 /  0. 7. 1

  libpostproc   51. 2. 0 / 51. 2. 0

[video4linux @ 0x2068010]Wrong time base (0)

/dev/video0: Error while opening file

root:/> ls /dev/video0

/dev/video0

root:/>

--

 

Follow-ups

 

--- Michael Hennerich                                        2009-10-28 04:54:49

I think this is due to the recent ffmpeg update.

Try to add '-r 15/1'

 

ffmpeg -f video4linux -r 15/1 -s 320x240 -i /dev/video0 -f mpegts

 

-Michael

 

--- Vivi Li                                                  2009-10-29 02:46:23

I add "-r 20" and it works.

So close this bug.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

config.camera_vs6624    application/octet-stream    36831    Vivi Li

Attachments

Outcomes