[#5630] ethernet driver smc91x fail to wake up by uart in bf533-stamp

Document created by Aaronwu Employee on Sep 5, 2013
Version 1Show Document
  • View in full screen mode

[#5630] ethernet driver smc91x fail to wake up by uart in bf533-stamp

Submitted By: Vivi Li

Open Date

2009-10-19 23:19:30     Close Date

2009-10-20 23:28:45

Priority:

Medium     Assignee:

Michael Hennerich

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2010R1     Release:

Category:

N/A     Board:

STAMP

Processor:

BF533     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.1-09r1-rc9

App binary format:

N/A     

Summary: ethernet driver smc91x fail to wake up by uart in bf533-stamp

Details:

 

After wake up by uart in bf533-stamp, error message shows up in for smc91x.

BF533-EZKIT is OK.

 

--

Linux version 2.6.31.4-ADI-2010R1-pre-svn7669 (test@uclinux77-bf533-ad1836-spi) (gcc version 4.1.2 (ADI svn)) #84 Sun Oct 18 01:9

register early platform devices

bootconsole [early_shadow0] enabled

bootconsole [early_BFuart0] enabled

early printk enabled on early_BFuart0

Limiting kernel memory to 56MB due to anomaly 05000263

Board Memory: 128MB

Kernel Managed Memory: 128MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x0010b690

  rodata    = 0x0010b690-0x001623dc

  bss       = 0x00163000-0x001739bc

  data      = 0x001739bc-0x00184000

    stack   = 0x00182000-0x00184000

  init      = 0x00184000-0x007b3000

  available = 0x007b3000-0x037ff000

  DMA Zone  = 0x07f00000-0x08000000

Hardware Trace Active and Enabled

Boot Mode: 0

Blackfin support (C) 2004-2009 Analog Devices, Inc.

Compiled for ADSP-BF533 Rev 0.3

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 497 MHz core clock and 99 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

  External memory: cacheable in instruction cache

Data Cache Enabled for CPU0

  External memory: cacheable (write-back) in data cache

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 14223

Kernel command line: root=/dev/mtdblock0 rw clkin_hz=11059200 earlyprintk=serial,uart0,57600 ip=10.100.4.50:10.100.4.174:10.100.f

PID hash table entries: 256 (order: 8, 1024 bytes)

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 48888k/131072k RAM, (6332k init code, 1065k kernel code, 483k data, 1024k dma, 73280k reserved)

NR_IRQS:49

Configuring Blackfin Priority Driven Interrupts

bfin-rtc: invalid date; resetting

console [ttyBF0] enabled, bootconsole disabled

console [ttyBF0] enabled, bootconsole disabled

Calibrating delay loop... 991.23 BogoMIPS (lpj=1982464)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (16 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 64 KB (52 KB free)

NET: Registered protocol family 16

Blackfin DMA Controller

stamp_init(): registering device resources

bio: create slab <bio-0> at 0

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

NET: Registered protocol family 1

msgmni has been set to 95

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

bfin-uart: Blackfin serial driver

bfin-uart.0: ttyBF0 at MMIO 0xffc00400 (irq = 21) is a BFIN-UART

brd: module loaded

smc91x.c: v1.1, sep 22 2004 by Nicolas Pitre <nico@cam.org>

eth0: SMC91C11xFD (rev 1) at 20300300 IRQ 40 [nowait]

eth0: Ethernet addr: 00:e0:22:fe:45:76

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@5

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 1970-01-01 00:00:01 UTC (1)

eth0: link down

IP-Config: Complete:

     device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,

     host=bf533-stamp, domain=, nis-domain=(none),

     bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=

Freeing unused kernel memory: 6332k freed

eth0: link up, 100Mbps, full-duplex, lpa 0x41E1

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            - http://blackfin.uclinux.org/

\    YP"    `| 8P  `.          - http://docs.blackfin.uclinux.org/

/     \.___.d|    .'           - http://www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    - http://www.analog.com/blackfin

 

Have a lot of fun...

 

 

BusyBox v1.15.2 (2009-10-17 18:33:30 MDT) hush - the humble shell

 

root:/> echo enabled > /sys/class/tty/ttyBF0/power/wakeup

root:/> cat /sys/class/tty/ttyBF0/power/wakeup

enabled

root:/> echo standby > /sys/power/state

PM: Syncing filesystems ... done.

Freezing user space processes ... (elapsed 0.00 seconds) done.

Freezing remaining freezable tasks ... (elapsed 0.00 seconds) done.

Suspending console(s) (use no_console_suspend to debug)

eth0: link down

Restarting tasks ... done.

root:/>  eth0: timeout drivers/net/smc91x.c line 751

eth0: timeout drivers/net/smc91x.c line 755

eth0: timeout drivers/net/smc91x.c line 751

eth0: timeout drivers/net/smc91x.c line 755

eth0: timeout drivers/net/smc91x.c line 751

eth0: timeout drivers/net/smc91x.c line 755

eth0: timeout drivers/net/smc91x.c line 751

(same messages come out and can not stop...)

--

 

Follow-ups

 

--- Michael Hennerich                                        2009-10-20 08:33:58

This was a ******* to debug ...

 

On the BF533-STAMP board there is some external logic that switches the

Asynchronous Memory Bank 3 between Flash and SMSC91c111 Ethernet controller.

This logic is controlled by GPIO_PF0 which is also the same PIN as SPI-SPISS

Slave Mode Select. The SPI driver defaults the SPI Control register to Slave

Mode - but doesn't enable the SPI. In case the SPI bus driver wasn't utilized

and is then suspended and resumed during the PM state transitions - the SPI

resume code enables the SPI - and this will case the SPI-SPISS = GPIO_PF0 being

driven low. In return this causes the Flash being enabled and the smc91x

Ethernet driver accesses Flash instead of the Ethernet controller.

 

Fixed by defaulting SPI_CTL to Master Mode after SPI driver init.

Checked into trunk and 2009R1

 

-Michael

 

--- Vivi Li                                                  2009-10-20 23:28:45

OK now. Close it.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

config.linux.uart_wakeup    application/octet-stream    34091    Vivi Li

Attachments

Outcomes