[#5629] Coreb test failed due to kernel update

Document created by Aaronwu Employee on Sep 5, 2013
Version 1Show Document
  • View in full screen mode

[#5629] Coreb test failed due to kernel update

Submitted By: Vivi Li

Open Date

2009-10-19 07:02:44     Close Date

2009-10-20 06:12:22

Priority:

Medium     Assignee:

Nobody

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2010R1     Release:

Category:

N/A     Board:

N/A

Processor:

BF561     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Rejected

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.1-09r1-9

App binary format:

N/A     

Summary: Coreb test failed due to kernel update

Details:

 

Coreb test failed due to kernel update.

 

--

Linux version 2.6.31-ADI-2010R1-pre-svn7361 (test@uclinux66-561ezkit) (gcc version 4.1.2 (ADI svn)) #57 Thu Sep 17 23:42:59 CST 2009^M

bootconsole [early_shadow0] enabled^M

bootconsole [early_BFuart0] enabled^M

early printk enabled on early_BFuart0^M

Board Memory: 64MB^M

Kernel Managed Memory: 64MB^M

Memory map:^M

  fixedcode = 0x00000400-0x00000490^M

  text      = 0x00001000-0x000f8710^M

  rodata    = 0x000f8710-0x0014bb80^M

  bss       = 0x0014c000-0x0015cbd4^M

  data      = 0x0015cbd4-0x0016e000^M

    stack   = 0x0016c000-0x0016e000^M

  init      = 0x0016e000-0x00717000^M

  available = 0x00717000-0x03eff000^M

  DMA Zone  = 0x03f00000-0x04000000^M

Hardware Trace Active and Enabled^M

Boot Mode: 0^M

Reset caused by Software reset^M

Blackfin support (C) 2004-2009 Analog Devices, Inc.^M

Compiled for ADSP-BF561 Rev 0.5^M

Blackfin Linux support by http://blackfin.uclinux.org/^M

Processor Speed: 600 MHz core clock and 100 MHz System Clock^M

NOMPU: setting up cplb tables^M

Instruction Cache Enabled for CPU0^M

  External memory: cacheable in instruction cache^M

  L2 SRAM        : uncacheable in instruction cache^M

Data Cache Enabled for CPU0^M

  External memory: cacheable (write-back) in data cache^M

  L2 SRAM        : uncacheable in data cache^M

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 16001^M

Kernel command line: root=/dev/mtdblock0 rw earlyprintk=serial,uart0,57600 ip=10.100.4.50:10.100.4.174:10.100.4.174:255.255.255.0:bf561-ezkit:eth0:off^M

PID hash table entries: 256 (order: 8, 1024 bytes)^M

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)^M

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)^M

Memory available: 56680k/65536k RAM, (5796k init code, 989k kernel code, 471k data, 1024k dma, 572k reserved)^M

NR_IRQS:121^M

Configuring Blackfin Priority Driven Interrupts^M

console [ttyBF0] enabled, bootconsole disabled^M

console [ttyBF0] enabled, bootconsole disabled^M

Calibrating delay loop... 1196.03 BogoMIPS (lpj=2392064)^M

Security Framework initialized^M

Mount-cache hash table entries: 512^M

Blackfin Scratchpad data SRAM: 4 KB^M

Blackfin L1 Data A SRAM: 16 KB (16 KB free)^M

Blackfin L1 Data B SRAM: 16 KB (16 KB free)^M

Blackfin L1 Instruction SRAM: 16 KB (5 KB free)^M

Blackfin L2 SRAM: 128 KB (128 KB free)^M

NET: Registered protocol family 16^M

Blackfin DMA Controller^M

ezkit_init(): registering device resources^M

bio: create slab <bio-0> at 0^M

NET: Registered protocol family 2^M

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)^M

TCP established hash table entries: 2048 (order: 2, 16384 bytes)^M

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)^M

TCP: Hash tables configured (established 2048 bind 2048)^M

TCP reno registered^M

NET: Registered protocol family 1^M

msgmni has been set to 110^M

io scheduler noop registered^M

io scheduler anticipatory registered (default)^M

io scheduler cfq registered^M

Serial: Blackfin serial driver^M

bfin-uart.0: ttyBF0 at MMIO 0x0 (irq = 35) is a BFIN-UART^M

brd: module loaded^M

smc91x.c: v1.1, sep 22 2004 by Nicolas Pitre <nico@cam.org>^M

eth0: SMC91C11xFD (rev 1) at 2c010300 IRQ 82 [nowait]^M

eth0: Ethernet addr: 00:e0:22:fe:b1:3c^M

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@16^M

bfin-wdt: initialized: timeout=20 sec (nowayout=0)^M

TCP cubic registered^M

NET: Registered protocol family 17^M

eth0: link down^M

IP-Config: Complete:^M

     device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,^M

     host=bf561-ezkit, domain=, nis-domain=(none),^M

     bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=^M

Freeing unused kernel memory: 5796k freed^M

dma_alloc_init: dma_page @ 0x0275d000 - 256 pages at 0x03f00000^M

                           _____________________________________^M

        a8888b.           / Welcome to the uClinux distribution \^M

       d888888b.         /       _     _                         \^M

       eP"YPtY8h  0  :     l  i |n| k | | u  p  ,    _1  0_ 0TMM  b^M

p  s  ,8| ||f|8u  l__l_/-  d  u |p| l  e _x__, _   l \p\/a/    0  x^M

4  1  E8'1 ^M .88

      \        | |   | |  _ \| | | | \  /        |^M

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |^M

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |^M

     dP   .    Y8b.       \   For embedded processors including   |^M

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /^M

   d8"         'Y88b        \___________________________________/^M

  :8P    '      :888^M

   8a.   :     _a88P         For further information, check out:^M

._/"Yaa_:   .| 88P|            - http://blackfin.uclinux.org/^M

\    YP"    `| 8P  `.          - http://docs.blackfin.uclinux.org/^M

/     \.___.d|    .'           - http://www.uclinux.org/^M

`--..__)8888P`._.'  jgs/a:f    - http://www.analog.com/blackfin^M

^M

Have a lot of fun...^M

^M

^M

BusyBox v1.15.1 (2009-09-17 23:40:00 CST) hush - the humble shell^M

^M

root:/> version^M

kernel:    Linux release 2.6.31-ADI-2010R1-pre-svn7361, build #57 Thu Sep 17 23:42:59 CST 2009^M

toolchain: bfin-uclinux-gcc release gcc version 4.1.2 (ADI svn)^M

user-dist: release svn-8866, build #412 Thu Sep 17 23:42:04 CST 2009^M

root:/> successful boot attempt

************** STEP 3: Start testing: test_cpp

 

modprobe dualcore_test^M

dualcore_test: version magic '2.6.31-ADI-2010R1-pre-svn7361 preempt mod_unload ' should be '2.6.31-ADI-2010R1-pre-svn7361 mod_unload '^M

modprobe: failed to load module dualcore_test (coreb/dualcore_test.ko): invalid module format^M

root:/>

--

 

Last passed version:

--

root:/> version^M

kernel:    Linux release 2.6.31-ADI-2010R1-pre-svn7337, build #51 Wed Sep 16 18:07:23 CST 2009^M

toolchain: bfin-uclinux-gcc release gcc version 4.1.2 (ADI svn)^M

user-dist: release svn-8859, build #352 Wed Sep 16 18:06:28 CST 2009^M

--

 

Follow-ups

 

--- Mike Frysinger                                           2009-10-19 15:15:18

version magic mismatch means you need to rebuild the module against your kernel

 

--- Vivi Li                                                  2009-10-20 06:12:22

I cleaned all source and build a new kernel. It works now. Close it.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

config.coreb    application/octet-stream    29059    Vivi Li

Attachments

Outcomes