[#5619] isp1760 module doesn't work on latest trunk

Document created by Aaronwu Employee on Sep 5, 2013
Version 1Show Document
  • View in full screen mode

[#5619] isp1760 module doesn't work on latest trunk

Submitted By: Vivi Li

Open Date

2009-10-15 05:36:11     Close Date

2009-10-20 03:32:12

Priority:

Medium     Assignee:

Michael Hennerich

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2010R1     Release:

Category:

Drivers     Board:

N/A

Processor:

BF537     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.1-09r1-rc9

App binary format:

N/A     

Summary: isp1760 module doesn't work on latest trunk

Details:

 

isp1760 module doesn't work on latest trunk.

 

Config is attached. Bellow is the log:

--

Linux version 2.6.31.3-ADI-2010R1-pre-svn7608 (test@uclinux57-usb176x) (gcc version 4.1.2 (ADI svn)) #150 Wed Oct 14 18:44:25 GM9

register early platform devices

bootconsole [early_shadow0] enabled

bootconsole [early_BFuart0] enabled

early printk enabled on early_BFuart0

Limiting kernel memory to 56MB due to anomaly 05000263

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x0013d6a0

  rodata    = 0x0013d6a0-0x001aab00

  bss       = 0x001ab000-0x001bc2dc

  data      = 0x001bc2dc-0x001d0000

    stack   = 0x001ce000-0x001d0000

  init      = 0x001d0000-0x00950000

  available = 0x00950000-0x037ff000

  DMA Zone  = 0x03f00000-0x04000000

Hardware Trace Active and Enabled

Boot Mode: 0

Reset caused by Software reset

Blackfin support (C) 2004-2009 Analog Devices, Inc.

Compiled for ADSP-BF537 Rev 0.2

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 500 MHz core clock and 125 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

  External memory: cacheable in instruction cache

Data Cache Enabled for CPU0

  External memory: cacheable (write-back) in data cache

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 14223

Kernel command line: root=/dev/mtdblock0 rw clkin_hz=25000000 earlyprintk=serial,uart0,57600 console=ttyBF0,57600 ip=10.100.4.50f

PID hash table entries: 256 (order: 8, 1024 bytes)

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 47236k/65536k RAM, (7680k init code, 1265k kernel code, 587k data, 1024k dma, 7744k reserved)

NR_IRQS:98

Configuring Blackfin Priority Driven Interrupts

bfin-rtc: invalid date; resetting

console [ttyBF0] enabled, bootconsole disabled

console [ttyBF0] enabled, bootconsole disabled

Calibrating delay loop... 997.37 BogoMIPS (lpj=1994752)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (16 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (36 KB free)

NET: Registered protocol family 16

Blackfin DMA Controller

stamp_init(): registering device resources

bio: create slab <bio-0> at 0

SCSI subsystem initialized

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

NET: Registered protocol family 1

msgmni has been set to 92

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

bfin-uart: Blackfin serial driver

bfin-uart.0: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART

brd: module loaded

bfin_mii_bus: probed

bfin_mac: attached PHY driver [SMSC LAN83C185] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=24)@sclk=125MHz)

bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@7

Initializing USB Mass Storage driver...

usbcore: registered new interface driver usb-storage

USB Mass Storage support registered.

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

usbcore: registered new interface driver usbhid

usbhid: v2.6:USB HID core driver

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 1970-01-01 00:00:01 UTC (1)

IP-Config: Complete:

     device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,

     host=bf537-stamp, domain=, nis-domain=(none),

     bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=

Freeing unused kernel memory: 7680k freed

dma_alloc_init: dma_page @ 0x0207d000 - 256 pages at 0x03f00000

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            - http://blackfin.uclinux.org/

\    YP"    `| 8P  `.          - http://docs.blackfin.uclinux.org/

/     \.___.d|    .'           - http://www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    - http://www.analog.com/blackfin

 

Have a lot of fun...

 

 

BusyBox v1.15.2 (2009-10-14 18:03:41 GMT) hush - the humble shell

 

root:/> PHY: 0:01 - Link is Up - 100/Full

 

root:/> modprobe isp1760

root:/> lsmod

Module                  Size  Used by

isp1760                14500  0

root:/> ls dev/

console             ptmx                ram2                stderr

cpu_dma_latency     pts                 ram3                stdin

fd                  ram0                ram4                stdout

full                ram1                ram5                tty

kmsg                ram10               ram6                ttyBF0

log                 ram11               ram7                urandom

mem                 ram12               ram8                usbmon0

network_latency     ram13               ram9                watchdog

network_throughput  ram14               random              zero

null                ram15               rtc0

root:/>

--

 

Follow-ups

 

--- Michael Hennerich                                        2009-10-15 06:38:33

struct platform_device .name changed from isp1760-hcd to isp1760 

 

fixed on trunk

-Michael

 

 

root:/> modprobe isp1760

isp1760 isp1760.0: NXP ISP1760 USB Host Controller

isp1760 isp1760.0: new USB bus registered, assigned bus number 1

isp1760 isp1760.0: bus width: 16, oc: digital

isp1760 isp1760.0: irq 57, io mem 0x203c0000

isp1760 isp1760.0: USB ISP 1761 HW rev. 1 started

usb usb1: New USB device found, idVendor=1d6b, idProduct=0002

usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1

usb usb1: Product: NXP ISP1760 USB Host Controller

usb usb1: Manufacturer: Linux 2.6.31.4-ADI-2010R1-pre-svn7653 isp1760-hcd

usb usb1: SerialNumber: isp1760.0

usb usb1: configuration #1 chosen from 1 choice

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

ISP1760 USB device initialised

root:/> port 1 high speed

usb 1-1: new high speed USB device using isp1760 and address 2

port 1 high speed

usb 1-1: New USB device found, idVendor=0471, idProduct=3526

usb 1-1: New USB device strings: Mfr=1, Product=2, SerialNumber=0

usb 1-1: Product: ISP1520

usb 1-1: Manufacturer: Philips Semiconductors

usb 1-1: configuration #1 chosen from 1 choice

hub 1-1:1.0: USB hub found

hub 1-1:1.0: 3 ports detected

 

root:/> usb 1-1.3: new high speed USB device using isp1760 and address 3

usb 1-1.3: New USB device found, idVendor=0781, idProduct=5406

usb 1-1.3: New USB device strings: Mfr=1, Product=2, SerialNumber=3

usb 1-1.3: Product: U3 Cruzer Micro

usb 1-1.3: Manufacturer: SanDisk Corporation

usb 1-1.3: SerialNumber: 0000162443743A6D

usb 1-1.3: configuration #1 chosen from 1 choice

 

root:/> version

kernel:    Linux release 2.6.31.4-ADI-2010R1-pre-svn7653, build #3160 Thu Oct

15 12:34:11 CEST 2009

toolchain: bfin-uclinux-gcc release gcc version 4.1.2 (ADI svn)

user-dist: release svn-8937, build #3688 Thu Oct 15 12:33:38 CEST 2009

root:/>

 

--- Vivi Li                                                  2009-10-20 03:32:12

OK now. Close it.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

config.linux.usbhost_176x    application/octet-stream    40660    Vivi Li

Outcomes