[#5596] Fail to boot up 561 SMP kernel for latest regression

Document created by Aaronwu Employee on Sep 5, 2013
Version 1Show Document
  • View in full screen mode

[#5596] Fail to boot up 561 SMP kernel for latest regression

Submitted By: Vivi Li

Open Date

2009-10-12 02:20:01     Close Date

2009-10-19 07:04:01

Priority:

Medium     Assignee:

Graf Yang

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2010R1     Release:

Category:

N/A     Board:

N/A

Processor:

BF561     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Out of Date

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.1-09r1-rc9

App binary format:

N/A     

Summary: Fail to boot up 561 SMP kernel for latest regression

Details:

 

Fail to boot up 561 SMP kernel for latest regression.

 

--

U-Boot 2008.10 (ADI-2009R1-rc3) (Jul 16 2009 - 18:03:27)

 

CPU:   ADSP bf561-0.3 (Detected Rev: 0.5) (bypass boot)

Board: ADI BF561 EZ-Kit Lite board

       Support: http://blackfin.uclinux.org/

Clock: VCO: 600 MHz, Core: 600 MHz, System: 100 MHz

RAM:   64 MB

Flash:  8 MB

In:    serial

Out:   serial

Err:   serial

Net:   MAC:   00:E0:22:FE:BA:2A

Hit any key to stop autoboot:  0

bfin>

bfin> run ramboot

Using MAC Address 00:E0:22:FE:BA:2A

TFTP from server 10.100.4.174; our IP address is 10.100.4.50

Filename 'uImage'.

Load address: 0x1000000

Loading: #################################################################

         #################################################################

         #################################################################

         #################################################################

         ##

done

Bytes transferred = 3844112 (3aa810 hex)

## Booting kernel from Legacy Image at 01000000 ...

   Image Name:   bf561-2.6.31.3-ADI-2010R1-pre-sv

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    3844048 Bytes =  3.7 MB

   Load Address: 00001000

   Entry Point:  0018eb84

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 0018eb84

Linux version 2.6.31.3-ADI-2010R1-pre-svn7580 (test@uclinux65-561-SMP) (gcc version 4.1.2 (ADI svn)) #66 SMP Mon Oct 12 00:49:089

register early platform devices

bootconsole [early_shadow0] enabled

bootconsole [early_BFuart0] enabled

early printk enabled on early_BFuart0

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x0010ae40

  rodata    = 0x0010ae40-0x00160e5c

  bss       = 0x00161000-0x00173428

  data      = 0x00173440-0x00184000

    stack   = 0x00182000-0x00184000

  init      = 0x00184000-0x0073a000

  available = 0x0073a000-0x03eff000

  DMA Zone  = 0x03f00000-0x04000000

Hardware Trace Active and Enabled

Boot Mode: 0

Reset caused by Software reset

Blackfin support (C) 2004-2009 Analog Devices, Inc.

Compiled for ADSP-BF561 Rev 0.5

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 600 MHz core clock and 100 MHz System Clock

NOMPU: setting up cplb tables

NOMPU: setting up cplb tables

--

 

Follow-ups

 

--- Vivi Li                                                  2009-10-19 07:04:01

It can boot now. Out of date. Close it.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes