[#5595] Run earlyprintk test on bf538-ezkit, kernel fails to boot up

Document created by Aaronwu Employee on Sep 5, 2013
Version 1Show Document
  • View in full screen mode

[#5595] Run earlyprintk test on bf538-ezkit, kernel fails to boot up

Submitted By: Vivi Li

Open Date

2009-10-10 06:36:53     Close Date

2009-10-15 03:48:10

Priority:

Medium     Assignee:

Sonic Zhang

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2010R1     Release:

Category:

N/A     Board:

N/A

Processor:

BF538     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.1-09r1-rc9

App binary format:

N/A     

Summary: Run earlyprintk test on bf538-ezkit, kernel fails to boot up

Details:

 

Run earlyprintk test on bf538-ezkit, kernel fails to boot up.

 

--

U-Boot 2008.10 (ADI-2009R1-rc3) (Jul 16 2009 - 18:01:55)

 

CPU:   ADSP bf538-0.4 (Detected Rev: 0.4) (bypass boot)

Board: ADI BF538F EZ-Kit Lite board

       Support: http://blackfin.uclinux.org/

Clock: VCO: 525 MHz, Core: 525 MHz, System: 131.250 MHz

RAM:   64 MB

Flash:  4 MB

In:    serial

Out:   serial

Err:   serial

Net:   MAC:   00:E0:22:FE:BC:8B

Hit any key to stop autoboot:  0

bfin> run ramboot

Using MAC Address 00:E0:22:FE:BC:8B

TFTP from server 10.100.4.174; our IP address is 10.100.4.50

Filename 'uImage'.

Load address: 0x1000000

Loading: #################################################################

         #################################################################

         #################################################################

         ########################################################

done

Bytes transferred = 3683993 (383699 hex)

## Booting kernel from Legacy Image at 01000000 ...

   Image Name:   bf538-2.6.31.1-ADI-2010R1-pre-sv

   Created:      2009-09-29  14:23:20 UTC

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    3683929 Bytes =  3.5 MB

   Load Address: 00001000

   Entry Point:  001920f0

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 001920f0

--

 

Follow-ups

 

--- Mike Frysinger                                           2009-10-10 11:46:39

command line processing of serial console has changed.  you probably need to

update all of your boards to u-boot trunk if you want to boot linux trunk.

 

--- Vivi Li                                                  2009-10-12 02:01:33

It still fails after u-boot is updated.

 

--

U-Boot 2009.08-svn2043 (ADI-2009R2-pre) (Oct 12 2009 - 12:57:54)

 

CPU:   ADSP bf538-0.4 (Detected Rev: 0.4) (bypass boot)

Board: ADI BF538F EZ-Kit Lite board

       Support: http://blackfin.uclinux.org/

Clock: VCO: 525 MHz, Core: 525 MHz, System: 131.250 MHz

RAM:   64 MB

Flash:  4 MB

In:    serial

Out:   serial

Err:   serial

Net:   SMC91111-0

MAC:   00:e0:22:fe:bc:8b

Hit any key to stop autoboot:  0

bfin>

bfin> run ramboot

SMC91111: MAC 00:e0:22:fe:bc:8b

Using SMC91111-0 device

TFTP from server 10.100.4.174; our IP address is 10.100.4.50

Filename 'uImage'.

Load address: 0x1000000

Loading: #################################################################

         #################################################################

         #################################################################

         ########################################################

done

Bytes transferred = 3684312 (3837d8 hex)

## Booting kernel from Legacy Image at 01000000 ...

   Image Name:   bf538-2.6.31.3-ADI-2010R1-pre-sv

   Created:      2009-10-11   3:11:06 UTC

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    3684248 Bytes =  3.5 MB

   Load Address: 00001000

   Entry Point:  001920d8

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 001920d8

--

 

--- Sonic Zhang                                              2009-10-13 05:05:12

Fixed

 

In order to probe early resource of a specified port, port id should be

included in the port name string when registering.

 

--- Vivi Li                                                  2009-10-15 03:48:10

OK now. Close it.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes