[#5581] trunk head build fails for get_fb_unmapped_area undefined when framebuffer is built as a module

Document created by Aaronwu Employee on Sep 5, 2013
Version 1Show Document
  • View in full screen mode

[#5581] trunk head build fails for get_fb_unmapped_area undefined when framebuffer is built as a module

Submitted By: Mingquan Pan

Open Date

2009-09-29 23:36:45     Close Date

2009-09-30 01:33:18

Priority:

Medium     Assignee:

Michael Hennerich

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2010R1     Release:

Category:

N/A     Board:

N/A

Processor:

BF537     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

09r1-rc9

App binary format:

N/A     

Summary: trunk head build fails for get_fb_unmapped_area undefined when framebuffer is built as a module

Details:

 

trunk head build fails for get_fb_unmapped_area undefined  on bf537 stamp now.

 

LD      .tmp_vmlinux1^M

  KSYM    .tmp_kallsyms1.S^M

  AS      .tmp_kallsyms1.o^M

  LD      .tmp_vmlinux2^M

  KSYM    .tmp_kallsyms2.S^M

  AS      .tmp_kallsyms2.o^M

  LD      vmlinux^M

  SYSMAP  System.map^M

  SYSMAP  .tmp_System.map^M

  OBJCOPY arch/blackfin/boot/vmlinux.bin^M

  GZIP    arch/blackfin/boot/vmlinux.bin.gz^M

  Building modules, stage 2.^M

  MODPOST 59 modules^M

ERROR: "get_fb_unmapped_area" [drivers/video/fb.ko] undefined!^M

make[2]: *** [__modpost] Error 1^M

make[1]: *** [modules] Error 2^M

make[1]: *** Waiting for unfinished jobs....^M

  UIMAGE  arch/blackfin/boot/vmImage.gz^M

Image Name:   bf537-2.6.31.1-ADI-2010R1-pre-sv^M

Created:      Wed Sep 30 09:36:38 2009^M

Image Type:   Blackfin Linux Kernel Image (gzip compressed)^M

Data Size:    904678 Bytes = 883.47 kB = 0.86 MB^M

Load Address: 0x00001000^M

Entry Point:  0x00191874^M

make[1]: Leaving directory `/home/test/work/cruise/checkouts/uclinux-dist/linux-2.6.x'^M

 

Follow-ups

 

--- Mike Frysinger                                           2009-09-29 23:59:47

should be fixed now

 

--- Mingquan Pan                                             2009-09-30 01:33:18

Yes,close.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes