[#5568] Framebuffer DMA Error!!

Document created by Aaronwu Employee on Sep 4, 2013
Version 1Show Document
  • View in full screen mode

[#5568] Framebuffer DMA Error!!

Submitted By: land land

Open Date

2009-09-28 01:18:46     Close Date

2009-09-28 17:33:04

Priority:

High     Assignee:

Nobody

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2007R1.1-RC3     Release:

uClinux-dist-2007R1.1-RC3

Category:

Make Errors     Board:

N/A

Processor:

BF561     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Rejected

Uboot version or rev.:

    Toolchain version or rev.:

blackfin-toolchain-07r1.1-3.i3

App binary format:

N/A     

Summary: Framebuffer DMA Error!!

Details:

 

when make the image of  uClinux-dist-2007R1.1-RC3.tar.bz2 with blackfin-toolchain-07r1.1-3.i386.rpm

 

when i chose the Framebuffer DMA BitBlit / Fill Rect Support (BF5xx_FBDMA) [N/m/y?] (NEW) Y

 

then there are the errors :drivers/built-in.o: In function `Enable_MemDMA1':

(.text+0x11168): undefined reference to `bfin_write_MDMA_D1_START_ADDR'

drivers/built-in.o: In function `Enable_MemDMA1':

(.text+0x1116e): undefined reference to `bfin_write_MDMA_D1_X_COUNT'

drivers/built-in.o: In function `Enable_MemDMA1':

(.text+0x11174): undefined reference to `bfin_write_MDMA_D1_X_MODIFY'

drivers/built-in.o: In function `Enable_MemDMA1':

(.text+0x1117a): undefined reference to `bfin_write_MDMA_D1_Y_COUNT'

 

i only find the definition of   bfin_write_MDMA_D0_X_MODIFY' in /linux-2.6.x/include/asm-blackfin/mach-bf561/cdefBF561.h,but not the ....D1_X_MODIFY' ??

 

HELP ME PLEASE!!!!!!!

 

Follow-ups

 

--- land land                                                2009-09-28 01:37:23

have to use this version, because i have changed some code to fit my own board.

 

so can you tell me how to fix this problem ,please give the details!!

 

if you can, please send me email to iamweeland@gmail.com!!

thanks a lot!!!

 

--- Sonic Zhang                                              2009-09-28 06:07:56

Already fixed. See reply on help forum.

 

--- Mike Frysinger                                           2009-09-28 17:33:04

do not spam our website with the same issue over and over.  doing so will get

you ignored and possibly banned.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes