[#5563] Some ltp test case will get warning of "Directory not empty"

Document created by Aaronwu Employee on Sep 4, 2013
Version 1Show Document
  • View in full screen mode

[#5563] Some ltp test case will get warning of "Directory not empty"

Submitted By: Vivi Li

Open Date

2009-09-27 04:00:41     Close Date

2009-10-28 22:34:09

Priority:

Medium     Assignee:

Graf Yang

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2010R1     Release:

Category:

Kernel Functions     Board:

N/A

Processor:

ALL     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Out of Date

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.1-09r1-rc9

App binary format:

N/A     

Summary: Some ltp test case will get warning of "Directory not empty"

Details:

 

Some ltp test case will get warning of "Directory not empty".

 

--

root:/> access04

access04    1  PASS  : Functionality of access(testdir/testfile, F_OK) successful

access04    0  WARN  :  tst_rmdir(): rmobj(/tmp/acc7FGefe) failed: rmdir(/tmp/acc7FGefe) failed; errno=39: Directory not empty

root:/>

--

 

Following test case will get the same warning:

access04, access05, chmod03, chmod04, fchmod03, fchmod04, fstat02, fstat04, lstat02, lstat03, mknod07, open08, readlink01, readlink03, stat01, stat02, stat03, symlink03, truncate03, truncate04, utime02, utime05.

 

Follow-ups

 

--- Graf Yang                                                2009-10-28 06:15:02

These warning disappeared when test using the latest code.

 

root:/ltp-emptydir> ./access04

access04    1  PASS  :  Functionality of access(testdir/testfile, F_OK)

successful

root:/ltp-emptydir> version

kernel:    Linux release 2.6.31.5-ADI-2010R1-pre-svn7722, build #10 Wed Oct 28

18:02:03 CST 2009

toolchain: bfin-uclinux-gcc release gcc version 4.1.2 (ADI svn)

user-dist: release svn-9061, build #1 Wed Oct 28 17:23:32 CST 2009

 

 

The old code do have this issue,

root:/ltp-emptydir> ./access04

access04    1  PASS  :  Functionality of access(testdir/testfile, F_OK)

successful

access04    0  WARN  :  tst_rmdir(): rmobj(/tmp/acc5VEid3) failed:

rmdir(/tmp/acc5VEid3) failed; errno=39: Directory not ey

root:/ltp-emptydir> version

kernel:    Linux release 2.6.30.5-ADI-2010R1-pre-svn7215, build #32 Wed Oct 28

16:03:10 CST 2009

toolchain: bfin-uclinux-gcc release gcc version 4.1.2 (ADI svn)

user-dist: release svn-8742, build #6 Wed Oct 28 12:32:48 CST 2009

 

--- Vivi Li                                                  2009-10-28 22:34:09

Yes, it's ok now.

So close it.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes