[#5536] sl811 and isp1362 don't work on bf533-ezkit

Document created by Aaronwu Employee on Sep 4, 2013
Version 1Show Document
  • View in full screen mode

[#5536] sl811 and isp1362 don't work on bf533-ezkit

Submitted By: Vivi Li

Open Date

2009-09-14 23:17:06     Close Date

2009-11-15 22:45:52

Priority:

Medium     Assignee:

Michael Hennerich

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2009R1-RC6     Release:

Category:

N/A     Board:

N/A

Processor:

BF533     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Rejected

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.1-09r1-rc9

App binary format:

N/A     

Summary: sl811 and isp1362 don't work on bf533-ezkit

Details:

 

sl811 and isp1362 don't work on bf533-ezkit. Config file is attached.

 

--

U-Boot 2008.10-svn1556 (ADI-2009R1-pre) (Dec 29 2008 - 14:51:27)

 

CPU:   ADSP bf533-0.3 (Detected Rev: 0.3)

Board: ADI BF533 EZ-Kit Lite board

       Support: http://blackfin.uclinux.org/

Clock: VCO: 594 MHz, Core: 594 MHz, System: 118.800 MHz

RAM:   32 MB

Flash:  2.1 MB

In:    serial

Out:   serial

Err:   serial

Net:   MAC:   00:E0:22:FE:BA:25

Hit any key to stop autoboot:  0

bfin> help loady

loady [ off ] [ baud ]

    - load binary file over serial line with offset 'off' and baudrate 'baud'

 

bfin> loady 0x1000000 115200

## Switch baudrate to 115200 bps and press ENTER ...

## Ready for binary (ymodem) download to 0x01000000 at 115200 bps...

Cackets, 6 retries

## Total Size      = 0x0033641c = 3367964 Bytes

## Switch baudrate to 57600 bps and press ESC ...

bfin> bootm 0x1000000

## Booting kernel from Legacy Image at 01000000 ...

   Image Name:   Linux-2.6.28.10-ADI-2009R1-svn72

   Created:      2009-09-14  17:31:05 UTC

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    3367900 Bytes =  3.2 MB

   Load Address: 00001000

   Entry Point:  001bf6d4

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 001bf6d4

Linux version 2.6.28.10-ADI-2009R1-svn7216 (test@uboot32-533ezkit) (gcc version 4.1.2 (ADI svn)) #19 Mon Sep 14 17:30:56 GMT 2009

bootconsole [early_shadow0] enabled

Warning: limiting memory to 31MB due to hardware anomaly 05000263

Board Memory: 32MB

Kernel Managed Memory: 32MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x001313f0

  rodata    = 0x001313f0-0x0018f1d8

  bss       = 0x00190000-0x001a0b48

  data      = 0x001a0b48-0x001b4000

    stack   = 0x001b2000-0x001b4000

  init      = 0x001b4000-0x00674000

  available = 0x00674000-0x01eff000

  DMA Zone  = 0x01f00000-0x02000000

Hardware Trace Active and Enabled

Boot Mode: 0

Blackfin support (C) 2004-2009 Analog Devices, Inc.

Compiled for ADSP-BF533 Rev 0.3

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 594 MHz core clock and 118 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

Data Cache Enabled for CPU0 (write-back)

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 7873

Kernel command line: ip=192.168.0.12:192.168.0.5:192.168.0.1:255.255.255.0::eth0:off

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 128 (order: 7, 512 bytes)

console [ttyBF0] enabled, bootconsole disabled

Dentry cache hash table entries: 4096 (order: 2, 16384 bytes)

Inode-cache hash table entries: 2048 (order: 1, 8192 bytes)

Memory available: 24844k/32768k RAM, (4864k init code, 1216k kernel code, 524k data, 1024k dma, 296k reserved)

Calibrating delay loop... 1183.74 BogoMIPS (lpj=2367488)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (15 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 64 KB (53 KB free)

net_namespace: 288 bytes

NET: Registered protocol family 16

Blackfin DMA Controller

ezkit_init(): registering device resources

SCSI subsystem initialized

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 1024 (order: 1, 8192 bytes)

TCP bind hash table entries: 1024 (order: 0, 4096 bytes)

TCP: Hash tables configured (established 1024 bind 1024)

TCP reno registered

NET: Registered protocol family 1

msgmni has been set to 48

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc00400 (irq = 21) is a BFIN-UART

brd: module loaded

smc91x: not found (-19).

Driver 'sd' needs updating - please use bus_type methods

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@5

driver isp1362-hcd, 2005-04-04

sl811: driver sl811-hcd, 19 May 2005

Initializing USB Mass Storage driver...

usbcore: registered new interface driver usb-storage

USB Mass Storage support registered.

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 1998-07-25 05:25:16 UTC (901344316)

IP-Config: Device `eth0' not found.

Freeing unused kernel memory: 4864k freed

dma_alloc_init: dma_page @ 0x01a33000 - 256 pages at 0x01f00000

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            - http://blackfin.uclinux.org/

\    YP"    `| 8P  `.          - http://docs.blackfin.uclinux.org/

/     \.___.d|    .'           - http://www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    - http://www.analog.com/blackfin

 

Have a lot of fun...

 

 

BusyBox v1.13.4 (2009-09-14 15:27:25 GMT) built-in shell (msh)

Enter 'help' for a list of built-in commands.

 

root:/>

root:/> cat /proc/interrupts

  6:       7747      CORE  Blackfin CoreTimer

14:          1      INTN  rtc-bfin

21:          0      INTN  BFIN_UART_RX

22:       4302      INTN  BFIN_UART_TX

NMI:          0      CORE  Non Maskable Interrupt

Err:          0

root:/>

root:/> ls /dev/

console             pts                 ram4                stdin

cpu_dma_latency     ram0                ram5                stdout

fd                  ram1                ram6                tty

full                ram10               ram7                ttyBF0

kmsg                ram11               ram8                urandom

log                 ram12               ram9                usbmon0

mem                 ram13               random              watchdog

network_latency     ram14               rtc0                zero

network_throughput  ram15               sport0

null                ram2                sport1

ptmx                ram3                stderr

root:/>

root:/> version

kernel:    Linux release 2.6.28.10-ADI-2009R1-svn7216, build #19 Mon Sep 14 17:30:56 GMT 2009

toolchain: bfin-uclinux-gcc release gcc version 4.1.2 (ADI svn)

user-dist: release svn-8738, build #6 Mon Sep 14 17:30:12 GMT 2009

root:/>

--

 

Follow-ups

 

--- Michael Hennerich                                        2009-09-21 06:43:15

Did you add board resources to the BF533-EZKIT platfrom file for the SL811 and

ISP1362?

 

I guess not - rejected.

-Michael

 

--- Vivi Li                                                  2009-11-15 22:45:51

Close it.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

config.kernel    application/octet-stream    31896    Vivi Li

Attachments

    Outcomes