[#5523] Blackfin MUSB build fails after update to 2.6.31

Document created by Aaronwu Employee on Sep 4, 2013
Version 1Show Document
  • View in full screen mode

[#5523] Blackfin MUSB build fails after update to 2.6.31

Submitted By: Mike Frysinger

Open Date

2009-09-11 18:13:36     Close Date

2009-09-16 13:40:08

Priority:

Medium     Assignee:

Cliff Cai

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2010R1     Release:

svn trunk 7304

Category:

N/A     Board:

N/A

Processor:

BF526     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

trunk

App binary format:

N/A     

Summary: Blackfin MUSB build fails after update to 2.6.31

Details:

 

drivers/built-in.o: In function `musb_platform_init':

drivers/usb/musb/blackfin.c:300: undefined reference to `usb_nop_xceiv_register'

make: *** [.tmp_vmlinux1] Error 1

 

happens for all BF52x/BF54x parts

 

Follow-ups

 

--- Cliff Cai                                                2009-09-16 01:24:09

The usb driver framework now introduce a new driver and force to use for all the

usb transceiver which are either built-in with usb ip or which are autonomous

and doesn't require any phy programming such as ISP1x04 etc.

 

So a new config item must be selected.

 

config NOP_USB_XCEIV

    tristate "NOP USB Transceiver Driver"

 

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes