[#5462] KGDBoE does not appear to work

Document created by Aaronwu Employee on Sep 4, 2013
Version 1Show Document
  • View in full screen mode

[#5462] KGDBoE does not appear to work

Submitted By: Mike Frysinger

Open Date

2009-08-26 20:46:40     Close Date

2009-09-08 23:22:51

Priority:

Medium     Assignee:

Sonic Zhang

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2010R1     Release:

svn trunk (2.6.30.3-ADI-2010R1

Category:

N/A     Board:

N/A

Processor:

BF527     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Not reproducible

Uboot version or rev.:

    Toolchain version or rev.:

trunk

App binary format:

N/A     

Summary: KGDBoE does not appear to work

Details:

 

user reported that trying to connect with gdb to kgdb over ethernet resulted in "connection refused" while say settings worked in the 2009R1 branch

 

Follow-ups

 

--- Sonic Zhang                                              2009-09-08 03:28:19

Can't replicated with kernel rev.7268 on SVN head and BF537-stamp board.

 

.....

Program received signal SIGTRAP, Trace/breakpoint trap.

[Switching to Thread -2]

 

Case 35 ...PASS

kgdb_breakpoint () at kernel/kgdb.c:1779

1779            atomic_set(&kgdb_setting_breakpoint, 0);

(gdb) detach

Ending remote debugging.

 

Case 36 ...PASS

(gdb)

root:/>

Case 37 ...PASS

Ending ./kgdb_test.exp

 

--- Mike Frysinger                                           2009-09-08 10:01:30

assuming "svn head" means "svn trunk", the problem was

reported against the 2009R1 branch.  both branch and trunk need to work.

 

--- Sonic Zhang                                              2009-09-08 23:20:38

The bug is reported "while say settings worked in the 2009R1 branch".

 

--- Sonic Zhang                                              2009-09-08 23:20:48

The bug was reported "while say settings worked in the 2009R1 branch".

 

--- Mike Frysinger                                           2009-09-08 23:22:51

yeah, you're right

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes