[#5392] irdaping failed for bfin irda driver

Document created by Aaronwu Employee on Sep 4, 2013
Version 1Show Document
  • View in full screen mode

[#5392] irdaping failed for bfin irda driver

Submitted By: Vivi Li

Open Date

2009-07-24 03:08:27     Close Date

2009-08-05 02:56:56

Priority:

Medium High     Assignee:

Graf Yang

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

Drivers     Board:

N/A

Processor:

ALL     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Rejected

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.1-09r1_rc9

App binary format:

N/A     

Summary: irdaping failed for bfin irda driver

Details:

 

irdaping failed for bfin irda driver.

 

Bellow is the log for bf537-stamp, and its config is attached.

--

Linux version 2.6.28.10-ADI-2009R1-svn7051 (test@uclinux54-adv7393-ad1981-usb1362) (gcc version 4.1.2 (ADI svn)) #40 Thu Jul 23 9

bootconsole [early_shadow0] enabled

bootconsole [early_BFuart0] enabled

early printk enabled on early_BFuart0

Warning: limiting memory to 56MB due to hardware anomaly 05000263

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x00110b00

  rodata    = 0x00110b00-0x00165508

  bss       = 0x00166000-0x001777a8

  data      = 0x001777a8-0x00188000

    stack   = 0x00186000-0x00188000

  init      = 0x00188000-0x008cc000

  available = 0x008cc000-0x037ff000

  DMA Zone  = 0x03f00000-0x04000000

Hardware Trace Active and Enabled

Boot Mode: 0

Blackfin support (C) 2004-2009 Analog Devices, Inc.

Compiled for ADSP-BF537 Rev 0.2

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 500 MHz core clock and 125 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

Data Cache Enabled for CPU0 (write-back)

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 14223

Kernel command line: root=/dev/mtdblock0 rw clkin_hz=25000000 earlyprintk=serial,uart0,57600 console=ttyBF0,57600 ip=10.100.4.50f

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 256 (order: 8, 1024 bytes)

bfin-rtc: invalid date; resetting

console handover:boot [early_BFuart0] boot [early_shadow0]  -> real [ttyBF0]

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 47764k/65536k RAM, (7440k init code, 1086k kernel code, 478k data, 1024k dma, 7744k reserved)

Calibrating delay loop... 995.32 BogoMIPS (lpj=1990656)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (15 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (37 KB free)

net_namespace: 288 bytes

NET: Registered protocol family 16

Blackfin DMA Controller

stamp_init(): registering device resources

NET: Registered protocol family 23

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

NET: Registered protocol family 1

msgmni has been set to 93

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART

brd: module loaded

bfin_mii_bus: probed

bfin_mac: attached PHY driver [SMSC LAN83C185] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=24)@sclk=125MHz)

bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@7

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 1970-01-01 00:00:01 UTC (1)

IP-Config: Gateway not on directly connected network.

Freeing unused kernel memory: 7440k freed

dma_alloc_init: dma_page @ 0x008c8000 - 256 pages at 0x03f00000

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            - http://blackfin.uclinux.org/

\    YP"    `| 8P  `.          - http://docs.blackfin.uclinux.org/

/     \.___.d|    .'           - http://www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    - http://www.analog.com/blackfin

 

Have a lot of fun...

 

 

BusyBox v1.13.4 (2009-07-23 09:54:37 CST) built-in shell (msh)

Enter 'help' for a list of built-in commands.

 

root:/> PHY: 0:01 - Link is Up - 100/Full

 

root:/> modprobe bfin_sir

root:/> irattach irda0 -s&

164

root:/> cat /proc/net/irda/discovery

IrLMP: Discovery log:

 

nickname: VLI-L01, hint: 0x8425, saddr: 0x1d4b2cb2, daddr: 0x0001a064

 

 

root:/> irdaping 0x0001a064

IrDA ping (0x0001a064 on irda0): 32 bytes

--

 

Follow-ups

 

--- Graf Yang                                                2009-07-24 07:11:13

I use the kernel checked out doday, toolchain RC9, irdaping, ircp works fine.

root:/> uname -r                                                           

  

2.6.28.10-ADI-2009R1-svn7066

root:/> cat /proc/net/irda/discovery                                       

  

IrLMP: Discovery log:                                                         

 

nickname: localhost, hint: 0x0400, saddr: 0x1dbb1d2b, daddr: 0x9e72517c       

 

root:/> irdaping 0x9e72517c                                                

  

IrDA ping (0x9e72517c on irda0): 32 bytes                                     

 

32 bytes from 0x9e72517c: irda_seq=0 time=104.00 ms.                          

 

32 bytes from 0x9e72517c: irda_seq=2 time=104.00 ms.                          

 

32 bytes from 0x9e72517c: irda_seq=3 time=104.00 ms.                          

 

32 bytes from 0x9e72517c: irda_seq=5 time=104.00 ms.                          

 

^C                                                                            

 

6 packets received by filter

root:/> ircp -r                                                            

  

Waiting for incoming connection                                               

 

Incoming connection                                                           

 

Receiving z...done                                                            

 

Disconnecting

 

--- Graf Yang                                                2009-07-24 07:14:46

I changed the irtty from COM4 to COM2 by setting the notebook's BIOS.

 

Would you test it under windows again?

 

--- Graf Yang                                                2009-08-03 03:28:34

irdaping a windows host will not get any response.

You'd use it to ping a linux host.

It's not a bug.

 

--- Vivi Li                                                  2009-08-05 02:56:56

OK, close it.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

config.irda    application/octet-stream    32693    Vivi Li

Attachments

Outcomes