[#5366] ad1836 audio shakes sometimes

Document created by Aaronwu Employee on Sep 4, 2013
Version 1Show Document
  • View in full screen mode

[#5366] ad1836 audio shakes sometimes

Submitted By: Vivi Li

Open Date

2009-07-17 01:09:19     Close Date

2009-07-29 05:02:18

Priority:

Medium High     Assignee:

Barry Song

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

BF537     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.1_2009r1-rc9

App binary format:

N/A     

Summary: ad1836 audio shakes sometimes

Details:

 

In ad1836 bf537-stamp, "tone" works alright, but audio played by alsa and oss tools shakes sometimes. Please refer to the commands in the log.

 

--

Linux version 2.6.28.10-ADI-2009R1-svn7010 (test@uclinux50-bf537-ad9960-ad1836) (gcc version 4.1.2 (ADI svn)) #28 Fri Jul 17 07:9

bootconsole [early_shadow0] enabled

bootconsole [early_BFuart0] enabled

early printk enabled on early_BFuart0

Warning: limiting memory to 56MB due to hardware anomaly 05000263

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x0011d950

  rodata    = 0x0011d950-0x001742b0

  bss       = 0x00175000-0x00186ecc

  data      = 0x00186ecc-0x00198000

    stack   = 0x00196000-0x00198000

  init      = 0x00198000-0x008dd000

  available = 0x008dd000-0x037ff000

  DMA Zone  = 0x03e00000-0x04000000

Hardware Trace Active and Enabled

Boot Mode: 0

Reset caused by Software reset

Blackfin support (C) 2004-2009 Analog Devices, Inc.

Compiled for ADSP-BF537 Rev 0.2

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 500 MHz core clock and 125 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

Data Cache Enabled for CPU0 (write-back)

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 14223

Kernel command line: root=/dev/mtdblock0 rw clkin_hz=25000000 earlyprintk=serial,uart0,57600 console=ttyBF0,57600 ip=10.100.4.50f

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 256 (order: 8, 1024 bytes)

console handover:boot [early_BFuart0] boot [early_shadow0]  -> real [ttyBF0]

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 47696k/65536k RAM, (7444k init code, 1138k kernel code, 490k data, 2048k dma, 6720k reserved)

Calibrating delay loop... 995.32 BogoMIPS (lpj=1990656)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (15 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (37 KB free)

net_namespace: 288 bytes

NET: Registered protocol family 16

Blackfin DMA Controller

stamp_init(): registering device resources

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

NET: Registered protocol family 1

msgmni has been set to 93

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART

brd: module loaded

bfin_mii_bus: probed

bfin_mac: attached PHY driver [SMSC LAN83C185] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=24)@sclk=125MHz)

bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@7

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

Advanced Linux Sound Architecture Driver Version 1.0.18rc3.

dma_alloc_init: dma_page @ 0x032f6000 - 512 pages at 0x03e00000

ALSA device list:

  #0: ADI ad1836 at PF4 SPORT0,rx/tx dma ch:3/4,err irq:45

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 1970-01-06 17:41:11 UTC (495671)

IP-Config: Complete:

     device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,

     host=bf537-stamp, domain=, nis-domain=(none),

     bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=

Freeing unused kernel memory: 7444k freed

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            - http://blackfin.uclinux.org/

\    YP"    `| 8P  `.          - http://docs.blackfin.uclinux.org/

/     \.___.d|    .'           - http://www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    - http://www.analog.com/blackfin

 

Have a lot of fun...

 

 

BusyBox v1.13.4 (2009-07-17 07:14:11 CST) built-in shell (msh)

Enter 'help' for a list of built-in commands.

 

root:/> PHY: 0:01 - Link is Up - 100/Full

 

root:/>

root:/> arecord -t wav -c 2 -f S32_LE -r 48000 -d 5 wav; aplay wav

Recording WAVE 'wav' : Signed 32 bit Little Endian, Rate 48000 Hz, Stereo

Playing WAVE 'wav' : Signed 32 bit Little Endian, Rate 48000 Hz, Stereo

root:/> arecord|aplay

Recording WAVE 'stdin' : Unsigned 8 bit, Rate 8000 Hz, Mono

Playing WAVE 'stdin' : Unsigned 8 bit, Rate 8000 Hz, Mono

Aborted by signal Interrupt...

root:/> Aborted by signal Interrupt...

 

root:/> vrec |vplay

Recording VOC : Speed 8000 Hz Mono ...

Playing Creative Labs Voice file ...

root:/>

root:/> version

kernel:    Linux release 2.6.28.10-ADI-2009R1-svn7010, build #28 Fri Jul 17 07:22:25 CST 2009

toolchain: bfin-linux-uclibc-gcc release gcc version 4.1.2 (ADI svn)

user-dist: release svn-8518, build #533 Fri Jul 17 07:17:27 CST 2009

root:/>

--

 

Follow-ups

 

--- Barry Song                                               2009-07-20 09:21:52

Yes. vrec| vplay, arecord | aplay both result in big noise and shaking.

 

--- Barry Song                                               2009-07-21 01:31:43

In 2 channels mode, the buffer is quadrupled. So we should change PCM_BUFFER_MAX

to 1/4 * AD1836_BUF_SZ.

-#define PCM_BUFFER_MAX  (AD1836_BUF_SZ / 2)

+#define PCM_BUFFER_MAX  (AD1836_BUF_SZ / 4)

 

--- Vivi Li                                                  2009-07-29 05:02:18

OK now. Close it.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

config.audio_ad1836    application/octet-stream    32050    Vivi Li

Attachments

Outcomes