[#5365] ad1980 module can not be installed in bf527-ezkit

Document created by Aaronwu Employee on Sep 4, 2013
Version 1Show Document
  • View in full screen mode

[#5365] ad1980 module can not be installed in bf527-ezkit

Submitted By: Vivi Li

Open Date

2009-07-16 22:38:39     Close Date

2009-07-27 23:05:37

Priority:

Medium High     Assignee:

Vivi Li

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

Audio     Board:

EZKIT Lite

Processor:

BF527     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.1_2009r1-rc9

App binary format:

N/A     

Summary: ad1980 module can not be installed in bf527-ezkit

Details:

 

ad1980 module can not be installed in bf527-ezkit in power case. But in audio case that ad1980 is built in, it can work.

 

--

Linux version 2.6.28.10-ADI-2009R1-svn7021 (test@uclinux63-527-usbdev) (gcc version 4.1.2 (ADI svn)) #8 Fri Jul 17 06:28:43 CST 9

bootconsole [early_shadow0] enabled

bootconsole [early_BFuart0] enabled

early printk enabled on early_BFuart0

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x0012af60

  rodata    = 0x0012af60-0x00187a34

  bss       = 0x00188000-0x001992a0

  data      = 0x001992a0-0x001ac000

    stack   = 0x001aa000-0x001ac000

  init      = 0x001ac000-0x0093d000

  available = 0x0093d000-0x03eff000

  DMA Zone  = 0x03f00000-0x04000000

Hardware Trace Active and Enabled

Boot Mode: 1

Reset caused by Software reset

Blackfin support (C) 2004-2009 Analog Devices, Inc.

Compiled for ADSP-BF527 Rev 0.2

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 525 MHz core clock and 131 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

Data Cache Enabled for CPU0 (write-back)

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 16001

Kernel command line: root=/dev/mtdblock0 rw clkin_hz=25000000 earlyprintk=serial,uart1,57600 console=tty0 console=ttyBF0,57600 if

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 256 (order: 8, 1024 bytes)

console handover:boot [early_BFuart0] boot [early_shadow0]  -> real [ttyBF0]

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 54480k/65536k RAM, (7748k init code, 1191k kernel code, 517k data, 1024k dma, 572k reserved)

Calibrating delay loop... 1046.52 BogoMIPS (lpj=2093056)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (15 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (42 KB free)

net_namespace: 288 bytes

NET: Registered protocol family 16

Blackfin DMA Controller

ezkit_init(): registering device resources

SCSI subsystem initialized

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

NET: Registered protocol family 1

msgmni has been set to 106

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

bfin-otp: initialized

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc02000 (irq = 31) is a BFIN-UART

brd: module loaded

bfin_mii_bus: probed

bfin_mac: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=25)@sclk=131MHz)

bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1

Driver 'sd' needs updating - please use bus_type methods

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

Advanced Linux Sound Architecture Driver Version 1.0.18rc3.

ALSA device list:

  No soundcards found.

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 1970-01-05 02:10:25 UTC (353425)

IP-Config: Complete:

     device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,

     host=bf527-ezkit, domain=, nis-domain=(none),

     bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=

Freeing unused kernel memory: 7748k freed

dma_alloc_init: dma_page @ 0x0093a000 - 256 pages at 0x03f00000

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            - http://blackfin.uclinux.org/

\    YP"    `| 8P  `.          - http://docs.blackfin.uclinux.org/

/     \.___.d|    .'           - http://www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    - http://www.analog.com/blackfin

 

Have a lot of fun...

 

 

BusyBox v1.13.4 (2009-07-17 06:24:43 CST) built-in shell (msh)

Enter 'help' for a list of built-in commands.

 

root:/> modprobe snd-ad1980

ASoC version 0.13.2

peripheral_request: Peripheral 31 function 0 is already reserved by bfin_mac !

Requesting Peripherals failed

soc-audio: probe of soc-audio failed with error -14

root:/> version

kernel:    Linux release 2.6.28.10-ADI-2009R1-svn7021, build #8 Fri Jul 17 06:28:43 CST 2009

toolchain: bfin-linux-uclibc-gcc release gcc version 4.1.2 (ADI svn)

user-dist: release svn-8529, build #10 Fri Jul 17 06:26:26 CST 2009

root:/>

--

 

--

Linux version 2.6.28.10-ADI-2009R1-svn7021 (test@uclinux63-527-usbdev) (gcc version 4.1.2 (ADI svn)) #8 Fri Jul 17 02:48:26 CST 9

bootconsole [early_shadow0] enabled

bootconsole [early_BFuart0] enabled

early printk enabled on early_BFuart0

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x00146410

  rodata    = 0x00146410-0x001adc3c

  bss       = 0x001ae000-0x001bf6d8

  data      = 0x001bf6d8-0x001d6000

    stack   = 0x001d4000-0x001d6000

  init      = 0x001d6000-0x00946000

  available = 0x00946000-0x03dff000

  DMA Zone  = 0x03e00000-0x04000000

Hardware Trace Active and Enabled

Boot Mode: 1

Blackfin support (C) 2004-2009 Analog Devices, Inc.

Compiled for ADSP-BF527 Rev 0.2

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 525 MHz core clock and 131 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

Data Cache Enabled for CPU0 (write-back)

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 15747

Kernel command line: root=/dev/mtdblock0 rw clkin_hz=25000000 earlyprintk=serial,uart1,57600 console=tty0 console=ttyBF0,57600 if

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 256 (order: 8, 1024 bytes)

console handover:boot [early_BFuart0] boot [early_shadow0]  -> real [ttyBF0]

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 53420k/65536k RAM, (7616k init code, 1301k kernel code, 575k data, 2048k dma, 572k reserved)

Calibrating delay loop... 1046.52 BogoMIPS (lpj=2093056)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (15 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (42 KB free)

net_namespace: 288 bytes

NET: Registered protocol family 16

Blackfin DMA Controller

ezkit_init(): registering device resources

SCSI subsystem initialized

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

musb_hdrc: version 6.0, musb-dma, host, debug=0

musb_hdrc: USB Host mode controller at ffc03800 using DMA, IRQ 59

musb_hdrc musb_hdrc.0: MUSB HDRC host driver

musb_hdrc musb_hdrc.0: new USB bus registered, assigned bus number 1

usb usb1: configuration #1 chosen from 1 choice

hub 1-0:1.0: USB hub found

dma_alloc_init: dma_page @ 0x009fe000 - 512 pages at 0x03e00000

hub 1-0:1.0: 1 port detected

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

NET: Registered protocol family 1

msgmni has been set to 104

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

bfin-otp: initialized

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc02000 (irq = 31) is a BFIN-UART

brd: module loaded

bfin_mii_bus: probed

bfin_mac: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=25)@sclk=131MHz)

bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1

Driver 'sd' needs updating - please use bus_type methods

m25p80 spi0.1: m25p16 (2048 Kbytes)

Creating 2 MTD partitions on "m25p80":

0x00000000-0x00040000 : "bootloader(spi)"

0x00040000-0x00200000 : "linux kernel(spi)"

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@7

Initializing USB Mass Storage driver...

usbcore: registered new interface driver usb-storage

USB Mass Storage support registered.

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

usbcore: registered new interface driver usbhid

usbhid: v2.6:USB HID core driver

Advanced Linux Sound Architecture Driver Version 1.0.18rc3.

ASoC version 0.13.2

dma rx:5 tx:6, err irq:16, regs:ffc00900

AD1980 SoC Audio Codec

asoc: AC97 <-> bf5xx-ac97 mapping ok

bf5xx_ac97_cold_reset: Not implemented

ad1980: Found AD1981 - only 2/2 IN/OUT Channels supported

ALSA device list:

  #0: bf5xx-board (AD1980)

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 2014-11-13 11:51:06 UTC (1415879466)

IP-Config: Complete:

     device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,

     host=bf527-ezkit, domain=, nis-domain=(none),

     bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=

Freeing unused kernel memory: 7616k freed

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            - http://blackfin.uclinux.org/

\    YP"    `| 8P  `.          - http://docs.blackfin.uclinux.org/

/     \.___.d|    .'           - http://www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    - http://www.analog.com/blackfin

 

Have a lot of fun...

 

 

BusyBox v1.13.4 (2009-07-17 02:44:15 CST) built-in shell (msh)

Enter 'help' for a list of built-in commands.

 

root:/> PHY: 0:01 - Link is Up - 100/Full

 

root:/> tone

TONE: generating sine wave at 1000 Hz...

root:/>

--

 

Follow-ups

 

--- Sonic Zhang                                              2009-07-22 03:53:55

Peripheral 31 is PG15 (PIN TFS0 on sport 0). It looks you forget to set the port

of ad1980 driver to sport0 on bf527-ezkit.

 

--- Vivi Li                                                  2009-07-22 05:09:19

Fixed in build script.

 

--- Vivi Li                                                  2009-07-27 23:05:37

OK now.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

config.power    application/octet-stream    34280    Vivi Li

config.audio_ad1981b    application/octet-stream    37313    Vivi Li

Outcomes