[#5364] ad1981b fails to work on bf533-stamp

Document created by Aaronwu Employee on Sep 4, 2013
Version 1Show Document
  • View in full screen mode

[#5364] ad1981b fails to work on bf533-stamp

Submitted By: Vivi Li

Open Date

2009-07-16 05:57:25     Close Date

2009-07-22 23:54:54

Priority:

Medium High     Assignee:

Cliff Cai

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

Audio     Board:

STAMP

Processor:

BF533     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Rejected

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.1_09r1-rc9

App binary format:

N/A     

Summary: ad1981b fails to work on bf533-stamp

Details:

 

For ad1981b on bf533-stamp, AD1980 AC97 reset failed for ad1981b v0.3 board; for ad1981b v0.1 board, reset ok, and tone is ok, but no sound output for alsa and oss tools.

 

Bellow is the log for ad1981b v0.3:

--

Linux version 2.6.28.10-ADI-2009R1-svn7006 (test@uclinux77-bf533-ad1836-spi) (gcc version 4.1.2 (ADI svn)) #20 Wed Jul 15 21:06:9

bootconsole [early_shadow0] enabled

bootconsole [early_BFuart0] enabled

early printk enabled on early_BFuart0

Warning: limiting memory to 56MB due to hardware anomaly 05000263

Board Memory: 128MB

Kernel Managed Memory: 128MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x001216b0

  rodata    = 0x001216b0-0x001777dc

  bss       = 0x00178000-0x00188c10

  data      = 0x00188c10-0x00198000

    stack   = 0x00196000-0x00198000

  init      = 0x00198000-0x0082b000

  available = 0x0082b000-0x037ff000

  DMA Zone  = 0x07e00000-0x08000000

Hardware Trace Active and Enabled

Boot Mode: 0

Reset caused by Software reset

Blackfin support (C) 2004-2009 Analog Devices, Inc.

Compiled for ADSP-BF533 Rev 0.3

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 497 MHz core clock and 99 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

Data Cache Enabled for CPU0 (write-back)

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 14223

Kernel command line: root=/dev/mtdblock0 rw clkin_hz=11059200 earlyprintk=serial,uart0,57600 console=ttyBF0,57600 ip=10.100.4.50f

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 256 (order: 8, 1024 bytes)

console handover:boot [early_BFuart0] boot [early_shadow0]  -> real [ttyBF0]

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 48408k/131072k RAM, (6732k init code, 1153k kernel code, 475k data, 2048k dma, 72256k reserved)

Calibrating delay loop... 991.23 BogoMIPS (lpj=1982464)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (15 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 64 KB (53 KB free)

net_namespace: 288 bytes

NET: Registered protocol family 16

Blackfin DMA Controller

stamp_init(): registering device resources

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

NET: Registered protocol family 1

msgmni has been set to 94

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc00400 (irq = 21) is a BFIN-UART

brd: module loaded

smc91x.c: v1.1, sep 22 2004 by Nicolas Pitre <nico@cam.org>

eth0: SMC91C11xFD (rev 1) at 20300300 IRQ 40 [nowait]

eth0: Ethernet addr: 00:e0:22:fe:04:cc

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@5

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

Advanced Linux Sound Architecture Driver Version 1.0.18rc3.

ASoC version 0.13.2

dma rx:1 tx:2, err irq:10, regs:ffc00800

AD1980 SoC Audio Codec

dma_alloc_init: dma_page @ 0x0310e000 - 512 pages at 0x07e00000

asoc: AC97 <-> bf5xx-ac97 mapping ok

bf5xx_ac97_cold_reset: Not implemented

bf5xx_ac97_cold_reset: Not implemented

bf5xx_ac97_cold_reset: Not implemented

bf5xx_ac97_cold_reset: Not implemented

bf5xx_ac97_cold_reset: Not implemented

bf5xx_ac97_cold_reset: Not implemented

bf5xx_ac97_cold_reset: Not implemented

bf5xx_ac97_cold_reset: Not implemented

bf5xx_ac97_cold_reset: Not implemented

bf5xx_ac97_cold_reset: Not implemented

bf5xx_ac97_cold_reset: Not implemented

AD1980 AC97 reset failed

AC97 link error

soc-audio: probe of soc-audio failed with error -5

ALSA device list:

  No soundcards found.

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 1975-03-03 00:05:50 UTC (163037150)

eth0: link down

IP-Config: Complete:

     device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,

     host=bf533-stamp, domain=, nis-domain=(none),

     bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=

Freeing unused kernel memory: 6732k freed

eth0: link up, 100Mbps, full-duplex, lpa 0x41E1

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            - http://blackfin.uclinux.org/

\    YP"    `| 8P  `.          - http://docs.blackfin.uclinux.org/

/     \.___.d|    .'           - http://www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    - http://www.analog.com/blackfin

 

Have a lot of fun...

 

 

BusyBox v1.13.4 (2009-07-15 21:03:20 MDT) built-in shell (msh)

Enter 'help' for a list of built-in commands.

 

root:/> version

kernel:    Linux release 2.6.28.10-ADI-2009R1-svn7006, build #20 Wed Jul 15 21:06:49 MDT 2009

toolchain: bfin-linux-uclibc-gcc release gcc version 4.1.2 (ADI svn)

user-dist: release svn-8498, build #323 Wed Jul 15 21:06:00 MDT 2009

root:/>

--

 

Bellow is the log for ad1981b v0.1:

--

Linux version 2.6.28.10-ADI-2009R1-svn7006 (test@uclinux77-bf533-ad1836-spi) (gcc version 4.1.2 (ADI svn)) #20 Wed Jul 15 21:06:9

bootconsole [early_shadow0] enabled

bootconsole [early_BFuart0] enabled

early printk enabled on early_BFuart0

Warning: limiting memory to 56MB due to hardware anomaly 05000263

Board Memory: 128MB

Kernel Managed Memory: 128MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x001216b0

  rodata    = 0x001216b0-0x001777dc

  bss       = 0x00178000-0x00188c10

  data      = 0x00188c10-0x00198000

    stack   = 0x00196000-0x00198000

  init      = 0x00198000-0x0082b000

  available = 0x0082b000-0x037ff000

  DMA Zone  = 0x07e00000-0x08000000

Hardware Trace Active and Enabled

Boot Mode: 0

Blackfin support (C) 2004-2009 Analog Devices, Inc.

Compiled for ADSP-BF533 Rev 0.3

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 497 MHz core clock and 99 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

Data Cache Enabled for CPU0 (write-back)

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 14223

Kernel command line: root=/dev/mtdblock0 rw clkin_hz=11059200 earlyprintk=serial,uart0,57600 console=ttyBF0,57600 ip=10.100.4.50f

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 256 (order: 8, 1024 bytes)

console handover:boot [early_BFuart0] boot [early_shadow0]  -> real [ttyBF0]

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 48408k/131072k RAM, (6732k init code, 1153k kernel code, 475k data, 2048k dma, 72256k reserved)

Calibrating delay loop... 991.23 BogoMIPS (lpj=1982464)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (15 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 64 KB (53 KB free)

net_namespace: 288 bytes

NET: Registered protocol family 16

Blackfin DMA Controller

stamp_init(): registering device resources

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

NET: Registered protocol family 1

msgmni has been set to 94

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc00400 (irq = 21) is a BFIN-UART

brd: module loaded

smc91x.c: v1.1, sep 22 2004 by Nicolas Pitre <nico@cam.org>

eth0: SMC91C11xFD (rev 1) at 20300300 IRQ 40 [nowait]

eth0: Ethernet addr: 00:e0:22:fe:04:cc

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@5

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

Advanced Linux Sound Architecture Driver Version 1.0.18rc3.

ASoC version 0.13.2

dma rx:1 tx:2, err irq:10, regs:ffc00800

AD1980 SoC Audio Codec

dma_alloc_init: dma_page @ 0x0310e000 - 512 pages at 0x07e00000

asoc: AC97 <-> bf5xx-ac97 mapping ok

bf5xx_ac97_cold_reset: Not implemented

ad1980: Found AD1981 - only 2/2 IN/OUT Channels supported

ALSA device list:

  #0: bf5xx-board (AD1980)

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 2036-08-06 15:00:09 UTC (2101647609)

eth0: link down

IP-Config: Complete:

     device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,

     host=bf533-stamp, domain=, nis-domain=(none),

     bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=

Freeing unused kernel memory: 6732k freed

eth0: link up, 100Mbps, full-duplex, lpa 0x41E1

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            - http://blackfin.uclinux.org/

\    YP"    `| 8P  `.          - http://docs.blackfin.uclinux.org/

/     \.___.d|    .'           - http://www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    - http://www.analog.com/blackfin

 

Have a lot of fun...

 

 

BusyBox v1.13.4 (2009-07-15 21:03:20 MDT) built-in shell (msh)

Enter 'help' for a list of built-in commands.

 

root:/> tone

TONE: generating sine wave at 1000 Hz...

root:/>

root:/>  arecord -t wav -c 2 -f S16_LE -r 8000 -d 5 wav

Recording WAVE 'wav' : Signed 16 bit Little Endian, Rate 8000 Hz, Stereo

root:/> aplay wav

Playing WAVE 'wav' : Signed 16 bit Little Endian, Rate 8000 Hz, Stereo

root:/>

root:/> version

kernel:    Linux release 2.6.28.10-ADI-2009R1-svn7006, build #20 Wed Jul 15 21:06:49 MDT 2009

toolchain: bfin-linux-uclibc-gcc release gcc version 4.1.2 (ADI svn)

user-dist: release svn-8498, build #323 Wed Jul 15 21:06:00 MDT 2009

root:/>

--

 

Follow-ups

 

--- Cliff Cai                                                2009-07-21 23:49:32

The two cards you used seems bad(one of it even causes reset signal of board to

be wrong).I've tried the other three cards,they work just fine.

 

Cliff

 

--- Vivi Li                                                  2009-07-22 23:54:54

OK now. Close it.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

config.audio_ad1981b    application/octet-stream    30989    Vivi Li

Attachments

Outcomes