[#5328] usb device will reset on bf527-ezkit for dma mode when mke2fs in usb storage

Document created by Aaronwu Employee on Sep 4, 2013
Version 1Show Document
  • View in full screen mode

[#5328] usb device will reset on bf527-ezkit for dma mode when mke2fs in usb storage

Submitted By: Vivi Li

Open Date

2009-07-08 06:50:47     Close Date

2009-08-09 19:30:18

Priority:

Medium     Assignee:

Cliff Cai

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

Drivers     Board:

N/A

Processor:

BF527     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.1_2009r1-rc9

App binary format:

N/A     

Summary: usb device will reset on bf527-ezkit for dma mode when mke2fs in usb storage

Details:

 

During mke2fs in usb storage on bf527-ezkit, usb device will reset several times for dma mode. PIO mode is ok.

 

Bellow is the log in dma mode:

--

U-Boot 2008.10-svn1954 (ADI-2009R1-rc2) (Jul  1 2009 - 14:04:59)

 

CPU:   ADSP bf527-0.0 (Detected Rev: 0.0) (parallel flash boot)

Board: ADI BF527 EZ-Kit board

       Support: http://blackfin.uclinux.org/

Clock: VCO: 525 MHz, Core: 525 MHz, System: 131.250 MHz

RAM:   64 MB

Flash:  4 MB

In:    serial

Out:   serial

Err:   serial

Net:   Blackfin EMAC

MAC:   00:E0:22:FE:B8:11

Hit any key to stop autoboot:  0

Using Blackfin EMAC device

TFTP from server 10.100.4.174; our IP address is 10.100.4.50

Filename \\\\\\\\\\\\\\\'uImage\\\\\\\\\\\\\\\'.

Load address: 0x1000000

Loading: #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         ##################################

done

Bytes transferred = 5268878 (50658e hex)

## Booting kernel from Legacy Image at 01000000 ...

   Image Name:   Linux-2.6.28.10-ADI-2009R1-svn69

   Created:      2009-07-07   5:44:18 UTC

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    5268814 Bytes =  5 MB

   Load Address: 00001000

   Entry Point:  001db61c

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 001db61c

Linux version 2.6.28.10-ADI-2009R1-svn6923 (test@uclinux60-bf527-std) (gcc version 4.1.2 (ADI svn)) #24 Tue Jul 7 13:44:02 CST 29

bootconsole [early_BFuart0] enabled

early printk enabled on early_BFuart0

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x0013f690

  rodata    = 0x0013f690-0x001a71f0

  bss       = 0x001a8000-0x001b906c

  data      = 0x001b906c-0x001ce000

    stack   = 0x001cc000-0x001ce000

  init      = 0x001ce000-0x009c2000

  available = 0x009c2000-0x03eff000

  DMA Zone  = 0x03f00000-0x04000000

Hardware Trace Active and Enabled

Boot Mode: 1

Blackfin support (C) 2004-2009 Analog Devices, Inc.

Compiled for ADSP-BF527 Rev 0.0

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 525 MHz core clock and 131 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

Data Cache Enabled for CPU0 (write-back)

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 16001

Kernel command line: root=/dev/mtdblock0 rw clkin_hz=25000000 earlyprintk=serial,uart1,57600 console=tty0 console=ttyBF0,57600 if

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 256 (order: 8, 1024 bytes)

console handover:boot [early_BFuart0]  -> real [ttyBF0]

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 53948k/65536k RAM, (8144k init code, 1273k kernel code, 571k data, 1024k dma, 572k reserved)

Calibrating delay loop... 1046.52 BogoMIPS (lpj=2093056)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (15 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (42 KB free)

net_namespace: 288 bytes

NET: Registered protocol family 16

Blackfin DMA Controller

ezkit_init(): registering device resources

SCSI subsystem initialized

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

musb_hdrc: version 6.0, musb-dma, host, debug=0

musb_hdrc: USB Host mode controller at ffc03800 using DMA, IRQ 59

musb_hdrc musb_hdrc.0: MUSB HDRC host driver

musb_hdrc musb_hdrc.0: new USB bus registered, assigned bus number 1

usb usb1: configuration #1 chosen from 1 choice

hub 1-0:1.0: USB hub found

dma_alloc_init: dma_page @ 0x03ea8000 - 256 pages at 0x03f00000

hub 1-0:1.0: 1 port detected

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

NET: Registered protocol family 1

msgmni has been set to 105

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

bfin-t350mcqb: 320x240 24-bit RGB FrameBuffer initializing...

bfin-otp: initialized

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc02000 (irq = 31) is a BFIN-UART

brd: module loaded

bfin_mii_bus: probed

bfin_mac: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=25)@sclk=131MHz)

bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1

Driver \\\\\\\\\\\\\\\'sd\\\\\\\\\\\\\\\' needs updating - please use bus_type methods

m25p80 spi0.1: m25p16 (2048 Kbytes)

Creating 2 MTD partitions on \\\\\\\\\\\\\\\"m25p80\\\\\\\\\\\\\\\":

0x00000000-0x00040000 : \\\\\\\\\\\\\\\"bootloader(spi)\\\\\\\\\\\\\\\"

0x00040000-0x00200000 : \\\\\\\\\\\\\\\"linux kernel(spi)\\\\\\\\\\\\\\\"

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@7

Initializing USB Mass Storage driver...

usbcore: registered new interface driver usb-storage

USB Mass Storage support registered.

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

usbcore: registered new interface driver usbhid

usbhid: v2.6:USB HID core driver

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 2004-05-31 21:24:27 UTC (1086038667)

IP-Config: Complete:

     device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,

     host=bf527-ezkit, domain=, nis-domain=(none),

     bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=

Freeing unused kernel memory: 8144k freed

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \\\\\\\\\\\\\\\\

       d888888b.         /       _     _                         \\\\\\\\\\\\\\\\

       8P\\\\\\\\\\\\\\\"YP\\\\\\\\\\\\\\\"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \\\\\\\\\\\\\\\\ \\\\\\\\\\\\\\\\/ /       |

       8\\\\\\\\\\\\\\\'    .88       \\\\\\\\\\\\\\\\        | |   | |  _ \\\\\\\\\\\\\\\\| | | | \\\\\\\\\\\\\\\\  /        |

       8`._.\\\\\\\\\\\\\\\' Y8.       \\\\\\\\\\\\\\\\       | |__ | | | | | |_| | /  \\\\\\\\\\\\\\\\        |

      d/      `8b.       \\\\\\\\\\\\\\\\      \\\\\\\\\\\\\\\\____||_|_| |_|\\\\\\\\\\\\\\\\____|/_/\\\\\\\\\\\\\\\\_\\\\\\\\\\\\\\\\       |

     dP   .    Y8b.       \\\\\\\\\\\\\\\\   For embedded processors including   |

    d8:\\\\\\\\\\\\\\\'  \\\\\\\\\\\\\\\"  `::88b        \\\\\\\\\\\\\\\\    the Analog Devices Blackfin      /

   d8\\\\\\\\\\\\\\\"         \\\\\\\\\\\\\\\'Y88b        \\\\\\\\\\\\\\\\___________________________________/

  :8P    \\\\\\\\\\\\\\\'      :888

   8a.   :     _a88P         For further information, check out:

._/\\\\\\\\\\\\\\\"Yaa_:   .| 88P|            - http://blackfin.uclinux.org/

| /0/ Fu\\\\\\\\\\\\\\\\ll__.| 8P  `.        PHY : t0:/01o -. Lainfk .isl Uup. r-

    .\\\\\\\\\\\\\\\'           - http://www.uclinux.org/

`--..__)8888P`._.\\\\\\\\\\\\\\\'  jgs/a:f    - http://www.analog.com/blackfin

 

Have a lot of fun...

 

 

BusyBox v1.13.4 (2009-07-07 13:17:36 CST) built-in shell (msh)

Enter \\\\\\\\\\\\\\\'help\\\\\\\\\\\\\\\' for a list of built-in commands.

 

root:/> usb 1-1: new high speed USB device using musb_hdrc and address 2

usb 1-1: configuration #1 chosen from 1 choice

scsi0 : SCSI emulation for USB Mass Storage devices

scsi 0:0:0:0: Direct-Access     SanDisk  U3 Cruzer Micro  2.21 PQ: 0 ANSI: 2

sd 0:0:0:0: [sda] 1994385 512-byte hardware sectors: (1.02 GB/973 MiB)

sd 0:0:0:0: [sda] Write Protect is off

sd 0:0:0:0: [sda] Assuming drive cache: write through

sd 0:0:0:0: [sda] 1994385 512-byte hardware sectors: (1.02 GB/973 MiB)

sd 0:0:0:0: [sda] Write Protect is off

sd 0:0:0:0: [sda] Assuming drive cache: write through

sda: sda1 sda2

sd 0:0:0:0: [sda] Attached SCSI removable disk

 

root:/>

root:/> date; mke2fs /dev/sda1; date

Mon May 31 21:25:32 UTC 2004

mke2fs 1.41.4 (27-Jan-2009)

ext2fs_check_if_mount: No such file or directory while determining whether /dev/sda1 is mounted.

Filesystem label=

OS type: Linux

Block size=1024 (log=0)

Fragment size=1024 (log=0)

123952 inodes, 495776 blocks

24788 blocks (5.00%) reserved for the super user

First data block=1

Maximum filesystem blocks=67633152

61 block groups

8192 blocks per group, 8192 fragments per group

2032 inodes per group

Superblock backups stored on blocks:

        8193, 24577, 40961, 57345, 73729, 204801, 221185, 401409

 

Writing inode tables: done

Writing superblocks and filesystem accounting information: usb 1-1: reset high speed USB device using musb_hdrc and address 2

done

 

This filesystem will be automatically checked every 35 mounts or

180 days, whichever comes first.  Use tune2fs -c or -i to override.

Mon May 31 21:26:20 UTC 2004

root:/>

--

 

Bellow is the result in PIO mode:

--

root:/> date; mke2fs /dev/sda1; date

Mon May 31 21:17:32 UTC 2004

mke2fs 1.41.4 (27-Jan-2009)

ext2fs_check_if_mount: No such file or directory while determining whether /dev/sda1 is mounted.

Filesystem label=

OS type: Linux

Block size=1024 (log=0)

Fragment size=1024 (log=0)

123952 inodes, 495776 blocks

24788 blocks (5.00%) reserved for the super user

First data block=1

Maximum filesystem blocks=67633152

61 block groups

8192 blocks per group, 8192 fragments per group

2032 inodes per group

Superblock backups stored on blocks:

        8193, 24577, 40961, 57345, 73729, 204801, 221185, 401409

 

Writing inode tables: done

Writing superblocks and filesystem accounting information: done

 

This filesystem will be automatically checked every 22 mounts or

180 days, whichever comes first.  Use tune2fs -c or -i to override.

Mon May 31 21:17:49 UTC 2004

root:/>

--

 

Follow-ups

 

--- Cliff Cai                                                2009-07-09 22:11:34

it works for me.

 

Cliff

 

--- Vivi Li                                                  2009-07-29 00:02:50

I can still see this bug happening on regression.

 

--- Cliff Cai                                                2009-08-04 03:26:10

I tried it with BF527 v0.2,it seemed Ok.

 

Cliff

 

--- Sonic Zhang                                              2009-08-06 01:40:44

This bug may relate to anomaly 05000380.

Temporary walkaround to 2009R1 is disable DMA for bf527 v0.0 and v0.1

 

--- Vivi Li                                                  2009-08-06 07:08:43

Yes, it works on BF527 v0.2 but fails on old revision.

 

--- Vivi Li                                                  2009-08-10 00:30:28

Disable usbhost test in dma mode with BF527-EZKIT 0.0 and 0.1 silicon.

So close this bug.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

config.usbhost_bf5xx.pio    application/octet-stream    38365    Vivi Li

config.usbhost_bf5xx.dma    application/octet-stream    38415    Vivi Li

Outcomes