[#5299] joystick fails to feel the touch now

Document created by Aaronwu Employee on Sep 4, 2013
Version 1Show Document
  • View in full screen mode

[#5299] joystick fails to feel the touch now

Submitted By: Mingquan Pan

Open Date

2009-06-30 04:23:51     Close Date

2009-07-07 06:24:36

Priority:

Medium High     Assignee:

Barry Song

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

BF537     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

09r1-rc7

App binary format:

N/A     

Summary: joystick fails to feel the touch now

Details:

 

joystick fails to feel the touch now on bf537 stamp. It didn't react to the touching on the board.

 

## Booting kernel from Legacy Image at 02000000 ...

   Image Name:   Linux-2.6.28.10-ADI-2009R1-svn68

   Created:      2009-06-30   7:59:28 UTC

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    4695435 Bytes =  4.5 MB

   Load Address: 00001000

   Entry Point:  0018e594

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 0018e594

Linux version 2.6.28.10-ADI-2009R1-svn6870 (test@my-local-machine) (gcc version 4.1.2 (ADI svn)) #12 Tue Jun 30 15:59:14 CST 2009

console [early_BFuart0] enabled

early printk enabled on early_BFuart0

Warning: limiting memory to 56MB due to hardware anomaly 05000263

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x0010aff0

  rodata    = 0x0010aff0-0x0015df6c

  bss       = 0x0015e000-0x0016f800

  data      = 0x0016f800-0x00180000

    stack   = 0x0017e000-0x00180000

  init      = 0x00180000-0x008c8000

  available = 0x008c8000-0x037ff000

  DMA Zone  = 0x03f00000-0x04000000

Hardware Trace Active and Enabled

Boot Mode: 0

Reset caused by Software reset

Blackfin support (C) 2004-2009 Analog Devices, Inc.

Compiled for ADSP-BF537 Rev 0.2

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 500 MHz core clock and 125 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

Data Cache Enabled for CPU0 (write-back)

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 14223

Kernel command line: root=/dev/mtdblock0 rw earlyprintk=serial,uart0,57600 ip=10.100.4.50:10.100.4.174:192.168.0.1:255.255.255.0:bf537-stamp:eth0:off

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 256 (order: 8, 1024 bytes)

console handover: boot [early_BFuart0] -> real [ttyBF0]

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 47780k/65536k RAM, (7456k init code, 1063k kernel code, 469k data, 1024k dma, 7744k reserved)

Calibrating delay loop... 995.32 BogoMIPS (lpj=1990656)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (15 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (37 KB free)

net_namespace: 288 bytes

NET: Registered protocol family 16

Blackfin DMA Controller

stamp_init(): registering device resources

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

NET: Registered protocol family 1

msgmni has been set to 93

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART

brd: module loaded

bfin_mii_bus: probed

bfin_mac: attached PHY driver [SMSC LAN83C185] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=24)@sclk=125MHz)

bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@7

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

i2c /dev entries driver

i2c-bfin-twi i2c-bfin-twi.0: Blackfin BF5xx on-chip I2C TWI Contoller, regs_base@ffc01400

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 1970-01-01 00:00:35 UTC (35)

IP-Config: Gateway not on directly connected network.

Freeing unused kernel memory: 7456k freed

dma_alloc_init: dma_page @ 0x008c5000 - 256 pages at 0x03f00000

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            - http://blackfin.uclinux.org/

\    YP"    `| 8P  `.          - http://docs.blackfin.uclinux.org/

/     \.___.d|    .'           - http://www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    - http://www.analog.com/blackfin

 

Have a lot of fun...

 

 

BusyBox v1.13.4 (2009-06-30 12:31:57 CST) built-in shell (msh)

Enter 'help' for a list of built-in commands.

 

root:/> verPHY: 0:01 - Link is Up - 100/Full

sion

kernel:    Linux release 2.6.28.10-ADI-2009R1-svn6870, build #12 Tue Jun 30 15:59:14 CST 2009

toolchain: bfin-uclinux-gcc release gcc version 4.1.2 (ADI svn)

user-dist: release svn-8385, build #6 Tue Jun 30 15:58:33 CST 2009

root:/>

*******************************************************************

STEP 3: Starting test.

 

 

modprobe ad7142

ad7142_joystick 0-002c: is attached at 0

module insert success.

 

 

Case 1 ...PASS

x2c

input: ad7142 joystick as /devices/virtual/input/input0

root:/> lsmod

Module                  Size  Used by

ad7142

module ls success.

 

 

Case 2 ...PASS

               4428  0

root:/> cd /bin

root:/bin> event_test /dev/input/event0

ad7142_joystick 0-002c: Open AD7142 Rev 0.2

Input driver version is 1.0.0

Input device ID: bus 0x18 vendor 0x1 product 0x1 version 0x100

Input device name: "ad7142 joystick"

Supported events:

  Event type 0 (Reset)

    Event code 0 (Reset)

    Event code 1 (Key)

  Event type 1 (Key)

    Event code 103 (Up)

    Event code 105 (Left)

    Event code 106 (Right)

    Event code 108 (Down)

    Event code 294 (BaseBtn)

    Event code 295 (BaseBtn2)

    Event code 296 (BaseBtn3)

    Event code 297 (BaseBtn4)

Testing ..

Please touch the Joystick board...

 

. (interrupt to exit)

 

 

Follow-ups

 

--- Barry Song                                               2009-06-30 09:01:49

At first, the hardware is completely normal. I2C is ok, and interrupt output

from AD7142 is ok while touching.

The interrupt line is connected to PF7 not PF5. In stamp.c, it is defined as

PF5. So it's wrong. But while using PF7, it is strange the enable_irq can't

enable it at all(without any other devices using PF7 compiled). So I weird a

fly-line to PF5 as interrupt, in order to enable_irq normally, I still need to

delete the call to disable_irq_nosync(client->irq) in ad7142_probe,

otherwise, the IRQ can't be really enabled in ad7142_open by enable_irq.

After making the two changes, the AD7142 works completely normally.

I can't accept that as a official fix and need to check what's the reason PF7

can't be enabled at all.

 

--- Barry Song                                               2009-07-07 03:29:38

According to the measure by multimeter, interrupt output of ad7142 is connected

to PIN13 of TWI, the net name is PG5_ELVIS_PF7. I misunderstood it to be PF7,

but in fact it's PG5.

So after making the following patch, joystick gets to work completely normal:

Index: stamp.c

===================================================================

--- stamp.c     (revision 6779)

+++ stamp.c     (working copy)

@@ -1277,7 +1277,7 @@

#if defined(CONFIG_JOYSTICK_AD7142) || defined(CONFIG_JOYSTICK_AD7142_MODULE)

        {

                I2C_BOARD_INFO("ad7142_joystick", 0x2C),

-               .irq = IRQ_PF5,

+               .irq = IRQ_PG5,

        },

#endif

#if defined(CONFIG_BFIN_TWI_LCD) || defined(CONFIG_TWI_LCD_MODULE)

 

 

--- Mingquan Pan                                             2009-07-07 06:24:36

Yes,fixed. Close.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

config.joystick    application/octet-stream    33580    Mingquan Pan

Attachments

Outcomes