[#5279] kernel build failure in boards with isp1760 enabled

Document created by Aaronwu Employee on Sep 4, 2013
Version 1Show Document
  • View in full screen mode

[#5279] kernel build failure in boards with isp1760 enabled

Submitted By: Peter Meerwald

Open Date

2009-06-18 12:41:27     Close Date

2009-08-10 04:40:28

Priority:

Medium     Assignee:

Nobody

Status:

Closed     Fixed In Release:

N/A

Found In Release:

snaps     Release:

Category:

Make Errors     Board:

STAMP

Processor:

BF537     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

svn

App binary format:

N/A     

Summary: kernel build failure in boards with isp1760 enabled

Details:

 

svn rev 6785

 

pmeerw@pmeerw-pc:~/bf/svn/linux-kernel$ make

  CHK     include/linux/version.h

  CHK     include/linux/utsrelease.h

  SYMLINK include/asm -> include/asm-blackfin

  CALL    scripts/checksyscalls.sh

  CHK     include/linux/compile.h

  CC      arch/blackfin/mach-bf537/boards/stamp.o

arch/blackfin/mach-bf537/boards/stamp.c:82: error: unknown field ‘port1_disable’ specified in initializer

 

 

arch/blackfin/mach-bf537/boards/stamp.c:

 

#if defined(CONFIG_USB_ISP1760_HCD) || defined(CONFIG_USB_ISP1760_HCD_MODULE)

 

// ...

 

static struct isp1760_platform_data isp1760_priv = {

        .is_isp1761 = 0,

        .port1_disable = 0,   <-- line 82, error!!!

        .bus_width_16 = 1,

        .port1_otg = 0,

        .analog_oc = 0,

        .dack_polarity_high = 0,

        .dreq_polarity_high = 0,

};

 

 

Follow-ups

 

--- Peter Meerwald                                           2009-06-18 12:43:22

likely broken by

 

pmeerw@pmeerw-pc:~/bf/svn/linux-kernel$ svn log include/linux/usb/isp1760.h

------------------------------------------------------------------------

r6669 | vapier | 2009-06-12 03:12:35 +0200 (Fri, 12 Jun 2009) | 1 line

 

drop support for port1 disable as upstream has dropped it as well

 

--- Mike Frysinger                                           2009-06-18 15:13:54

dropped from all the boards, not just bf537-stamp.  thanks.

 

--- Michael Hennerich                                        2009-08-10 09:40:39

close it

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes