[#5267] ping flood test fails for gadget ethernet test with DMA mode

Document created by Aaronwu Employee on Sep 4, 2013
Version 1Show Document
  • View in full screen mode

[#5267] ping flood test fails for gadget ethernet test with DMA mode

Submitted By: Vivi Li

Open Date

2009-06-18 00:39:44     Close Date

2009-06-30 23:37:22

Priority:

Medium High     Assignee:

Cliff Cai

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

Drivers     Board:

N/A

Processor:

ALL     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.1_09r1-rc7

App binary format:

N/A     

Summary: ping flood test fails for gadget ethernet test with DMA mode

Details:

 

For gadget ethernet test with DMA mode, on both bf527 and bf548, ping flood test fails. Bellow is the log.

 

--

ping -f -l50 -c 1000 192.168.1.66

PING 192.168.1.66 (192.168.1.66) 56(84) bytes of data.

..........................................................................................................................................................................................................................................................................................................^HE^HE^HE^HE............................................................................................................................................................................................................................................................................................................^HE^HE^HE...........................................................................................................................................................................................................................................................................................................^HE^HE^HE.......................................................................................................^HE^HE^HE^M

--- 192.168.1.66 ping statistics ---

1000 packets transmitted, 0 received, +13 errors, 100% packet loss, time 9647ms^M

, pipe 52, ipg/ewma 9.657/0.000 ms

--

 

Follow-ups

 

--- Cliff Cai                                                2009-06-30 06:10:57

fixed by clearing interrupt flags at the beginning of ISR.

 

Cliff

 

--- Vivi Li                                                  2009-06-30 23:37:22

Yes it's OK now. Close it.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes