[#5261] USB audio gadget feedback

Document created by Aaronwu Employee on Sep 4, 2013
Version 1Show Document
  • View in full screen mode

[#5261] USB audio gadget feedback

Submitted By: Mike Frysinger

Open Date

2009-06-16 09:06:22     Close Date

2010-01-19 01:19:41

Priority:

Medium     Assignee:

Cliff Cai

Status:

Closed     Fixed In Release:

N/A

Found In Release:

snaps     Release:

Category:

N/A     Board:

N/A

Processor:

BF548     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

trunk

App binary format:

N/A     

Summary: USB audio gadget feedback

Details:

 

feedback from Sergey Lapin <slapin@ossfans.org>:

 

As first, it never frees ALSA devices.

When that is fixed, it never able to recover operation

on second load. Tested on MUSB on OMAP3530EVM.

It is very useful gadget, so I'd really like to see it fixed.

.wTotalLength in ac_header_descriptor descriptor should contain sum of sizes

of interface and unit descriptors, per Audio Device Class specification

1.0 (also worth mentioning in documentation, because spec. 2.0 exists

too). In this patch this field contains only USB_DT_AC_HEADER_LENGH

which is totally wrong. This all magically works in Linux, though,

but making Linux-only solution here is wrong, IMHO.

Just my $0.05.

 

Follow-ups

 

--- Mike Frysinger                                           2009-09-16 19:20:00

while we should get this fixed, the driver has been merged into mainline ...

 

--- Cliff Cai                                                2009-11-30 04:27:13

all the problems mentioned above are fixed.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes