[#5260] test 10 fails for gadget_fs control test on bf548/bf527

Document created by Aaronwu Employee on Sep 4, 2013
Version 1Show Document
  • View in full screen mode

[#5260] test 10 fails for gadget_fs control test on bf548/bf527

Submitted By: Vivi Li

Open Date

2009-06-16 06:12:44    

Priority:

Low     Assignee:

Bob Liu

Status:

Open     Fixed In Release:

N/A

Found In Release:

2009R1.1-RC4     Release:

Category:

Tests     Board:

N/A

Processor:

ALL     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Out of Date

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.1_09r1-rc7

App binary format:

N/A     

Summary: test 10 fails for gadget_fs control test on bf548/bf527

Details:

 

test 10 fails for gadget_fs control test on bf548/bf527, for both DMA and PIO.

 

--

sudo ./src/testusb -D /proc/bus/usb/002/125 -t10

unknown speed   /proc/bus/usb/002/125

/proc/bus/usb/002/125 test 10 --> 33 (Numerical argument out of domain)

--

 

Follow-ups

 

--- Cliff Cai                                                2009-06-17 06:15:11

it works for me, it seems that your PC linux doesn't support this test.

 

Cliff

 

--- Vivi Li                                                  2009-06-18 02:30:32

I think the test machine need to update kernel to the latest.

 

--- Vivi Li                                                  2009-06-18 02:37:59

Disable test 10 until kernel is updated to 2.6.26 in host PC.

 

--- Bob Liu                                                  2010-07-13 00:00:15

It works with kernel 2.6.31 in host PC.

 

root@adam-desktop:~/usb# ./testusb -D /proc/bus/usb/002/013 -t10

unknown speed    /proc/bus/usb/002/013

/proc/bus/usb/002/013 test 10,    1.743668 secs

root@adam-desktop:~/usb#

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes