[#5259] at13 test case fails for gadget_fs bulk test on bf548/bf527

Document created by Aaronwu Employee on Sep 4, 2013
Version 1Show Document
  • View in full screen mode

[#5259] at13 test case fails for gadget_fs bulk test on bf548/bf527

Submitted By: Vivi Li

Open Date

2009-06-16 04:58:56     Close Date

2009-06-17 03:15:39

Priority:

Medium High     Assignee:

Cliff Cai

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

Tests     Board:

N/A

Processor:

ALL     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Rejected

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.1_09r1-rc7

App binary format:

N/A     

Summary: at13 test case fails for gadget_fs bulk test on bf548/bf527

Details:

 

at13 test case will fail for gadget_fs bulk test on bf548/bf527, for both dma and pio mode.

 

On host PC:

--

test@uclinux62-548-usbdev:~/uclinux-dist/testsuites/usbdev> sudo ./src/testusb -D /proc/bus/usb/002/056 -at13

unknown speed   /proc/bus/usb/002/056

/proc/bus/usb/002/056 test 13 --> 32 (Broken pipe)

--

 

Error message on target board:

--

write: Broken pipe

get fifo status: Invalid argument

--

 

Follow-ups

 

--- Cliff Cai                                                2009-06-17 02:41:35

Don't do this test for gadget_fs.the gadget_fs tests always try to write or read

someting to/from usb device,while "-t13" means to halt the endpoint.So

doing this test always returns EPIPE.

 

Cliff  

 

--- Vivi Li                                                  2009-06-17 03:15:39

OK, as test 13 is not supported for gadget fs, I have disabled it.

Close it.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes