[#5190] [ltp] sysctl01, sysctl03, sysctl04 fail since 2009.4.1

Document created by Aaronwu Employee on Sep 3, 2013
Version 1Show Document
  • View in full screen mode

[#5190] [ltp] sysctl01, sysctl03, sysctl04 fail since 2009.4.1

Submitted By: Sonic Zhang

Open Date

2009-06-02 04:20:52     Close Date

2009-06-04 04:14:33

Priority:

Medium     Assignee:

Vivi Li

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

ALL     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Assigned (Not Start)

Uboot version or rev.:

    Toolchain version or rev.:

09-r1

App binary format:

N/A     

Summary: [ltp] sysctl01, sysctl03, sysctl04 fail since 2009.4.1

Details:

 

ltp test case sysctl01, sysctl03, sysctl04 fail since 2009.4.1

 

************** STEP 2906: Start to test [sysctl01]

 

 

************** STEP 2907: get test case [sysctl01] from server

 

^M

root:/bin>

************** STEP 2908: execute [sysctl01] ...

 

sysctl01^M

warning: process `sysctl01' used the deprecated sysctl system call with 1.1.^M

swsctl01    1  FAIL  :  sysctl(2) failed u

---fail

nexpectedly errno:38arning: process `sysctl01' used the deprecated sysctl system call with ^M

1.2.^M

sysctl01    2  FAIL  :  sysctl(2) fai

---fail

led unexpectedly errno:38^M

sysctl01    3  FAIL  :  sysctl(2) failed unex

---fail

pectedly errno:38^M

root:/bin>

---done

 

************** STEP 2909: goto test_cleanup

 

 

sending marker

echo 1239258967^M

 

got marker back

1239258967^M

root:/bin>

got marker back

 

got kernel prompt

 

************** STEP 2910: remove testcase done

 

rm -f /bin/sysctl01^M

root:/bin> ^M

root:/bin>

System is fine.

 

===== Recording result: sysctl01 is FAIL

 

Follow-ups

 

--- Mike Frysinger                                           2009-06-02 04:24:12

we disable sysctl in our defconfigs on purpose:

# CONFIG_SYSCTL_SYSCALL is not set

 

this isnt a function should care about ...

 

--- Sonic Zhang                                              2009-06-03 06:00:56

Vivi should disable sysctl test cases in LTP since we don't support

CONFIG_SYSCTL_SYSCALL in kernel by default.

 

--- Vivi Li                                                  2009-06-04 04:14:33

OK, disable sysctl test.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes