[#5189] [ltp] fcntl14 case 21 fails since 2009.5.8

Document created by Aaronwu Employee on Sep 3, 2013
Version 1Show Document
  • View in full screen mode

[#5189] [ltp] fcntl14 case 21 fails since 2009.5.8

Submitted By: Sonic Zhang

Open Date

2009-06-02 04:00:46     Close Date

2009-07-14 02:31:24

Priority:

Medium     Assignee:

Sonic Zhang

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

ALL     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

09-r1

App binary format:

N/A     

Summary: [ltp] fcntl14 case 21 fails since 2009.5.8

Details:

 

ltp test case fcntl14 fails in WB cache mode since 2009.5.8

 

 

************** STEP 701: Start to test [fdatasync01]

 

 

************** STEP 702: get test case [fdatasync01] from server

 

^M

root:/bin> The child didnot terminate on it

************** STEP 703: execute [fdatasync01] ...

 

s own accord: No such file or directory^M

fcntl14     0  INFO  :  Pause terminated without signal SIGUSR1 from child^M

fcntl14    35  FAIL  :  tchild returne

---fail

d status 0x100^M

fcntl14    36  FAIL  :  testcase

---fail

:34 FAILED^M

fcntl14

---fail

0  WARN  :  tst_rmdir(): rmobj(/tmp/fcnvf7yYI) failed: lstat(/tmp/fcnvf7yYI) failed; errno=2: No such file or directory^M

fdatasync01^M

fdatasync01    1  PASS  :  fdatasync() successful^M

root:/bin>

---done

 

************** STEP 704: goto test_cleanup

 

 

sending marker

echo 1243719077^M

 

got marker back

1243719077^M

root:/bin>

got marker back

 

got kernel prompt

 

************** STEP 705: remove testcase done

 

rm -f /bin/fdatasync01^M

root:/bin> ^M

root:/bin>

System is fine.

 

===== Recording result: fdatasync01 is FAIL

 

Follow-ups

 

--- Sonic Zhang                                              2009-06-04 04:59:37

fcntl14    13  PASS

got marker back

:  testcase:13 PASSED^M

root:~>

got kernel prompt

fcntl14    14  PASS  :  testcase:14 PASSED^M

fcntl14    15  PASS  :  testcase:15 PASSED^M

fcntl14    16  PASS  :  testcase:16 PASSED^M

fcntl14    17  PASS  :  testcase:17 PASSED^M

fcntl14    18  PASS  :  testcase

************** STEP 644: remove testcase done

 

:18 PASSED^M

fcntl14    19  PASS  :  testcase:19 PASSED^M

rm -f /bin/fcntl14^M

root:~> ^M

root:~> fcntl14    20  PASS  :  testcase:20 PASSED^M

fcntl14    21  FAIL  :  self_exec failed^M

 

************** STEP 645: System abnormal

 

 

---System abnormal

 

!!!! recovering

 

!!!! hit ENTER

 

===== Recording result: fcntl14 is LTP test never ran

 

 

--- Sonic Zhang                                              2009-06-04 06:10:22

fcntl14 cause msh relaunch.

 

fcntl14     0  INFO  :  Enter block 1: without mandatory locking

 

 

BusyBox v1.13.4 (2009-06-04 17:49:13 CST) built-in shell (msh)

Enter 'help' for a list of built-in commands.

root:/> fcntl14     1  PASS  :  testcase:1 PASSED

fcntl14     2  PASS  :  testcase:2 PASSED

fcntl14     3  PASS  :  testcase:3 PASSED

fcntl14     4  PASS  :  testcase:4 PASSED

fcntl14     5  PASS  :  testcase:5 PASSED

fcntl14     6  PASS  :  testcase:6 PASSED

fcntl14     7  PASS  :  testcase:7 PASSED

 

--- Sonic Zhang                                              2009-06-05 05:32:15

Fixed.

 

--- Vivi Li                                                  2009-07-14 02:31:24

OK now. Close it.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes