[#5164] shell prompt become # on trunk head

Document created by Aaronwu Employee on Sep 3, 2013
Version 1Show Document
  • View in full screen mode

[#5164] shell prompt become # on trunk head

Submitted By: Mingquan Pan

Open Date

2009-05-26 05:21:03     Close Date

2009-05-27 02:16:48

Priority:

Medium     Assignee:

Mike Frysinger

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2010R1     Release:

Category:

N/A     Board:

N/A

Processor:

ALL     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

09r1-rc6

App binary format:

N/A     

Summary: shell prompt become # on trunk head

Details:

 

shell prompt become # on trunk head  instead of root:/> after updating over the weekend.

 

## Booting kernel from Legacy Image at 02000000 ...

   Image Name:   Linux-2.6.28.10-ADI-2010R1-pre-s

   Created:      2009-05-26   8:15:48 UTC

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    4119582 Bytes =  3.9 MB

   Load Address: 00001000

   Entry Point:  001896dc

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 001896dc

Linux version 2.6.28.10-ADI-2010R1-pre-svn6473 (test@uclinux75-bf533-stamp-wb) (gcc version 4.1.2 (ADI svn)) #189 Tue May 26 16:15:33 CST 2009

Warning: limiting memory to 56MB due to hardware anomaly 05000263

Board Memory: 128MB

Kernel Managed Memory: 128MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x0010be30

  rodata    = 0x0010be30-0x0015ebb4

  bss       = 0x0015f000-0x0016f458

  data      = 0x0016f458-0x0017e000

    stack   = 0x0017c000-0x0017e000

  init      = 0x0017e000-0x007cf000

  available = 0x007cf000-0x037ff000

  DMA Zone  = 0x07f00000-0x08000000

Hardware Trace Active and Enabled

Boot Mode: 0

Reset caused by Software reset

Blackfin support (C) 2004-2009 Analog Devices, Inc.

Compiled for ADSP-BF533 Rev 0.3

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 398 MHz core clock and 79 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

Data Cache Enabled for CPU0 (write-back)

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 14223

Kernel command line:

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 256 (order: 8, 1024 bytes)

bfin-rtc: invalid date; resetting

console [ttyBF0] enabled

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 48776k/131072k RAM, (6468k init code, 1067k kernel code, 457k data, 1024k dma, 73280k reserved)

Calibrating delay loop... 792.57 BogoMIPS (lpj=1585152)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (15 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 64 KB (53 KB free)

net_namespace: 288 bytes

NET: Registered protocol family 16

Blackfin DMA Controller

stamp_init(): registering device resources

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

NET: Registered protocol family 1

msgmni has been set to 95

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc00400 (irq = 21) is a BFIN-UART

brd: module loaded

smc91x.c: v1.1, sep 22 2004 by Nicolas Pitre <nico@cam.org>

eth0: SMC91C11xFD (rev 1) at 20300300 IRQ 40 [nowait]

eth0: Ethernet addr: f2:06:01:61:68:b5

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@5

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 1970-01-01 10:42:38 UTC (38558)

Freeing unused kernel memory: 6468k freed

dma_alloc_init: dma_page @ 0x007cc000 - 256 pages at 0x07f00000

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            - http://blackfin.uclinux.org/

\    YP"    `| 8P  `.          - http://docs.blackfin.uclinux.org/

/     \.___.d|    .'           - http://www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    - http://www.analog.com/blackfin

 

Have a lot of fun...

 

 

BusyBox v1.14.0 (2009-05-26 15:12:17 CST) hush - the humble shell

Enter 'help' for a list of built-in commands.

 

/ # version

kernel:    Linux release 2.6.28.10-ADI-2010R1-pre-svn6473, build #189 Tue May 26 16:15:33 CST 2009

toolchain: bfin-uclinux-gcc release gcc version 4.1.2 (ADI svn)

user-dist: release svn-8133, build #1288 Tue May 26 16:14:29 CST 2009

/ #

************** STEP 3: Start SERIAL TEST

 

 

Follow-ups

 

--- Mike Frysinger                                           2009-05-26 05:25:53

thought i fixed that, but guess i'll double check

 

--- Mike Frysinger                                           2009-05-26 16:43:16

yeah, i cant reproduce this.  current trunk installs an /etc/profile which all

login shells source and that sets the PS1 variable.

 

--- Mike Frysinger                                           2009-05-26 18:16:29

mmm nm, i had fixed this upstream but didnt put the fix in our local version.

ive done that now.

 

--- Mingquan Pan                                             2009-05-27 02:16:48

Yes, it is back to normal. Close.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes