[#5159] boa 120 sec timeout error

Document created by Aaronwu Employee on Sep 3, 2013
Version 1Show Document
  • View in full screen mode

[#5159] boa 120 sec timeout error

Submitted By: Dominik Herwald

Open Date

2009-05-25 05:02:39    

Priority:

Low     Assignee:

Nobody

Status:

Open     Fixed In Release:

N/A

Found In Release:

2010R1     Release:

SVN

Category:

Networking     Board:

N/A

Processor:

ALL     Silicon Revision:

0.1

Is this bug repeatable?:

Yes     Resolution:

N/A

Uboot version or rev.:

    Toolchain version or rev.:

SVN

App binary format:

N/A     

Summary: boa 120 sec timeout error

Details:

 

120 seconds after boa is started with boa -f /etc/boa.conf

(no change was made to boa.conf (from vendors/bluetechnix) )

an error message appears:

INFO: task boa:44 blocked for more than 120 seconds.

... (stack trace - s. forum thread)

 

Apart from that Boa is working fine.

 

s.

https://blackfin.uclinux.org/gf/project/uclinux-dist/forum/?_forum_action=ForumMessageBrowse&thread_id=33092&action=ForumBrowse&forum_id=39

 

(This thread did not get updated in the main thread list  when I posted a followup so it is still on page 3 where nobody notices it, thus I opened this tracker item)

 

 

Follow-ups

 

--- Robin Getz                                               2009-05-25 19:05:41

Dominik:

 

We don't support the bluetechnix boards (that is why it was not answered) - can

you re-create on a EZKit or STAMP? If not - you will need to go to bluetechnix

for help.

 

-Robin

 

--- Dominik Herwald                                          2009-05-26 02:55:43

Hello Robin,

 

OK I understand that, but I did NOT start the mentioned thread! It was Daniele

Pagani - he did not specify which board he uses but it's a BF537 based one.

I use a BF548.

 

Anyway I checked boa.conf from the Ezkit and it is exactly the same. I guess

Bluetechnix just copied all that stuff from vendors/AnalogDevices.

 

I can try a BF533 Stamp Board later on if you want but I did not use it for

quite some time now ... ;-)

 

Regards,

Dominik

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes