[#5151] coreb test fails on 561

Document created by Aaronwu Employee on Sep 3, 2013
Version 1Show Document
  • View in full screen mode

[#5151] coreb test fails on 561

Submitted By: Vivi Li

Open Date

2009-05-20 22:31:25     Close Date

2009-06-10 05:11:22

Priority:

Medium High     Assignee:

Mike Frysinger

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

Drivers     Board:

N/A

Processor:

BF561     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.1-09r1_rc6

App binary format:

N/A     

Summary: coreb test fails on 561

Details:

 

coreb test fails on 561 and file coreb_status is also missing.

 

Config is attached and bellow is the log:

--

root:/> ls /sys/class/misc/coreb/coreb_status

ls: /sys/class/misc/coreb/coreb_status: No such file or directory

root:/> ls /sys/class/misc/coreb/

dev        subsystem  uevent

root:/> modprobe dualcore_test

dualcore_test: module license 'unspecified' taints kernel.

Dual core test module inserted: set testarg = [1]

@ [feb1fffc]

root:/> corebld /usr/coreb/test_cpp

writing to 0xfeb00000, 0xc9f0    bytes: OK

 

ERROR: Your destination address looks wrong: 0xff400000

This seems to be Core A L1 memory; aborting.

(re-run with --force to skip this check)

 

writing to 0xff400000, 0x4       bytes: FAILED

 

ERROR: Your destination address looks wrong: 0xff600000

This seems to be Core A L1 memory; aborting.

(re-run with --force to skip this check)

 

writing to 0xff600000, 0xa       bytes: FAILED

root:/> modprobe -r dualcore_test

Dual core test module removed: testarg = [1]

root:/>

root:/> corebld /usr/coreb/test_c

 

ERROR: Your destination address looks wrong: 0xff400000

This seems to be Core A L1 memory; aborting.

(re-run with --force to skip this check)

 

writing to 0xff400000, 0x89c     bytes: FAILED

 

ERROR: Your destination address looks wrong: 0xff600000

This seems to be Core A L1 memory; aborting.

(re-run with --force to skip this check)

 

writing to 0xff600000, 0xea4     bytes: FAILED

root:/>

--

 

Follow-ups

 

--- Mike Frysinger                                           2009-05-21 14:17:25

should be fixed now

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

config.coreb    application/octet-stream    26937    Vivi Li

Attachments

Outcomes