[#5139] XIP kernel can not boot up in bf537-stamp with MPU enabled

Document created by Aaronwu Employee on Sep 3, 2013
Version 1Show Document
  • View in full screen mode

[#5139] XIP kernel can not boot up in bf537-stamp with MPU enabled

Submitted By: Vivi Li

Open Date

2009-05-19 03:16:29     Close Date

2009-07-12 23:46:30

Priority:

Medium High     Assignee:

Bernd Schmidt

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

BF537     Silicon Revision:

bf537-0.3

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.1-09r1_rc6

App binary format:

N/A     

Summary: XIP kernel can not boot up in bf537-stamp with MPU enabled

Details:

 

XIP kernel can not boot up in bf537-stamp with MPU enabled. Some application crashed during boot up procedure.

CPU revision is 0.3, and it both failed for FDPIC and shared-flat formats.

Kernel config file is attached.

 

Bellow is the log for FDPIC format:

--

U-Boot 2008.10-svn1868 (ADI-2009R1-rc1) (May 19 2009 - 14:39:13)

 

CPU:   ADSP bf537-0.3 (Detected Rev: 0.3) (bypass boot)

Board: ADI BF537 stamp board

       Support: http://blackfin.uclinux.org/

Clock: VCO: 500 MHz, Core: 500 MHz, System: 125 MHz

RAM:   64 MB

Flash:  4 MB

In:    serial

Out:   serial

Err:   serial

Net:   Blackfin EMAC

MAC:   00:E0:22:FE:58:9C

Hit any key to stop autoboot:  0

bfin> set bootargs root=mtd0 rootfstype=romfs ro

bfin> tftpboot 0x1000000 uImage.romfs

Using Blackfin EMAC device

TFTP from server 10.100.4.174; our IP address is 10.100.4.50

Filename 'uImage.romfs'.

Load address: 0x1000000

Loading: #################################################################

         #################################################################

         #################################################################

         #################################################################

         ############

done

Bytes transferred = 3989470 (3cdfde hex)

bfin> bootm

## Booting kernel from Legacy Image at 01000000 ...

   Image Name:   Linux Kernel and romfs

   Created:      2009-05-18  20:08:55 UTC

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    3989406 Bytes =  3.8 MB

   Load Address: 00001000

   Entry Point:  001864ec

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 001864ec

Linux version 2.6.28.10-ADI-2009R1-pre-svn6363 (test@uclinux74-mpu) (gcc version 4.1.2 (ADI svn)) #133 Mon May 18 20:02:51 GMT 29

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x001040d0

  rodata    = 0x001040d0-0x00155a4c

  bss       = 0x00156000-0x001676b0

  data      = 0x001676b0-0x00178000

    stack   = 0x00176000-0x00178000

  init      = 0x00178000-0x00197000

  available = 0x00197000-0x038be000

  rootfs    = 0x038be000-0x03f00000

  DMA Zone  = 0x03f00000-0x04000000

Hardware Trace Active and Enabled

Boot Mode: 0

Reset caused by Software reset

Blackfin support (C) 2004-2009 Analog Devices, Inc.

Compiled for ADSP-BF537 Rev 0.3

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 500 MHz core clock and 125 MHz System Clock

MPU: setting up cplb tables with memory protection

Instruction Cache Enabled for CPU0

Data Cache Enabled for CPU0 (write-back)

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 14412

Kernel command line: root=mtd0 rootfstype=romfs ro

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 256 (order: 8, 1024 bytes)

console [ttyBF0] enabled

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 53440k/65536k RAM, (124k init code, 1036k kernel code, 464k data, 1024k dma, 3040k reserved)

Calibrating delay loop... 997.37 BogoMIPS (lpj=1994752)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (15 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (38 KB free)

PDA for CPU0 reserved at 00159000

net_namespace: 288 bytes

NET: Registered protocol family 16

Blackfin DMA Controller

stamp_init(): registering device resources

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

NET: Registered protocol family 1

ROMFS MTD (C) 2006 Red Hat, Inc.

msgmni has been set to 104

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART

brd: module loaded

bfin_mii_bus: probed

bfin_mac: attached PHY driver [SMSC LAN83C185] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=24)@sclk=125MHz)

bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1

uclinux[mtd]: RAM probe address=0x38be000 size=0x641d30

Creating 1 MTD partitions on "RAM":

0x00000000-0x00641d30 : "ROMfs"

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@7

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 2004-06-01 03:12:27 UTC (1086059547)

ROMFS: Mounting image 'rom 4a11c054'

VFS: Mounted root (romfs filesystem) readonly.

dma_alloc_init: dma_page @ 0x0050c000 - 256 pages at 0x03f00000

Data access CPLB miss

- Used by the MMU to signal a CPLB miss on a data access.

Deferred Exception context

CURRENT PROCESS:

COMM=init PID=1

CPU = 0

TEXT = 0x03a97cc0-0x03a9a4c8        DATA = 0x0387e808-0x0387ebbc

BSS = 0x0387ebbc-0x00520000  USER-STACK = 0x0053fef0

 

return address: [0x03dad470]; contents of:

0x03dad450:  321d  e410  ffff  e3ff  b3d1  640f  09b7  1ff3

0x03dad460:  321d  e801  0000  3044  05ac  e2ff  b3c7  0000

0x03dad470: [e519] 0037  04c5  e800  0003  e50a  ffff  0c7a

0x03dad480:  180b  0000  3269  6fc5  0000  9151  ac53  0061

 

SEQUENCER STATUS:               Not tainted

SEQSTAT: 00062026  IPEND: 0030  SYSCFG: 0006

  EXCAUSE   : 0x26

  interrupts disabled

  physical IVG5 asserted : <0xffa00b6c> { _evt_ivhw + 0x0 }

RETE: <0x00000000> { _do_one_initcall + 0xfffff000 }

RETN: <0x038ae000> /* kernel dynamic memory */

RETX: <0xffa0058c> { _exception_to_level5 + 0x0 }

RETS: <0x03da3a3e> [ /lib/libgcc_s.so.1 + 0x1f4e ]

PC  : <0x03dad470> [ /lib/libgcc_s.so.1 + 0xb980 ]

DCPLB_FAULT_ADDR: <0x0015bffc> /* kernel dynamic memory */

ICPLB_FAULT_ADDR: <0x03dad470> [ /lib/libgcc_s.so.1 + 0xb980 ]

 

PROCESSOR STATE:

R0 : 00000000    R1 : 00000000    R2 : 00000000    R3 : 00000002

R4 : 00504144    R5 : 00504178    R6 : 00504458    R7 : 03da3a2c

P0 : 005043e0    P1 : 03dab9ac    P2 : 00517324    P3 : 00517608

P4 : 00000002    P5 : 03873290    FP : 0053fabc    SP : 038adf24

LB0: 03db49f1    LT0: 03db49e4    LC0: 00000000

LB1: 03db3e6b    LT1: 03db3e6a    LC1: 00000000

B0 : 00000000    L0 : 00000000    M0 : 00000000    I0 : 0053fa25

B1 : 00000000    L1 : 00000000    M1 : 00000000    I1 : 005041b0

B2 : 00000000    L2 : 00000000    M2 : 00000000    I2 : 00000000

B3 : 00000000    L3 : 00000000    M3 : 00000000    I3 : 00000000

A0.w: 00000000   A0.x: 00000000   A1.w: 00000000   A1.x: 00000000

USP : 0053fab0  ASTAT: 00003025

 

No trace since you do not have CONFIG_DEBUG_BFIN_NO_KERN_HWTRACE enabled

 

Userspace Stack

Stack info:

SP: [0x0053fab0] <0x0053fab0> [ init + 0x1fab0 ]

FP: (0x0053fabc)

Memory from 0x0053fab0 to 00540000

0053fab0:[038733c8] 00000003  038733ac (0053fcf8)<03db4048> 00517608  03db527c  038734c8

0053fad0: 0053ffb0  0387ea88  00000000  00000000 <03da31a2> 00000000  038733c8  03db6136

0053faf0: 00000000  038733c8  03a988c9  0053fb08  038733c8  03a988bb  0053fb14  03873290

0053fb10: 03a98877  00000000  03873158  00000000  00000000  03873028  00000000  00504148

0053fb30: 03db5694  03db5180  00504144  00000000  00000000  005043e0  005043c4  005043d4

0053fb50: 0050445c  00504400  00504404  00504140  0053fb04  03db5694  03db5288  03db5694

0053fb70: 03db5208  03db51d8  00000000  00000000  00000000  0053fe50  03a97cc0  00000000

0053fb90: 00000000  00000000  03873000  00000000  00000000  0053ff90  00504178  0053ffb0

0053fbb0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

0053fbd0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

0053fbf0: 00000000  00000335  00000190  0387ea88  03a97dc8  03a98594  03a98034  00000000

0053fc10: 00000000  00000000  0000036d  00000010  00000f00  000024a0  00000000  00000000

0053fc30: 00000000  03a989d0  000001f0  00000008  00000011  00000000  00000000  03a98a30

0053fc50: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

0053fc70: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

0053fc90: 00000000  00000000  00000000  00001f00  004f0680  000181ed  00000000  00000000

0053fcb0: 00007688  00000400  00000000  00000000  00000000  00000000  00000000  00000000

0053fcd0: 00000000  00000000  00000000  03da3a2c  00517608  00000000  00000000  00000000

0053fcf0: 00000000  038735f0 (0053feb0)<03db487a> 0053ff90  000005c0  0000b020  00000002

0053fd10: 00000512  00504178  0053fd48  0053ff90  00504178  0053fe38  0053fefc  0053fef4

0053fd30: 0053ffb0  00504178  0053ff90  00504178  0053fef4  0053fefc  0053ff90  00504178

0053fd50: 03a97db4  005040a8  00000000  00000000  00000000  00000000  00000000  00000000

0053fd70: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

0053fd90: 00000000  00000000  00504178  03dae774  03daee14  03dae9a4  00000000  00000000

0053fdb0: 00000000  00000429  00000010  00000000  00000000  0000040e  00000000  00000000

0053fdd0: 03daf240  000005c0  00000008  00000000  00000000  00000000  00000000  00000001

0053fdf0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

0053fe10: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

0053fe30: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

0053fe50: 00000003  03a97cf4  00000004  00000020  00000005  00000006  00000006  00001000

0053fe70: 00000007  03dae6a0  00000008  00000000  00000009  03a98f08  00000000  00000000

0053fe90: 0000000b  00000000  0000000c  00000000  0000000d  00000000  0000000e  00000000

0053feb0:(00000000)<03daf850> 00504178  00000000  005040a8  0053ff90  0053ffb0 <03daf804>

0053fed0: 00504178  0053ffb0  00000000  005040a8  0053fee8  0053fef0  00000000  00000000

0053fef0: 00000001  0053ffd4  00000000  0053ffdf  0053ffe6  00000000  00000010  00000000

0053ff10: 00000006  00001000  00000011  00000064  00000003  03a97cf4  00000004  00000020

0053ff30: 00000005  00000006  00000007  03dae6a0  00000008  00000000  00000009  03a98f08

0053ff50: 0000000b  00000000  0000000c  00000000  0000000d  00000000  0000000e  00000000

0053ff70: 00000017  00000000  0000001f  0001fff1  00000000  00000000  00000000  00000000

0053ff90: 00020000  03dae6a0  00000000  0000701c  0050401c  0000b01c  00000450  00000000

0053ffb0: 00020000  03a97cc0  00000000  00002808  0387e808  00006808  000003b4  00000000

0053ffd0: 00000000  6962732f  6e692f6e  48007469  3d454d4f  4554002f  6c3d4d52  78756e69

0053fff0: 62732f00  692f6e69  0074696e  00000000  4bdecfa9

Return addresses in stack:

   frame  1 : <0x03db4048> [ /lib/ld-uClibc.so.0 + 0x59a8 ]

    address : <0x03da31a2> [ /lib/libgcc_s.so.1 + 0x16b2 ]

   frame  2 : <0x03db487a> [ /lib/ld-uClibc.so.0 + 0x61da ]

   frame  3 : <0x03daf850> [ /lib/ld-uClibc.so.0 + 0x11b0 ]

    address : <0x03daf804> [ /lib/ld-uClibc.so.0 + 0x1164 ]

Kernel panic - not syncing: Attempted to kill init!

--

 

Follow-ups

 

--- Bernd Schmidt                                            2009-05-19 04:47:05

When did this start happening?  Are there known good recent kernel and toolchain

versions?

 

--- Vivi Li                                                  2009-05-19 06:37:52

Sorry I don't have ...

 

--- Sonic Zhang                                              2009-05-19 23:36:16

Current logs on that machine shows kernel building for MPU failed since last

release. After the building issue was solved on 2008-9-9, the XIP test always

fails till now.

 

--- Bernd Schmidt                                            2009-05-20 05:02:45

That can't be right.  I seem to remember fixing build and other errors in that

period of time - for example bug 4616.

If it fails since 2008-09-09, why hasn't anyone opened a bug _then_?

 

--- Sonic Zhang                                              2009-05-20 05:13:14

MPU related regressions all run on one of the 40 testing machines. Vivi forgot

to take a look at it since 2008R1.5 release. I am working on a check list to

avoid this kind of issues.

 

 

--- Vivi Li                                                  2009-06-05 05:04:39

It still fails on test machine.

 

--- Vivi Li                                                  2009-06-05 05:32:36

other test cases used to pass now also fail after 2009_May_20.

for example, dll test:

--

./test_dll^M

Data access CPLB protection violation^M

- Attempted read or write to Supervisor resource,^M

   or illegal data memory access. ^M

Deferred Exception context^M

CURRENT PROCESS:^M

COMM=test_dll PID=169^M

CPU = 0^M

TEXT = 0x03edb000-0x03edb9f8        DATA = 0x03e949f8-0x03e94b98^M

BSS = 0x03e94b98-0x030e0000  USER-STACK = 0x030ffec0^M

^M

return address: [0x030cbbe2]; contents of:^M

0x030cbbc0:  bbdb  e3ff  fef3  0c00  b9db  17d8  e51a  0015 ^M

0x030cbbd0:  63e9  9114  3004  67f8  0a08  145b  320c  303c ^M

0x030cbbe0:  6487 [accc] 320f  5ca4  5e51  3215  bbf9  9110 ^M

0x030cbbf0:  0c00  1814  e120  011b  b0f0  e51a  000a  e418 ^M

^M

ADSP-BF537-0.3 500(MHz CCLK) 125(MHz SCLK) (mpu on)^M

Linux version 2.6.28.10-ADI-2009R1-svn6523^M

Built with gcc version 4.1.2 (ADI svn)^M

^M

SEQUENCER STATUS:               Not tainted^M

SEQSTAT: 00062023  IPEND: 0030  SYSCFG: 0006^M

  EXCAUSE   : 0x23^M

  interrupts disabled^M

  physical IVG5 asserted : <0xffa00bb8> { _evt_ivhw + 0x0 }^M

RETE: <0x00000000> /* Maybe null pointer? */^M

RETN: <0x030c6000> /* kernel dynamic memory */^M

RETX: <0x00000480> /* Maybe fixed code section */^M

RETS: <0x030cd480> [ /lib/ld-uClibc.so.0 + 0x5480 ]^M

PC  : <0x030cbbe2> [ /lib/ld-uClibc.so.0 + 0x3be2 ]^M

DCPLB_FAULT_ADDR: <0x030c5d78> /* kernel dynamic memory */^M

ICPLB_FAULT_ADDR: <0x0008a174> { _sprintf + 0x0 }^M

^M

PROCESSOR STATE:^M

R0 : 00caffff    R1 : fffffffd    R2 : 0000002f    R3 : 00000000^M

R4 : 00cb0000    R5 : 03e953e0    R6 : 03edb3e9    R7 : 00cb0010^M

P0 : 03e953e0    P1 : 00cb0000    P2 : 03e95410    P3 : 03e95178^M

P4 : 03e95178    P5 : 03e953c0    FP : 030ffaa8    SP : 030c5f24^M

LB0: 03b8cc03    LT0: 03b8cc02    LC0: 00000000^M

LB1: 030caea5    LT1: 030caea4    LC1: 00000000^M

B0 : 00000000    L0 : 00000000    M0 : 00000000    I0 : 000005c0^M

B1 : 00000000    L1 : 00000000    M1 : 00000000    I1 : 03e951b0^M

B2 : 00000000    L2 : 00000000    M2 : 00000000    I2 : 00000000^M

B3 : 00000000    L3 : 00000000    M3 : 00000000    I3 : 00000000^M

A0.w: 00000000   A0.x: 00000000   A1.w: 00000000   A1.x: 00000000^M

USP : 030ffa88  ASTAT: 02002020^M

^M

Hardware Trace:^M

   0 Target : <0x00004c8c> { _trap_c + 0x0 }^M

     Source : <0xffa0062a> { _exception_to_level5 + 0x9e } CALL pcrel^M

   1 Target : <0xffa0058c> { _exception_to_level5 + 0x0 }^M

     Source : <0xffa00470> { _bfin_return_from_exception + 0x18 } RTX^M

   2 Target : <0xffa00458> { _bfin_return_from_exception + 0x0 }^M

     Source : <0xffa004e6> { _ex_trap_c + 0x46 } JUMP.S^M

   3 Target : <0xffa0069c> { _trap + 0x0 }^M

     Source : <0xffa00408> { _ex_dcplb_miss + 0x78 } RTX^M

   4 Target : <0xffa00390> { _ex_dcplb_miss + 0x0 }^M

     Source : <0xffa006f5> { _trap + 0x59 } ^M

   5 Target : <0xffa0069c> { _trap + 0x0 }^M

     Source : <0x030cbbe0> [ /lib/ld-uClibc.so.0 + 0x3be0 ] 0x6487^M

   6 Target : <0x030cbbcc> [ /lib/ld-uClibc.so.0 + 0x3bcc ]^M

     Source : <0x030cbb8a> [ /lib/ld-uClibc.so.0 + 0x3b8a ] IF !CC

JUMP^M

   7 Target : <0x030cbb82> [ /lib/ld-uClibc.so.0 + 0x3b82 ]^M

     Source : <0x030cbb40> [ /lib/ld-uClibc.so.0 + 0x3b40 ] IF !CC

JUMP^M

   8 Target : <0x030cbb3e> [ /lib/ld-uClibc.so.0 + 0x3b3e ]^M

     Source : <0x030cbb1e> [ /lib/ld-uClibc.so.0 + 0x3b1e ] IF !CC

JUMP^M

   9 Target : <0x030cbb14> [ /lib/ld-uClibc.so.0 + 0x3b14 ]^M

     Source : <0x030cbc8e> [ /lib/ld-uClibc.so.0 + 0x3c8e ] JUMP.S^M

  10 Target : <0x030cbc8c> [ /lib/ld-uClibc.so.0 + 0x3c8c ]^M

     Source : <0x030cbb0e> [ /lib/ld-uClibc.so.0 + 0x3b0e ] IF !CC

JUMP^M

  11 Target : <0x030cbb01> [ /lib/ld-uClibc.so.0 + 0x3b01 ]^M

     Source : <0x030cbb0a> [ /lib/ld-uClibc.so.0 + 0x3b0a ] IF CC JUMP^M

  12 Target : <0x030cbb04> [ /lib/ld-uClibc.so.0 + 0x3b04 ]^M

     Source : <0x030cbafe> [ /lib/ld-uClibc.so.0 + 0x3afe ] JUMP.S^M

  13 Target : <0x030cbae5> [ /lib/ld-uClibc.so.0 + 0x3ae5 ]^M

     Source : <0x030cbaea> [ /lib/ld-uClibc.so.0 + 0x3aea ] IF CC JUMP^M

  14 Target : <0x030cbac8> [ /lib/ld-uClibc.so.0 + 0x3ac8 ]^M

     Source : <0x030cd47c> [ /lib/ld-uClibc.so.0 + 0x547c ] CALL pcrel^M

  15 Target : <0x030cd46a> [ /lib/ld-uClibc.so.0 + 0x546a ]^M

     Source : <0x030cd444> [ /lib/ld-uClibc.so.0 + 0x5444 ] IF !CC

JUMP^M

Userspace Stack^M

Stack info:^M

SP: [0x030ffa88] <0x030ffa88> [ test_dll + 0x1fa88 ]^M

Memory from 0x030ffa80 to 03100000^M

030ffa80: 00000013  00cb0010 [03edb3bd] 03e953e0  00cb0000  4a24c78e  030ffcc4

00cb02fe ^M

030ffaa0: 03e95464  45984f00  030ffcc8 <030cd480> 03e94a14  03e95178

03edb3e9  03ed9028 ^M

030ffac0: 03e95178  00000001  00000000  030ffcc4  00000001  03edb3e9  00000000

00000000 ^M

030ffae0: 03edb3bd  00000000  03ed9158  00000000  00000000  03ed9028  00000000

03e95148 ^M

030ffb00: 030ceff4  030ceae0  03e95144  00000000  00000000  03e953e0  03e953c4

03e953d4 ^M

030ffb20: 03e9545c  03e95400  03e95404  03e95140  030ffad4  00000000  00000000

00000000 ^M

030ffb40: 00000000  030ceb38  00000000  00000000  00000000  030ffe20  03edb000

00000000 ^M

030ffb60: 00000000  00000000  03ed9000  00000000  00000000  030fff60  03e95178

030fff80 ^M

030ffb80: 00000000  00000000  00000000  00000000  00000000  00000000  00000000

00000000 ^M

030ffba0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000

00000000 ^M

030ffbc0: 00000000  000000eb  00000040  03e94b28  03edb108  03edb30c  03edb1ac

00000000 ^M

030ffbe0: 00000000  00000000  00000118  00000010  000004e8  00000978  00000000

00000000 ^M

030ffc00: 00000000  03edb470  00000078  00000008  00000011  00000000  00000000

03edb4a8 ^M

030ffc20: 00000000  00000000  00000000  00000000  00000000  00000000  00000000

00000000 ^M

030ffc40: 00000000  00000000  00000000  00000000  00000000  00000000  00000000

00000000 ^M

030ffc60: 00000000  00000000  00000000  00000000  00000000  00000000  00000000

00000000 ^M

030ffc80: 00000000  00000000  00000000  00000000  00000000  00000000  00000000

00000000 ^M

030ffca0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000

00000000 ^M

030ffcc0: 00000000  03ed9258  030ffe80 <030ce1da> 030fff60  000005c0

0000b020  00000002 ^M

030ffce0: 00000512  03e95178  030ffd18  030fff60  03e95178  030ffe08  030ffecc

030ffec4 ^M

030ffd00: 030fff80  03e95178  030fff60  03e95178  030ffec4  030ffecc  030fff60

03e95178 ^M

030ffd20: 03edb0f4  03e950a8  00000000  00000000  00000000  00000000  00000000

00000000 ^M

030ffd40: 00000000  00000000  00000000  00000000  00000000  00000000  00000000

00000000 ^M

030ffd60: 00000000  00000000  03e95178  030c80d4  030c8774  030c8304  00000000

00000000 ^M

030ffd80: 00000000  00000429  00000010  00000000  00000000  0000040e  00000000

00000000 ^M

030ffda0: 030c8ba0  000005c0  00000008  00000000  00000000  00000000  00000000

00000001 ^M

030ffdc0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000

00000000 ^M

030ffde0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000

00000000 ^M

030ffe00: 00000000  00000000  00000000  00000000  00000000  00000000  00000000

00000000 ^M

030ffe20: 00000003  03edb034  00000004  00000020  00000005  00000006  00000006

00001000 ^M

030ffe40: 00000007  030c8000  00000008  00000000  00000009  03edb590  00000000

00000000 ^M

030ffe60: 0000000b  00000000  0000000c  00000000  0000000d  00000000  0000000e

00000000 ^M

030ffe80: 03be8b94 <030c91b0> 03e95178  0308c004  03e950a8  030fff60

030fff80 <030c9164>^M

030ffea0: 03e95178  030fff80  00000000  03e950a8  030ffeb8  030ffec0  00000000

00000000 ^M

030ffec0: 00000001  030fffa3  00000000  030fffae  030fffb5  030fffc3  030fffe6

00000000 ^M

030ffee0: 00000010  00000000  00000006  00001000  00000011  00000064  00000003

03edb034 ^M

030fff00: 00000004  00000020  00000005  00000006  00000007  030c8000  00000008

00000000 ^M

030fff20: 00000009  03edb590  0000000b  00000000  0000000c  00000000  0000000d

00000000 ^M

030fff40: 0000000e  00000000  00000017  00000000  0000001f  0001fff1  00000000

00000000 ^M

030fff60: 00020000  030c8000  00000000  0000701c  03e9501c  0000b01c  00000450

00000000 ^M

030fff80: 00020000  03edb000  00000000  000009f8  03e949f8  000049f8  000001a0

00000000 ^M

030fffa0: 2e000000  7365742f  6c645f74  4f48006c  2f3d454d  45485300  2f3d4c4c

2f6e6962 ^M

030fffc0: 50006873  3d485441  6e69622f  73752f3a  69622f72  732f3a6e  3a6e6962

7273752f ^M

030fffe0: 6962732f  4554006e  6c3d4d52  78756e69  742f2e00  5f747365  006c6c64

00000000 ^M

03100000: 544c4662 ^M

Return addresses in stack:^M

    address : <0x030cd480> [ /lib/ld-uClibc.so.0 + 0x5480 ]^M

    address : <0x030ce1da> [ /lib/ld-uClibc.so.0 + 0x61da ]^M

    address : <0x030c91b0> [ /lib/ld-uClibc.so.0 + 0x11b0 ]^M

    address : <0x030c9164> [ /lib/ld-uClibc.so.0 + 0x1164 ]^M

Bus error^M

root:/>

Last passed time: 2009_May_20_18_21.

--

 

--- Vivi Li                                                  2009-07-12 23:46:30

This bug is fixed by fixation of bug 5331.

Close this bug.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

config.xip.shared-flat    application/octet-stream    32720    Vivi Li

config.xip.fdpic    application/octet-stream    32720    Vivi Li

Outcomes