[#5121] pnormtd test fails on bf518-ezbrd trunk and makes board fail to boot up

Document created by Aaronwu Employee on Sep 3, 2013
Version 1Show Document
  • View in full screen mode

[#5121] pnormtd test fails on bf518-ezbrd trunk and makes board fail to boot up

Submitted By: Vivi Li

Open Date

2009-05-12 04:30:21     Close Date

2009-08-05 22:23:46

Priority:

Medium High     Assignee:

Graf Yang

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

Tests     Board:

N/A

Processor:

BF518     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

toolchain-09r1-rc6

App binary format:

N/A     

Summary: pnormtd test fails on bf518-ezbrd trunk and makes board fail to boot up

Details:

 

Pnormtd test fails on bf518-ezbrd trunk. When execute flash_eraseall, message \"Input/output error\" will show up, then it fails to mount jffs2 filesystem. After that, board can not boot up until we burn a new u-boot.

 

Bellow is the log:

--

Linux version 2.6.28.9-ADI-2009R1-pre-svn6313 (test@uclinux80-518f) (gcc version 4.1.2 (ADI svn)) #4 Wed May 6 00:16:17 GMT 2009^M

console [early_BFuart0] enabled^M

early printk enabled on early_BFuart0^M

Board Memory: 64MB^M

Kernel Managed Memory: 64MB^M

Memory map:^M

  fixedcode = 0x00000400-0x00000490^M

  text      = 0x00001000-0x00110c30^M

  rodata    = 0x00110c30-0x00163160^M

  bss       = 0x00164000-0x00175300^M

  data      = 0x00175300-0x00186000^M

    stack   = 0x00184000-0x00186000^M

  init      = 0x00186000-0x00429000^M

  available = 0x00429000-0x03eff000^M

  DMA Zone  = 0x03f00000-0x04000000^M

Hardware Trace Active and Enabled^M

Boot Mode: 1^M

Blackfin support (C) 2004-2009 Analog Devices, Inc.^M

Compiled for ADSP-BF518 Rev 0.0^M

Blackfin Linux support by http://blackfin.uclinux.org/^M

Processor Speed: 400 MHz core clock and 80 MHz System Clock^M

NOMPU: setting up cplb tables^M

Instruction Cache Enabled for CPU0^M

Data Cache Enabled for CPU0 (write-back)^M

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 16001^M

Kernel command line: root=/dev/mtdblock0 rw earlyprintk=serial,uart0,57600 ip=10.100.4.50:10.100.4.174:10.100.4.174:255.255.255.0:bf518f-ezbrd:eth0:off^M

Configuring Blackfin Priority Driven Interrupts^M

PID hash table entries: 256 (order: 8, 1024 bytes)^M

console handover: boot [early_BFuart0] -> real [ttyBF0]^M

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)^M

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)^M

Memory available: 59680k/65536k RAM, (2700k init code, 1087k kernel code, 469k data, 1024k dma, 572k reserved)^M

Calibrating delay loop... 796.67 BogoMIPS (lpj=1593344)^M

Security Framework initialized^M

Mount-cache hash table entries: 512^M

Blackfin Scratchpad data SRAM: 4 KB^M

Blackfin L1 Data A SRAM: 16 KB (15 KB free)^M

Blackfin L1 Data B SRAM: 16 KB (16 KB free)^M

Blackfin L1 Instruction SRAM: 48 KB (42 KB free)^M

PDA for CPU0 reserved at 00166000^M

net_namespace: 288 bytes^M

NET: Registered protocol family 16^M

Blackfin DMA Controller^M

ezbrd_init(): registering device resources^M

NET: Registered protocol family 2^M

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)^M

TCP established hash table entries: 2048 (order: 2, 16384 bytes)^M

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)^M

TCP: Hash tables configured (established 2048 bind 2048)^M

TCP reno registered^M

NET: Registered protocol family 1^M

JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.^M

msgmni has been set to 116^M

io scheduler noop registered (default)^M

Serial: Blackfin serial driver^M

bfin-uart.1: ttyBF0 at MMIO 0xffc00400 (irq = 29) is a BFIN-UART^M

brd: module loaded^M

bfin_mii_bus: probed^M

bfin_mac: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:03, irq=-1, mdc_clk=2500000Hz(mdc_div=15)@sclk=80MHz)^M

bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1^M

physmap platform flash device: 00400000 at 20000000^M

physmap-flash.0: Found 1 x16 devices at 0x0 in 16-bit bank^M

Amd/Fujitsu Extended Query Table at 0x0040^M

number of CFI chips: 1^M

cfi_cmdset_0002: Disabling erase-suspend-program due to code brokenness.^M

cmdlinepart partition parsing not available^M

RedBoot partition parsing not available^M

Using physmap partition information^M

Creating 3 MTD partitions on \"physmap-flash.0\":^M

0x00000000-0x00040000 : \"bootloader(nor)\"^M

0x00040000-0x00200000 : \"linux kernel(nor)\"^M

0x00200000-0x00400000 : \"file system(nor)\"^M

i2c /dev entries driver^M

i2c-bfin-twi i2c-bfin-twi.0: Blackfin BF5xx on-chip I2C TWI Contoller, regs_base@ffc01400^M

TCP cubic registered^M

NET: Registered protocol family 17^M

dma_alloc_init: dma_page @ 0x00694000 - 256 pages at 0x03f00000^M

IP-Config: Complete:^M

     device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,^M

     host=bf518f-ezbrd, domain=, nis-domain=(none),^M

     bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=^M

Freeing unused kernel memory: 2700k freed^M

                           _____________________________________^M

        a8888b.           / Welcome to the uClinux distribution \\^M

       d888888b.         /       _     _                         \\^M

       8P\"YP\"Y88        /       | |   |_|            __  __ (TM)  |^M

       8|o||o|88  _____/        | |    _ ____  _   _ \\ \\/ /       |^M

       8\'    .88       \\        | |   | |  _ \\| | | | \\  /        |^M

       8`._.\' Y8.       \\       | |__ | | | | | |_| | /  \\        |^M

      d/      `8b.       \\      \\____||_|_| |_|\\____|/_/\\_\\       |^M

     dP   .    Y8b.       \\   For embedded processors including   |^M

    d8:\'  \"  `::88b        \\    the Analog Devices Blackfin      /^M

   d8\"         \'Y88b        \\___________________________________/^M

  :8P    \'      :888^M

   8a.   :     _a88P         For further information, check out:^M

._/\"Yaa_:   .| 88P|            - http://blackfin.uclinux.org/^M

\\    YP\"    `| 8P  `.          - http://docs.blackfin.uclinux.org/^M

/     \\.___.d|    .\'           - http://www.uclinux.org/^M

`--..__)8888P`._.\'  jgs/a:f    - http://www.analog.com/blackfin^M

Have a lot of fun...^M

 

 

BusyBox v1.13.4 (2009-05-05 19:07:33 GMT) built-in shell (msh)^M

Enter \'help\' for a list of built-in commands.^M

 

root:/>

root:/> cat /proc/mtd

dev:    size   erasesize  name

mtd0: 00040000 00010000 \"bootloader(nor)\"

mtd1: 001c0000 00010000 \"linux kernel(nor)\"

mtd2: 00200000 00010000 \"file system(nor)\"

root:/> flash_eraseall -j /dev/mtd2

Erasing 64 Kibyte @ 0 --  0 % complete.

flash_eraseall: /dev/mtd2: MTD Erase failure: Input/output error

Erasing 64 Kibyte @ 10000 --  3 % complete.

flash_eraseall: /dev/mtd2: MTD Erase failure: Input/output error

Erasing 64 Kibyte @ 20000 --  6 % complete.

flash_eraseall: /dev/mtd2: MTD Erase failure: Input/output error

Erasing 64 Kibyte @ 30000 --  9 % complete.

flash_eraseall: /dev/mtd2: MTD Erase failure: Input/output error

Erasing 64 Kibyte @ 40000 -- 12 % complete.

flash_eraseall: /dev/mtd2: MTD Erase failure: Input/output error

Erasing 64 Kibyte @ 50000 -- 15 % complete.

flash_eraseall: /dev/mtd2: MTD Erase failure: Input/output error

Erasing 64 Kibyte @ 60000 -- 18 % complete.

flash_eraseall: /dev/mtd2: MTD Erase failure: Input/output error

Erasing 64 Kibyte @ 70000 -- 21 % complete.

flash_eraseall: /dev/mtd2: MTD Erase failure: Input/output error

Erasing 64 Kibyte @ 80000 -- 25 % complete.

flash_eraseall: /dev/mtd2: MTD Erase failure: Input/output error

Erasing 64 Kibyte @ 90000 -- 28 % complete.

flash_eraseall: /dev/mtd2: MTD Erase failure: Input/output error

Erasing 64 Kibyte @ a0000 -- 31 % complete.

flash_eraseall: /dev/mtd2: MTD Erase failure: Input/output error

Erasing 64 Kibyte @ b0000 -- 34 % complete.

flash_eraseall: /dev/mtd2: MTD Erase failure: Input/output error

Erasing 64 Kibyte @ c0000 -- 37 % complete.

flash_eraseall: /dev/mtd2: MTD Erase failure: Input/output error

Erasing 64 Kibyte @ d0000 -- 40 % complete.

flash_eraseall: /dev/mtd2: MTD Erase failure: Input/output error

Erasing 64 Kibyte @ e0000 -- 43 % complete.

flash_eraseall: /dev/mtd2: MTD Erase failure: Input/output error

Erasing 64 Kibyte @ f0000 -- 46 % complete.

flash_eraseall: /dev/mtd2: MTD Erase failure: Input/output error

Erasing 64 Kibyte @ 100000 -- 50 % complete.

flash_eraseall: /dev/mtd2: MTD Erase failure: Input/output error

Erasing 64 Kibyte @ 110000 -- 53 % complete.

flash_eraseall: /dev/mtd2: MTD Erase failure: Input/output error

Erasing 64 Kibyte @ 120000 -- 56 % complete.

flash_eraseall: /dev/mtd2: MTD Erase failure: Input/output error

Erasing 64 Kibyte @ 130000 -- 59 % complete.

flash_eraseall: /dev/mtd2: MTD Erase failure: Input/output error

Erasing 64 Kibyte @ 140000 -- 62 % complete.

flash_eraseall: /dev/mtd2: MTD Erase failure: Input/output error

Erasing 64 Kibyte @ 150000 -- 65 % complete.

flash_eraseall: /dev/mtd2: MTD Erase failure: Input/output error

Erasing 64 Kibyte @ 160000 -- 68 % complete.

flash_eraseall: /dev/mtd2: MTD Erase failure: Input/output error

Erasing 64 Kibyte @ 170000 -- 71 % complete.

flash_eraseall: /dev/mtd2: MTD Erase failure: Input/output error

Erasing 64 Kibyte @ 180000 -- 75 % complete.

flash_eraseall: /dev/mtd2: MTD Erase failure: Input/output error

Erasing 64 Kibyte @ 190000 -- 78 % complete.

flash_eraseall: /dev/mtd2: MTD Erase failure: Input/output error

Erasing 64 Kibyte @ 1a0000 -- 81 % complete.

flash_eraseall: /dev/mtd2: MTD Erase failure: Input/output error

Erasing 64 Kibyte @ 1b0000 -- 84 % complete.

flash_eraseall: /dev/mtd2: MTD Erase failure: Input/output error

Erasing 64 Kibyte @ 1c0000 -- 87 % complete.

flash_eraseall: /dev/mtd2: MTD Erase failure: Input/output error

Erasing 64 Kibyte @ 1d0000 -- 90 % complete.

flash_eraseall: /dev/mtd2: MTD Erase failure: Input/output error

Erasing 64 Kibyte @ 1e0000 -- 93 % complete.

flash_eraseall: /dev/mtd2: MTD Erase failure: Input/output error

Erasing 64 Kibyte @ 1f0000 -- 96 % complete.

flash_eraseall: /dev/mtd2: MTD Erase failure: Input/output error

Erasing 64 Kibyte @ 200000 -- 100 % complete.

root:/> mkdir -p rootfs

root:/> echo \"This is test for mtd driver\" > rootfs/test

root:/> mkfs.jffs2 -r rootfs -o mtd.img

root:/> cp mtd.img /dev/mtd2

root:/> mount -t jffs2 /dev/mtdblock2 /mnt

jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00000000: 0x6c42 instead^M

jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00000044: 0xe6b8 instead^M

jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00000048: 0xe6b8 instead^M

jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x0000004c: 0xe6b8 instead^M

jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00000050: 0xe6b8 instead^M

jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00000054: 0xe6b8 instead^M

jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00000058: 0xe6b8 instead^M

jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x0000005c: 0xe6b8 instead^M

jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00000060: 0xe6b8 instead^M

jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00000064: 0x1866 instead^M

Further such events for this erase block will not be printed^M

jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00010000: 0xe3ca instead^M

jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00010004: 0xe3ca instead^M

jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00010008: 0xe3ca instead^M

jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x0001000c: 0xe3ca instead^M

jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00010010: 0xe3ca instead^M

jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00010014: 0xe3ca instead^M

jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00010018: 0xe3ca instead^M

jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x0001001c: 0xe3ca instead^M

jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00010020: 0xe3ca instead^M

jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00010024: 0xe3ca instead^M

Further such events for this erase block will not be printed^M

jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00020000: 0x0003 instead^M

jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00020004: 0x0003 instead^M

jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00020008: 0x0003 instead^M

jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x0002000c: 0x0003 instead^M

jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00020010: 0x0003 instead^M

jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00020014: 0x0003 instead^M

jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00020018: 0x0003 instead^M

jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x0002001c: 0x0003 instead^M

jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00020020: 0x0003 instead^M

jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00020024: 0x0003 instead^M

Further such events for this erase block will not be printed^M

jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00030000: 0xe3ca instead^M

jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x00030004: 0xe3ca instead^M

...

Empty flash at 0x001e0940 ends at 0x001e0944

jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x001f0000: 0x0003 instead

jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x001f0004: 0x0003 instead

jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x001f0008: 0x0003 instead

jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x001f000c: 0x0003 instead

jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x001f0010: 0x0003 instead

jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x001f0014: 0x0003 instead

jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x001f0018: 0x0003 instead

jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x001f001c: 0x0003 instead

jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x001f0020: 0x0003 instead

jffs2_scan_eraseblock(): Magic bitmask 0x1985 not found at 0x001f0024: 0x0003 instead

Further such events for this erase block will not be printed

Cowardly refusing to erase blocks on filesystem with no valid JFFS2 nodes

empty_blocks 0, bad_blocks 0, c->nr_blocks 32

root:/>

--

 

Follow-ups

 

--- Graf Yang                                                2009-05-20 02:11:26

The AMS bus pin AMS2/3 is shared with SPI0, and is not set as AMS2/3 by

default.

 

Now I have setting it for Nor flash, and when testing Nor flash, please turn

off SPI driver and DSA driver(it uses SPI0).

 

--- Vivi Li                                                  2009-08-06 03:23:46

OK now.

Close it.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes