[#5053] EXT2_INODES and EXT2_BLOCKS values reversed in vendor.mak

Document created by Aaronwu Employee on Sep 3, 2013
Version 1Show Document
  • View in full screen mode

[#5053] EXT2_INODES and EXT2_BLOCKS values reversed in vendor.mak

Submitted By: Jeff Otterson

Open Date

2009-04-04 14:23:02     Close Date

2009-04-08 22:11:53

Priority:

Medium     Assignee:

Nobody

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

svn 7942

Category:

Make Errors     Board:

STAMP

Processor:

ALL     Silicon Revision:

0.2

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

n/a     Toolchain version or rev.:

svn

App binary format:

FDPIC     

Summary: EXT2_INODES and EXT2_BLOCKS values reversed in vendor.mak

Details:

 

It looks like when the EXT2_INODES and EXT_BLOCKS values were promoted up to vendor.mak in revsion 7942, the values got reversed.  The end result is that an ext2 image cannot be created and the build fails. 

 

I reversed the values as shown:

 

  EXT2_INODES ?= 1024

  EXT2_BLOCKS ?= 8192 # Blocks must be a multiple of 1024

 

and I can build anm ext2 image again...

 

I marked this item as release 2009r1 because that is the label put on the kernel.  This is current in SVN as of today, 2009/04/04.

 

Kernel svn version 6244

uclinux svn version 7958

 

Follow-ups

 

--- Mike Frysinger                                           2009-04-04 14:42:42

thanks, fixed in svn now

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes