[#5025] AD1981 sometimes gets bad quality sound and would reset after a long time play.

Document created by Aaronwu Employee on Sep 3, 2013
Version 1Show Document
  • View in full screen mode

[#5025] AD1981 sometimes gets bad quality sound and would reset after a long time play.

Submitted By: Cliff Cai

Open Date

2009-03-30 05:34:32     Close Date

2009-11-17 22:20:39

Priority:

Medium High     Assignee:

Cliff Cai

Status:

Closed     Fixed In Release:

2008R1.5-RC3

Found In Release:

2008R1-RC8     Release:

08r1

Category:

Drivers     Board:

N/A

Processor:

BF537     Silicon Revision:

all

Is this bug repeatable?:

Yes     Resolution:

Out of Date

Uboot version or rev.:

    Toolchain version or rev.:

08r1

App binary format:

N/A     

Summary: AD1981 sometimes gets bad quality sound and would reset after a long time play.

Details:

 

see:  blackfin.uclinux.org/gf/project/uclinux-dist/forum/?action=ForumBrowse&forum_id=39&_forum_action=ForumMessageBrowse&thread_id=32179

 

Follow-ups

 

--- Cliff Cai                                                2009-04-17 04:56:14

it seems that this problem is caused by the content of dummy buffer,

sometimes the codec doesn't understand the frame sent to it,when DMA is the

switched to dummy buffer.I will do more tests to verify it.

 

--- Cliff Cai                                                2009-06-24 23:10:18

fixed,sendind out the remaining data in TX FIFO when stop sport.

 

Cliff

 

--- Vivi Li                                                  2009-07-29 04:24:39

When I test ad1980 power case on bf548-ezkit with 09r1, sometimes command

"vrec -w -S -b 16 -s 48000 |vplay" gives high pitch noise, like tone.

Stop it and run again, it will get back to normal.

I built ad1980 as module.

 

--- Cliff Cai                                                2009-08-02 21:38:30

I've taken this into account,the module case was ignored before.

 

Cliff

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes