[#4929] ethernet gadget don't work on 537 with a USB-LAN extender

Document created by Aaronwu Employee on Aug 30, 2013
Version 1Show Document
  • View in full screen mode

[#4929] ethernet gadget don't work on 537 with a USB-LAN extender

Submitted By: Vivi Li

Open Date

2009-02-23 04:35:19     Close Date

2009-03-26 23:56:09

Priority:

Medium     Assignee:

Michael Hennerich

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

STAMP

Processor:

BF537     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.1_2009-01-19

App binary format:

N/A     

Summary: ethernet gadget don't work on 537 with a USB-LAN extender

Details:

 

For bf537 with a USB-LAN extender, ethernet gadget and RNDIS don't work.

 

Kernel config file is attached. Bellow is the log:

--

Linux version 2.6.28.5-ADI-2009R1-pre-svn6104 (test@uclinux58-mmc-usblan) (gcc version 4.1.2 (ADI s9

console [early_BFuart0] enabled

early printk enabled on early_BFuart0

Warning: limiting memory to 56MB due to hardware anomaly 05000263

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x00110df0

  rodata    = 0x00110df0-0x00163f48

  bss       = 0x00163f50-0x00172aa4

  data      = 0x00172aa4-0x00184000

    stack   = 0x00182000-0x00184000

  init      = 0x00184000-0x0061e000

  available = 0x0061e000-0x037ff000

  DMA Zone  = 0x03f00000-0x04000000

Hardware Trace Active and Enabled

Boot Mode: 0

Reset caused by Software reset

Blackfin support (C) 2004-2009 Analog Devices, Inc.

Compiled for ADSP-BF537 Rev 0.2

Blackfin Linux support by   blackfin.uclinux.org/

Processor Speed: 500 MHz core clock and 125 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

Data Cache Enabled for CPU0 (write-back)

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 14223

Kernel command line: root=/dev/mtdblock0 rw earlyprintk=serial,uart0,57600 console=ttyBF0,57600 ip=f

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 256 (order: 8, 1024 bytes)

console handover: boot [early_BFuart0] -> real [ttyBF0]

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 50496k/65536k RAM, (4712k init code, 1087k kernel code, 461k data, 1024k dma, 775)

Calibrating delay loop... 997.37 BogoMIPS (lpj=1994752)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (15 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (41 KB free)

PDA for CPU0 reserved at 00165038

net_namespace: 288 bytes

NET: Registered protocol family 16

Blackfin GPIO Controller

Blackfin DMA Controller

stamp_init(): registering device resources

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

NET: Registered protocol family 1

msgmni has been set to 98

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART

brd: module loaded

bfin_mii_bus: probed

bfin_mac: attached PHY driver [SMSC LAN83C185] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(md)

bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1

net2272: PLX NET2272 USB Peripheral Controller

net2272: irq 57, mapped mem 20300000, chip rev 0011

net2272: running in 16-bit, no byte swap local bus mode

net2272: version: 2005 Sept 8

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 1970-01-04 16:23:34 UTC (318214)

IP-Config: Complete:

     device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,

     host=bf537-stamp, domain=, nis-domain=(none),

     bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=

Freeing unused kernel memory: 4712k freed

dma_alloc_init: dma_page @ 0x0061b000 - 256 pages at 0x03f00000

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            -   blackfin.uclinux.org/

\    YP"    `| 8P  `.          -   docs.blackfin.uclinux.org/

/     \.___.d|    .'           -   www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    -   www.analog.com/blackfin

 

Have a lot of fun...

 

 

BusyBox v1.13.2 (2009-02-18 14:46:47 GMT) built-in shell (msh)

Enter 'help' for a list of built-in commands.

 

root:/> PHY: 0:01 - Link is Up - 100/Full

root:/>

root:/> dmesg |grep net2272

net2272: PLX NET2272 USB Peripheral Controller

net2272: irq 57, mapped mem 20300000, chip rev 0011

net2272: running in 16-bit, no byte swap local bus mode

net2272: version: 2005 Sept 8

root:/> dmesg |grep usb0

root:/>

root:/>

root:/> ifconfig -a

eth0      Link encap:Ethernet  HWaddr 00:E0:22:FE:47:DE

          inet addr:10.100.4.50  Bcast:10.100.4.255  Mask:255.255.255.0

          UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1

          RX packets:2 errors:0 dropped:0 overruns:0 frame:0

          TX packets:1 errors:0 dropped:0 overruns:0 carrier:0

          collisions:0 txqueuelen:1000

          RX bytes:128 (128.0 B)  TX bytes:42 (42.0 B)

 

lo        Link encap:Local Loopback

          inet addr:127.0.0.1  Mask:255.0.0.0

          UP LOOPBACK RUNNING  MTU:16436  Metric:1

          RX packets:0 errors:0 dropped:0 overruns:0 frame:0

          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0

          collisions:0 txqueuelen:0

          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

 

root:/>

--

 

Following message should appear during kernel booting if usb network is OK.

--

net2272: PLX NET2272 USB Peripheral Controller

net2272: irq 57, mapped mem 20300000, chip rev 0011

net2272: running in 16-bit, no byte swap local bus mode

net2272: version: 2005 Sept 8

ether gadget: using random self ethernet address

ether gadget: using random host ethernet address

usb0: Ethernet Gadget, version: May Day 2005

usb0: using net2272, OUT ep-b IN ep-a STATUS ep-c

usb0: MAC b2:d5:5a:dd:97:6b

usb0: HOST MAC b6:79:97:c0:40:c4

usb0: RNDIS ready

--

 

Follow-ups

 

--- Michael Hennerich                                        2009-03-18 12:39:38

Fixed on svn trunk:

 

Fix usb_gadget_register_driver don't test for unbind.

Unbind is declared __exit_p(f) which defaults to NULL if not MODULE

 

Fix compile warnings - WARN redefined

 

Use board defines to workaround board issues rather than processor

defines.

 

Fix Kconfig indention

 

-Michael

 

--- Vivi Li                                                  2009-03-26 23:56:09

It works now. Close this bug.

Thanks!

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

config.usbnet    application/octet-stream    36466    Vivi Li

Attachments

Outcomes