[#4928] ad1981b add-on board fails to work on bf527-ezkit sport1

Document created by Aaronwu Employee on Aug 30, 2013
Version 1Show Document
  • View in full screen mode

[#4928] ad1981b add-on board fails to work on bf527-ezkit sport1

Submitted By: Vivi Li

Open Date

2009-02-23 04:11:14     Close Date

2009-03-29 23:30:35

Priority:

Medium     Assignee:

Cliff Cai

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

EZKIT Lite

Processor:

BF527     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.1_2009-01-19

App binary format:

N/A     

Summary: ad1981b add-on board fails to work on bf527-ezkit sport1

Details:

 

ad1981b add-on board fails to work on bf527-ezkit sport1 port. It works well on bf527-ezkit sport0 port.

 

--

root:/> dmesg

Linux version 2.6.28.6-ADI-2009R1-pre-svn6120 (test@uclinux63-527-usbdev) (gcc version 4.1.2 (ADI s9

console [early_BFuart0] enabled

early printk enabled on early_BFuart0

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x0013a980

  rodata    = 0x0013a980-0x0019bc38

  bss       = 0x0019bc40-0x001ab2d8

  data      = 0x001ab2d8-0x001be000

    stack   = 0x001bc000-0x001be000

  init      = 0x001be000-0x00604000

  available = 0x00604000-0x03dff000

  DMA Zone  = 0x03e00000-0x04000000

Hardware Trace Active and Enabled

Boot Mode: 1

Reset caused by Software reset

Blackfin support (C) 2004-2009 Analog Devices, Inc.

Compiled for ADSP-BF527 Rev 0.0

Warning: Compiled for Rev 0, but running on Rev 2

Blackfin Linux support by   blackfin.uclinux.org/

Processor Speed: 525 MHz core clock and 131 MHz System Clock

boot memmap: 0000000000604000 - 0000000003dff000 (usable)

On node 0 totalpages: 15871

free_area_init_node: node 0, pgdat 001ba370, node_mem_map 00609000

  DMA zone: 124 pages used for memmap

  DMA zone: 0 pages reserved

  DMA zone: 15747 pages, LIFO batch:3

  Normal zone: 0 pages used for memmap

  Movable zone: 0 pages used for memmap

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

Data Cache Enabled for CPU0 (write-back)

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 15747

Kernel command line: root=/dev/mtdblock0 rw earlyprintk=serial,uart0,57600 ip=10.100.4.50:10.100.4.f

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 256 (order: 8, 1024 bytes)

console handover: boot [early_BFuart0] -> real [ttyBF0]

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Kernel managed physical pages: 15871

Memory available: 56744k/65536k RAM, (4376k init code, 1254k kernel code, 526k data, 2048k dma, 584)

Calibrating delay loop... 1046.52 BogoMIPS (lpj=2093056)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (15 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (42 KB free)

PDA for CPU0 reserved at 0019cb70

net_namespace: 288 bytes

NET: Registered protocol family 16

Blackfin GPIO Controller

Blackfin DMA Controller

ezkit_init(): registering device resources

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

musb_hdrc: version 6.0, pio, peripheral, debug=0

musb_hdrc: ConfigData=0x00 (UTMI-8)

musb_hdrc: HDRC RTL version 0.0

musb_hdrc: hw_ep 0shared, max 64

musb_hdrc: hw_ep 1tx, max 128

musb_hdrc: hw_ep 1rx, max 128

musb_hdrc: hw_ep 2tx, max 128

musb_hdrc: hw_ep 2rx, max 128

musb_hdrc: hw_ep 3tx, max 128

musb_hdrc: hw_ep 3rx, max 128

musb_hdrc: hw_ep 4tx, max 128

musb_hdrc: hw_ep 4rx, max 128

musb_hdrc: hw_ep 5tx, max 1024

musb_hdrc: hw_ep 5rx, max 1024

musb_hdrc: hw_ep 6tx, max 1024

musb_hdrc: hw_ep 6rx, max 1024

musb_hdrc: hw_ep 7tx, max 1024

musb_hdrc: hw_ep 7rx, max 1024

musb_hdrc: USB Peripheral mode controller at ffc03800 using PIO, IRQ 59

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

NET: Registered protocol family 1

Setting up Blackfin MMR debugfs

msgmni has been set to 110

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

bfin-otp: initialized

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc02000 (irq = 31) is a BFIN-UART

brd: module loaded

bfin_mii_bus: probed

bfin_mac: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:03, irq=-1, mdc_clk=2500000Hz(mdc_d)

bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1

m25p80 spi0.1: m25p16 (2048 Kbytes)

Creating 2 MTD partitions on "m25p80":

0x00000000-0x00040000 : "bootloader(spi)"

0x00040000-0x00200000 : "linux kernel(spi)"

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma c7

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

hid_tmff: Unknown symbol _input_ff_create_memless

usbcore: registered new interface driver usbhid

usbhid: v2.6:USB HID core driver

Advanced Linux Sound Architecture Driver Version 1.0.18rc3.

ASoC version 0.13.2

dma rx:5 tx:6, err irq:16, regs:ffc00900

AD1980 SoC Audio Codec

dma_alloc_init: dma_page @ 0x03aa8000 - 512 pages at 0x03e00000

asoc: AC97 <-> bf5xx-ac97 mapping ok

bf5xx_ac97_cold_reset: Not implemented

bf5xx_ac97_cold_reset: Not implemented

bf5xx_ac97_cold_reset: Not implemented

bf5xx_ac97_cold_reset: Not implemented

bf5xx_ac97_cold_reset: Not implemented

bf5xx_ac97_cold_reset: Not implemented

bf5xx_ac97_cold_reset: Not implemented

bf5xx_ac97_cold_reset: Not implemented

bf5xx_ac97_cold_reset: Not implemented

bf5xx_ac97_cold_reset: Not implemented

bf5xx_ac97_cold_reset: Not implemented

AD1980 AC97 reset failed

AC97 link error

soc-audio: probe of soc-audio failed with error -5

ALSA device list:

  No soundcards found.

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 2014-12-25 16:07:09 UTC (1419523629)

IP-Config: Gateway not on directly connected network.

Freeing unused kernel memory: 4376k freed

PHY: 0:03 - Link is Up - 100/Full

root:/>

--

 

Follow-ups

 

--- Cliff Cai                                                2009-03-04 23:10:47

By default ,the pins needed by SPORT1 are connected to other devices,So we need

to turn off those connections before using SPORT1,but unfortunately,PF8(DR1PRI)

is occupied by LED1 or LCD,and the connection can't be turned off totally.So,I

couldn't get record work on SPORT1.

Following settings will make playback work:

SW11:OFF,OFF,OFF,OFF,ON;SW5:OFF,OFF,OFF,ON.

 

Cliff

 

--- Cliff Cai                                                2009-03-05 05:25:40

The cause is that the DR1PRI is shared with signal LED0,and LED0 has a

pull-up,after I removed the pull-up R176, receive works just fine.

 

SW11:OFF,OFF,OFF,ON;SW5:OFF,OFF,OFF,OFF

 

Cliff

 

--- Vivi Li                                                  2009-03-29 23:30:35

OK now. Close it.

Thanks!

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes