[#4923] usb gadget zero control test NO. 10 fails

Document created by Aaronwu Employee on Aug 30, 2013
Version 1Show Document
  • View in full screen mode

[#4923] usb gadget zero control test NO. 10 fails

Submitted By: Vivi Li

Open Date

2009-02-20 05:35:38     Close Date

2009-06-18 03:50:47

Priority:

Medium High     Assignee:

Nobody

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

Drivers     Board:

EZKIT Lite

Processor:

BF527     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Not reproducible

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.1_2009-01-19

App binary format:

N/A     

Summary: usb gadget zero control test NO. 10 fails

Details:

 

For usb gadget zero control test NO. 10, it will fail for both BF527-EZKIT and BF548-EZKIT.

 

--

sudo ./src/testusb -D /proc/bus/usb/005/113 -t10

unknown speed   /proc/bus/usb/005/113

/proc/bus/usb/005/113 test 10 --> 33 (Numerical argument out of domain)

--

 

Follow-ups

 

--- Bryan Wu                                                 2009-02-25 04:19:04

I can not reproduce this on my BF548-EZKIT board, which is 1.4 rev with 0.2

silicon.

 

-Bryan

 

--- Sonic Zhang                                              2009-04-03 04:59:52

Can't replicate also on kernl SVN 6173 and uClinux-dist SVN 7888 on bf548 v0.2

 

--- Vivi Li                                                  2009-06-18 03:50:47

The test machine need to update kernel, the same reason as bug 5260.

Disable test 10 in gadget zero control test until kernel is updated to 2.6.26

or higher in host PC.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes