[#4887] watchdog fails to reboot on bf548 ezkit when get killed

Document created by Aaronwu Employee on Aug 30, 2013
Version 1Show Document
  • View in full screen mode

[#4887] watchdog fails to reboot on bf548 ezkit when get killed

Submitted By: Mingquan Pan

Open Date

2009-02-11 02:22:06     Close Date

2009-06-18 04:56:04

Priority:

Medium High     Assignee:

Graf Yang

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

ALL     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

4.1 of Jan 16

App binary format:

N/A     

Summary: watchdog fails to reboot on bf548 ezkit when get killed

Details:

 

watchdog fails to reboot on bf548 ezkit when get killed from about Feb 4.

 

## Booting image at 02000000 ...

   Image Name:   Linux-2.6.28-ADI-2009R1-pre-svn6

   Created:      2009-02-04  23:58:30 UTC

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    4862014 Bytes =  4.6 MB

   Load Address: 00001000

   Entry Point:  002795cc

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 2795cc

Linux version 2.6.28-ADI-2009R1-pre-svn6055 (test@uclinux61-bf548-std) (gcc version 4.1.2 (ADI svn)) #8 Wed Feb 4 23:58:08 GMT 2009

console [early_BFuart0] enabled

early printk enabled on early_BFuart0

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x001aa350

  rodata    = 0x001aa350-0x002394b4

  bss       = 0x002394c0-0x0024b56c

  data      = 0x0024b56c-0x00264000

    stack   = 0x00262000-0x00264000

  init      = 0x00264000-0x0092d000

  available = 0x0092d000-0x03dff000

  DMA Zone  = 0x03e00000-0x04000000

Hardware Trace Active and Enabled

Boot Mode: 1

Reset caused by Software reset

Blackfin support (C) 2004-2009 Analog Devices, Inc.

Compiled for ADSP-BF548 Rev 0.1

Blackfin Linux support by   blackfin.uclinux.org/

Processor Speed: 525 MHz core clock and 131 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

Data Cache Enabled for CPU0 (write-through)

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 15747

Kernel command line: root=/dev/mtdblock0 rw earlyprintk=serial,uart0,57600 ip=10.100.4.50:10.100.4.174:192.168.0.1:255.255.255.0:bf548-ezkit:eth0:off

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 256 (order: 8, 1024 bytes)

console handover: boot [early_BFuart0] -> real [ttyBF0]

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 53508k/65536k RAM, (6948k init code, 1700k kernel code, 744k data, 2048k dma, 584k reserved)

Calibrating delay loop... 1044.48 BogoMIPS (lpj=2088960)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (15 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (42 KB free)

Blackfin L2 SRAM: 128 KB (128 KB free)

PDA for CPU0 reserved at 0023ad78

net_namespace: 288 bytes

NET: Registered protocol family 16

Blackfin GPIO Controller

Blackfin DMA Controller

ezkit_init(): registering device resources

SCSI subsystem initialized

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

musb_hdrc: version 6.0, musb-dma, host, debug=0

musb_hdrc: USB Host mode controller at ffc03c00 using DMA, IRQ 82

musb_hdrc musb_hdrc.0: MUSB HDRC host driver

musb_hdrc musb_hdrc.0: new USB bus registered, assigned bus number 1

usb usb1: configuration #1 chosen from 1 choice

hub 1-0:1.0: USB hub found

dma_alloc_init: dma_page @ 0x03d94000 - 512 pages at 0x03e00000

hub 1-0:1.0: 1 port detected

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

NET: Registered protocol family 1

msgmni has been set to 104

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

bf54x-lq043: FrameBuffer initializing...

bfin-otp: initialized

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc02000 (irq = 48) is a BFIN-UART

brd: module loaded

smsc911x: Driver version 2007-07-13.

eth0: SMSC911x MAC Address: 00:e0:22:fe:b8:54

Driver 'sd' needs updating - please use bus_type methods

Driver 'sr' needs updating - please use bus_type methods

register bfin atapi driver

scsi0 : pata-bf54x

ata1: PATA max UDMA/66 irq 68

ata1.00: ATA-6: TOSHIBA MK4032GAX, AD101A, max UDMA/100

ata1.00: 78140160 sectors, multi 16: LBA48

ata1.00: configured for UDMA/66

blk_queue_max_hw_segments: set to minimum 1

scsi 0:0:0:0: Direct-Access     ATA      TOSHIBA MK4032GA AD10 PQ: 0 ANSI: 5

sd 0:0:0:0: [sda] 78140160 512-byte hardware sectors: (40.0 GB/37.2 GiB)

sd 0:0:0:0: [sda] Write Protect is off

sd 0:0:0:0: [sda] Write cache: enabled, read cache: enabled, doesn't support DPO or FUA

sd 0:0:0:0: [sda] 78140160 512-byte hardware sectors: (40.0 GB/37.2 GiB)

sd 0:0:0:0: [sda] Write Protect is off

sd 0:0:0:0: [sda] Write cache: enabled, read cache: enabled, doesn't support DPO or FUA

sda: sda1 sda2

sd 0:0:0:0: [sda] Attached SCSI disk

physmap platform flash device: 02000000 at 20000000

physmap-flash.0: Found 1 x16 devices at 0x0 in 16-bit bank

Intel/Sharp Extended Query Table at 0x010A

Intel/Sharp Extended Query Table at 0x010A

Intel/Sharp Extended Query Table at 0x010A

Intel/Sharp Extended Query Table at 0x010A

Intel/Sharp Extended Query Table at 0x010A

Using buffer write method

Using auto-unlock on power-up/resume

cfi_cmdset_0001: Erase suspend on write enabled

RedBoot partition parsing not available

Using physmap partition information

Creating 3 MTD partitions on "physmap-flash.0":

0x00000000-0x00040000 : "bootloader(nor)"

0x00040000-0x00440000 : "linux kernel(nor)"

0x00440000-0x01000000 : "file system(nor)"

BF5xx on-chip NAND FLash Controller Driver, Version 1.2 (c) 2007 Analog Devices, Inc.

bf5xx-nand bf5xx-nand.0: page_size=256, data_width=8, wr_dly=3, rd_dly=3

NAND device: Manufacturer ID: 0x20, Chip ID: 0xda (ST Micro NAND 256MiB 3,3V 8-bit)

Creating 2 MTD partitions on "NAND 256MiB 3,3V 8-bit":

0x00000000-0x00400000 : "linux kernel(nand)"

0x00400000-0x10000000 : "file system(nand)"

m25p80 spi0.1: m25p16 (2048 Kbytes)

Creating 2 MTD partitions on "m25p80":

0x00000000-0x00040000 : "bootloader(spi)"

0x00040000-0x00200000 : "linux kernel(spi)"

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@4

bfin-spi bfin-spi.1: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc02300, dma channel@5

input: bf54x-keys as /devices/platform/bf54x-keys/input/input0

bf54x-keys: Blackfin BF54x Keypad registered IRQ 76

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

i2c /dev entries driver

i2c-bfin-twi i2c-bfin-twi.0: Blackfin BF5xx on-chip I2C TWI Contoller, regs_base@ffc00700

i2c-bfin-twi i2c-bfin-twi.1: Blackfin BF5xx on-chip I2C TWI Contoller, regs_base@ffc02200

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

hid_zpff: Unknown symbol _input_ff_create_memless

usbcore: registered new interface driver usbhid

usbhid: v2.6:USB HID core driver

Advanced Linux Sound Architecture Driver Version 1.0.18rc3.

ASoC version 0.13.2

dma rx:0 tx:1, err irq:10, regs:ffc00800

AD1980 SoC Audio Codec

asoc: AC97 <-> bf5xx-ac97 mapping ok

ALSA device list:

  #0: bf5xx-board (AD1980)

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 2004-05-31 02:46:19 UTC (1085971579)

eth0: SMSC911x/921x identified at 0x24000000, IRQ: 175

eth0: link down

IP-Config: Gateway not on directly connected network.

Freeing unused kernel memory: 6948k freed

eth0: link up, 100Mbps, full-duplex, lpa 0x41E1

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            -   blackfin.uclinux.org/

\    YP"    `| 8P  `.          -   docs.blackfin.uclinux.org/

/     \.___.d|    .'           -   www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    -   www.analog.com/blackfin

 

Have a lot of fun...

 

 

BusyBox v1.13.2 (2009-02-04 19:36:50 GMT) built-in shell (msh)

Enter 'help' for a list of built-in commands.

 

root:/>

************** STEP 3: Start testing.

 

cd /bin

root:/bin> ./watchdogd

Start in daemon mode.

r

Case 1 ...PASS

 

Case 1 ...PASS

oot:/bin> ps aux| grep watchdogd | head -1

  307 root        32 S    ./watchdogd -f

Case 2 ...PASS

 

Case 2 ...PASS

 

root:/bin> kill -9 307

bfin-wdt: Unexpected close, not stopping watchdog!

root:/bin>

Case 3 ...FAIL

 

 

The resivion of the last working source is:

echo "************* Tested uclinux-dist svn info *************"

Path: .

URL: svn://10.99.22.20/uclinux-dist/trunk

Repository Root: svn://10.99.22.20/uclinux-dist

Repository UUID: 3e2a5524-39e8-4cb9-84a9-c49da69cba3a

Revision: 7699

Node Kind: directory

Schedule: normal

Last Changed Author: vivili

Last Changed Rev: 7699

Last Changed Date: 2009-02-02 03:37:47 +0000 (Mon, 02 Feb 2009)

echo "************* Tested linux svn info ********************"

Path: .

URL: svn://10.99.22.20/linux-kernel/trunk

Repository Root: svn://10.99.22.20/linux-kernel

Repository UUID: 526b6c2d-f592-4532-a319-5dd88ccb003d

Revision: 6046

Node Kind: directory

Schedule: normal

Last Changed Author: gyang

Last Changed Rev: 6046

Last Changed Date: 2009-02-02 09:40:25 +0000 (Mon, 02 Feb 2009)

 

 

Follow-ups

 

--- Graf Yang                                                2009-04-29 00:50:57

I can't duplicate this bug.

I use toolchain 09r1 rc5, kernel 2009-04-26 rev 6307.

 

--- Mingquan Pan                                             2009-05-18 05:37:51

Yes, it is ok with trunk head kernel and toolchain 09r1 rc6 on board ADSP-BF548

Rev 0.2. Close it.

 

--- Mingquan Pan                                             2009-06-02 03:44:41

This issue shows up again in log from May 20.

It looks this is due to the u-boot updated to 09r1 from 08r1.5 that day,

because using the uImage prior May 20 to run on the same board with updated

u-boot also fails.

 

Failed log:

 

U-Boot 2008.10-svn1872 (ADI-2009R1-rc1) (May 20 2009 - 17:37:34)

 

CPU:   ADSP bf548-0.2 (Detected Rev: 0.2) (parallel flash boot)

Board: ADI BF548 EZ-Kit board

       Support:   blackfin.uclinux.org/

Clock: VCO: 525 MHz, Core: 525 MHz, System: 131.250 MHz

RAM:   64 MB

Flash:

RAM size is 64 MB.

16 MB

NAND:  256 MiB

In:    serial

Out:   serial

Err:   serial

Net:   MAC:   00:E0:22:FE:BF:4E

Hit any key to stop autoboot:  0

bfin>

bfin> set bootargs root=/dev/mtdblock0 rw earlyprintk=serial,uart0,57600

bfin> set serverip 10.100.4.174

bfin> set ipaddr 10.100.4.50

bfin> save

Saving Environment to Flash...

. done

Un-Protected 1 sectors

Erasing Flash...

. done

Erased 1 sectors

Writing to Flash... done

. done

Protected 1 sectors

bfin>

bfin> tftpboot 0x2000000 uImage

smc911x: initializing

smc911x: detected LAN9218 controller

smc911x: phy initialized

smc911x: MAC 00:e0:22:fe:bf:4e

TFTP from server 10.100.4.174; our IP address is 10.100.4.50

Filename 'uImage'.

Load address: 0x2000000

Loading: #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         ##########################################

done

Bytes transferred = 5386071 (522f57 hex)

Image size is 522f57

bfin> run addip

bfin> bootm

## Booting kernel from Legacy Image at 02000000 ...

   Image Name:   Linux-2.6.28.10-ADI-2009R1-pre-s

   Created:      2009-05-18  19:08:02 UTC

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    5386007 Bytes =  5.1 MB

   Load Address: 00001000

   Entry Point:  0026178c

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 0026178c

Linux version 2.6.28.10-ADI-2009R1-pre-svn6364 (test@uclinux61-bf548-std) (gcc

version 4.1.2 (ADI svn)) #229 Mon May 18 19:07:43 GMT 2009

console [early_BFuart0] enabled

early printk enabled on early_BFuart0

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x001923e0

  rodata    = 0x001923e0-0x0021d918

  bss       = 0x0021e000-0x00232150

  data      = 0x00232150-0x0024c000

    stack   = 0x0024a000-0x0024c000

  init      = 0x0024c000-0x009f8000

  available = 0x009f8000-0x03dff000

  DMA Zone  = 0x03e00000-0x04000000

Hardware Trace Active and Enabled

Boot Mode: 1

Blackfin support (C) 2004-2009 Analog Devices, Inc.

Compiled for ADSP-BF548 Rev 0.2

Blackfin Linux support by   blackfin.uclinux.org/

Processor Speed: 525 MHz core clock and 131 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

Data Cache Enabled for CPU0 (write-back)

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 15747

Kernel command line: root=/dev/mtdblock0 rw earlyprintk=serial,uart0,57600

ip=10.100.4.50:10.100.4.174:10.100.4.174:255.255.255.0:bf548-ezkit:eth0:off

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 256 (order: 8, 1024 bytes)

console handover: boot [early_BFuart0] -> real [ttyBF0]

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

...

...

root:/> successful boot attempt

version

kernel:    Linux release 2.6.28.10-ADI-2009R1-pre-svn6364, build #229 Mon May

18 19:07:43 GMT 2009

toolchain: bfin-uclinux-gcc release gcc version 4.1.2 (ADI svn)

user-dist: release svn-8068, build #2295 Mon May 18 19:06:10 GMT 2009

root:/>

*******************************************************************

STEP 3: Start testing.

 

 

cd scsi 1:0:0:0: Direct-Access     SanDisk  U3 Cruzer Micro  6.51 PQ: 0 ANSI: 0

CCS

sd 1:0:0:0: [sdb] 2014271 512-byte hardware sectors: (1.03 GB/983 MiB)

sd 1:0:0:0: [sdb] Write Protect is off

sd 1:0:0:0: [sdb] Assuming drive cache: write through

sd 1:0:0:0: [sdb] 2014271 512-byte hardware sectors: (1.03 GB/983 MiB)

sd 1:0:0:0: [sdb] Write Protect is off

sd 1:0:0:0: [sdb] Assuming drive cache: write through

sdb:/ sdb1 sdb2

bsd 1:0:0:0: [sdb] Attached SCSI removable disk

in

root:/bin> ./watchdogd

Start in daemon mode.

r

Case 1 ...PASS

oot:/bin> ps aux| grep watchdogd | head -1

  343 root        32 S    ./watchdogd -f

root:/bin>

Case 2 ...PASS

kill -9 343

bfin-wdt: Unexpected close, not stopping watchdog!

root:/bin>

Last passed time: 2009_May_18_14_52, ucdist ver: 8068, kernel ver: 6364

 

Case 3 ...FAIL

 

 

Passed log:

U-Boot 1.1.6-svn1273 (ADI-2008R1.5) (Jul 21 2008 - 00:35:28)

 

CPU:   ADSP bf548-0.0 (Detected Rev: 0.2)

Board: ADI BF548 EZ-Kit board

       Support:   blackfin.uclinux.org/

Clock: VCO: 525 MHz, Core: 525 MHz, System: 131 MHz

RAM:   64 MB

Flash:

RAM size is 64 MB.

16 MB

NAND:  256 MiB

In:    serial

Out:   serial

Err:   serial

Net:   LAN9x18 (0x118a0000) detected at 0x24000000

MAC:   00:E0:22:FE:BF:4E

Hit any key to stop autoboot:  0

bfin> set bootargs root=/dev/mtdblock0 rw earlyprintk=serial,uart0,57600

bfin> set serverip 10.100.4.174

bfin> set ipaddr 10.100.4.50

bfin> save

Saving Environment to EEPROM...

..done

bfin> tftpboot 0x2000000 uImage

start Auto negotiation... (take ~2sec)

Auto negotiation complete, 100BaseTX, full duplex

TFTP from server 10.100.4.174; our IP address is 10.100.4.50

Filename 'uImage'.

Load address: 0x2000000

Loading: #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         ############

done

Bytes transferred = 5386071 (522f57 hex)

Image size is 522f57

bfin> run addip

bfin> bootm

## Booting image at 02000000 ...

   Image Name:   Linux-2.6.28.10-ADI-2009R1-pre-s

   Created:      2009-05-18  19:08:02 UTC

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    5386007 Bytes =  5.1 MB

   Load Address: 00001000

   Entry Point:  0026178c

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 26178c

Linux version 2.6.28.10-ADI-2009R1-pre-svn6364 (test@uclinux61-bf548-std) (gcc

version 4.1.2 (ADI svn)) #229 Mon May 18 19:07:43 GMT 2009

console [early_BFuart0] enabled

early printk enabled on early_BFuart0

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x001923e0

  rodata    = 0x001923e0-0x0021d918

  bss       = 0x0021e000-0x00232150

  data      = 0x00232150-0x0024c000

    stack   = 0x0024a000-0x0024c000

  init      = 0x0024c000-0x009f8000

  available = 0x009f8000-0x03dff000

  DMA Zone  = 0x03e00000-0x04000000

Hardware Trace Active and Enabled

Boot Mode: 3

Reset caused by Software reset

Blackfin support (C) 2004-2009 Analog Devices, Inc.

Compiled for ADSP-BF548 Rev 0.2

Blackfin Linux support by   blackfin.uclinux.org/

Processor Speed: 525 MHz core clock and 131 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

Data Cache Enabled for CPU0 (write-back)

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 15747

Kernel command line: root=/dev/mtdblock0 rw earlyprintk=serial,uart0,57600

ip=10.100.4.50:10.100.4.174:192.168.0.1:255.255.255.0:bf548-ezkit:eth0:off

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 256 (order: 8, 1024 bytes)

console handover: boot [early_BFuart0] -> real [ttyBF0]

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 52708k/65536k RAM, (7856k init code, 1604k kernel code, 744k

data, 2048k dma, 572k reserved)

Calibrating delay loop... 1046.52 BogoMIPS (lpj=2093056)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (15 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (42 KB free)

Blackfin L2 SRAM: 128 KB (128 KB free)

PDA for CPU0 reserved at 00221000

net_namespace: 288 bytes

NET: Registered protocol family 16

Blackfin DMA Controller

ezkit_init(): registering device resources

SCSI subsystem initialized

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

...

...

root:/> version

kernel:    Linux release 2.6.28.10-ADI-2009R1-pre-svn6364, build #229 Mon May

18 19:07:43 GMT 2009

toolchain: bfin-uclinux-gcc release gcc version 4.1.2 (ADI svn)

user-dist: release svn-8068, build #2295 Mon May 18 19:06:10 GMT 2009

root:/>

************** STEP 3: Start testing.

 

cd /bin

root:/bin> ./watchdogd

Start in daemon mode.

root:/bin>

Case 1 ...PASS

 

Case 1 ...PASS

ps aux| grep watchdogd | head -1

  324 root        32 S

Case 2 ...PASS

 

Case 2 ...PASS

  ./watchdogd -f

root:/bin> kill -9 324

bfin-wdt: Unexpected close, not stopping watchdog!

root:/bin> usb 1-1: new high speed USB device using musb_hdrc and address 2

usb 1-1: configuration #1 chosen from 1 choice

scsi1 : SCSI emulation for USB Mass Storage devices

scsi 1:0:0:0: Direct-Access     SanDisk  U3 Cruzer Micro  6.51 PQ: 0 ANSI: 0

CCS

sd 1:0:0:0: [sdb] 2014271 512-byte hardware sectors: (1.03 GB/983 MiB)

sd 1:0:0:0: [sdb] Write Protect is off

sd 1:0:0:0: [sdb] Assuming drive cache: write through

sd 1:0:0:0: [sdb] 2014271 512-byte hardware sectors: (1.03 GB/983 MiB)

sd 1:0:0:0: [sdb] Write Protect is off

sd 1:0:0:0: [sdb] Assuming drive cache: write through

sdb: sdb1 sdb2

sd 1:0:0:0: [sdb] Attached SCSI removable disk

 

 

U-Boot 1.1.6-svn1273 (ADI-2008R1.5) (Jul 21 2008 - 00:35:28)

 

CPU:   ADSP bf548-0.0 (Detected Rev: 0.2)

Board: ADI BF548 EZ-Kit board

       Support:   blackfin.uclinux.org/

Clock: VCO: 525 MHz, Core: 525 MHz, System: 131 MHz

RAM:   64 MB

Flash: 16 MB

NAND:  256 MiB

In:    serial

Out:   serial

Err:   serial

Net:   LAN9x18 (0x118a0000) detected at 0x24000000

MAC:   00:E0:22:FE:BF:4E

Hit any key to stop autoboot:  0

start Auto negotiation... (take ~2sec)

 

Maybe this bug should move to the u-boot bug tracker.

 

--- Mike Frysinger                                           2009-06-02 04:04:26

are you sure this isnt a dupe of [#4942] ?  your tests there arent equivalent.

the first is u-boot in parallel flash while the second is in spi flash.

 

--- Mingquan Pan                                             2009-06-02 22:25:22

There should be two issues, because this kernel config CONFIG_PM is not set and

I try reboot with this kernel, it is ok.

The detailed config is attached.

 

--- Graf Yang                                                2009-06-04 01:00:19

You have not remove 'watchdog -f -s' from /etc/inittab

 

...

Have a lot of fun...

 

BusyBox v1.13.4 (2009-06-04 11:47:42 GMT) built-in shell (msh)                

 

Enter 'help' for a list of built-in commands.                                 

 

                                                                              

 

root:/> ps aux | grep watch                                                

  

    4 root         0 SW<  [watchdog/0]                                     

  

  239 root       484 S    /bin/watchdogd -f -s                                

 

root:/> kill -9 239                                                        

  

bfin-wdt: Unexpected close, not stopping watchdog!                            

 

root:/> ps aux | grep watch                                                

  

    4 root         0 SW<  [watchdog/0]                                     

  

  243 root       484 S    /bin/watchdogd -f -s

 

so you can't kill watchdogd, and the board will not reset.

 

It's not a bug.

 

--- Graf Yang                                                2009-06-04 21:59:42

Grace,

Sorry, now I duplicated this bug, boot nor flash fail, but spi flash is OK,

under debugging.

 

--- Graf Yang                                                2009-06-09 02:50:09

Fixed.

This intel nor flash chip is in status mode when watchdog reboot happen, this

cause nor flash boot fail.

Now it is put into array mode, after chip is unlocked.

None-intel chip will not do unlock operation in this case, so have not this

bug.

 

--- Mingquan Pan                                             2009-06-18 04:56:03

Yes, fixed. Close.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

config.watchdog    application/octet-stream    40730    Mingquan Pan

Attachments

Outcomes