[#4882] up arrow key works abnormal for bf561 ezkit board

Document created by Aaronwu Employee on Aug 30, 2013
Version 1Show Document
  • View in full screen mode

[#4882] up arrow key works abnormal for bf561 ezkit board

Submitted By: Mingquan Pan

Open Date

2009-02-10 05:11:21     Close Date

2010-07-11 19:51:13

Priority:

Medium     Assignee:

Nobody

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2009R1-RC6     Release:

Category:

N/A     Board:

N/A

Processor:

BF561     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

4.1 of Jan 16

App binary format:

N/A     

Summary: up arrow key works abnormal for bf561 ezkit board

Details:

 

up arrow key works abnormal for bf561 ezkit board now.

 

## Booting image at 02000000 ...

   Image Name:   Linux-2.6.28.3-ADI-2009R1-pre-sv

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    3570899 Bytes =  3.4 MB

   Load Address: 00001000

   Entry Point:  0017527c

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 17527c

Linux version 2.6.28.3-ADI-2009R1-pre-svn6083 (test@linux) (gcc version 4.1.2 (ADI svn)) #9 Tue Feb 10 17:07:59 GMT-8 2009

console [early_BFuart0] enabled

early printk enabled on early_BFuart0

Warning: limiting memory to 56MB due to hardware anomaly 05000263

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x000fdb20

  rodata    = 0x000fdb20-0x00149e94

  bss       = 0x00149ea0-0x00158ad0

  data      = 0x00158ad0-0x00168000

    stack   = 0x00166000-0x00168000

  init      = 0x00168000-0x006b7000

  available = 0x006b7000-0x037ff000

  DMA Zone  = 0x03f00000-0x04000000

Hardware Trace Active and Enabled

Boot Mode: 0

Reset caused by Software reset

Blackfin support (C) 2004-2009 Analog Devices, Inc.

Compiled for ADSP-BF561 Rev 0.3

Blackfin Linux support by   blackfin.uclinux.org/

Processor Speed: 600 MHz core clock and 100 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

Data Cache Enabled for CPU0 (write-through)

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 14223

Kernel command line: root=/dev/mtdblock0 rw earlyprintk=serial,uart0,57600

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 256 (order: 8, 1024 bytes)

console handover: boot [early_BFuart0] -> real [ttyBF0]

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 49884k/65536k RAM, (5436k init code, 1010k kernel code, 426k data, 1024k dma, 7756k reserved)

Calibrating delay loop... 1196.03 BogoMIPS (lpj=2392064)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (15 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 16 KB (9 KB free)

Blackfin L2 SRAM: 128 KB (128 KB free)

PDA for CPU0 reserved at 0014b0c0

net_namespace: 288 bytes

NET: Registered protocol family 16

Blackfin GPIO Controller

Blackfin DMA Controller

ezkit_init(): registering device resources

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

NET: Registered protocol family 1

BF561 Core B driver v0.1 initialized.

msgmni has been set to 97

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc00400 (irq = 35) is a BFIN-UART

brd: module loaded

smc91x.c: v1.1, sep 22 2004 by Nicolas Pitre <nico@cam.org>

eth0: SMC91C11xFD (rev 1) at 2c010300 IRQ 82 [nowait]

eth0: Ethernet addr: 00:e0:22:fe:b2:01

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@16

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

TCP cubic registered

NET: Registered protocol family 17

Freeing unused kernel memory: 5436k freed

dma_alloc_init: dma_page @ 0x006b4000 - 256 pages at 0x03f00000

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            -   blackfin.uclinux.org/

\    YP"    `| 8P  `.          -   docs.blackfin.uclinux.org/

/     \.___.d|    .'           -   www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    -   www.analog.com/blackfin

 

Have a lot of fun...

 

 

BusyBox v1.13.2 (2009-02-10 17:01:05 GMT-8) built-in shell (msh)

Enter 'help' for a list of built-in commands.

 

root:/> ifconfig

lo        Link encap:Local Loopback

          inet addr:127.0.0.1  Mask:255.0.0.0

          UP LOOPBACK RUNNING  MTU:16436  Metric:1

          RX packets:0 errors:0 dropped:0 overruns:0 frame:0

          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0

          collisions:0 txqueuelen:0

          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

 

root:/> ifconfig eth0 10.100.4.50

eth0: link down

root:/> eth0: link up, 100Mbps, full-duplex, lpa 0x45E1

pwd

/

root:/> ls

bin   etc   init  mnt   root  sys   usr

dev   home  lib   proc  sbin  tmp   var

root:/> pwd

/

root:/> ls

bin   etc   init  mnt   root  sys   usr

dev   home  lib   proc  sbin  tmp   var

root:/> pwd

/

root:/> ls

bin   etc   init  mnt   root  sys   usr

dev   home  lib   proc  sbin  tmp   var

root:/> date

Mon Jan  1 00:00:42 UTC 2007

root:/> date

datehh: not found

root:/> pwd

/

root:/> date梃

datehh: not found

root:/> ls

bin   etc   init  mnt   root  sys   usr

dev   home  lib   proc  sbin  tmp   var

root:/> pwd

/

root:/> date

Mon Jan  1 00:00:58 UTC 2007                                                                                                                              

 

It would give out abnormal sound when you firstly hit the uparrow key, and it would not reponse until about the third time. And sometimes there is random characters show up.

 

Follow-ups

 

--- Graf Yang                                                2009-02-27 00:57:31

Both DMA and PIO mode have this bug.

 

It seems it is a timing compatible issue.

When I connect BF561 board with desktop or laptop serial ports, both of them

have random chars.

When I use a USB2Serail dangle to connect to the BF561 board, all the things

are OK.

 

 

--- Graf Yang                                                2009-02-27 04:33:32

Use the equation on HRM instead of the common code equation to calculate the

divisor for uart. Now it's OK.

I also tested it for BF537(both DMA/PIO), it is OK.

 

 

 

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

 

File Name     File Type     File Size     Posted By

No Files Were Found

Attachments

    Outcomes